Custom Meta Tags

Category Attributes

Category Attributes

Category Attributes

Training & Events
No related Training & Events found

Articles Categories SEO Wrapper

Interconnect, Passives & Electromechanical

Interconnect, Passives & Electromechanical RSS FEED

 
 
As electronic equipment and devices become more and more integrated into our daily lives, speedy and reliable data, content and power transfer will rely on your ability to select the right, high quality products. Explore our resources to stay up to date in the world of IP&E trends, technology, and technical expertise.

A printed circuit board showing power components
Six capacitor design takeaways for power supply engineers
By Avnet Staff   -   22/09/2026
Power supplies are found in almost every electronic design, yet each one has different characteristics. Passive components may appear consistent, but their behavior changes with the application, too. Here’s how.
An open-frame power supply showing heatsinks, transistors and capacitors
Reducing ESL in power distribution networks
By Avnet Staff   -   22/09/2026
Power distribution networks depend on capacitors for stability and suppression. As switching frequencies increase, equivalent series inductance (ESL) can dominate capacitance and reduce effectiveness. New developments are tackling the issue.
A power supply PCB showing electrolytic capacitors alongside power transistor heatsinks
How dielectric innovation is reshaping capacitor selection for high-power designs
By Avnet Staff   -   22/09/2026
The latest growth markets are pushing capacitors harder. Learn how new dielectric materials help engineers improve density, stability and reliability in high-stress power applications.
An open-frame power supply showing transformers and electrolytic capacitors
DC bias derating in multi-layer ceramic capacitors is a focus area for suppliers
By Avnet Staff   -   22/09/2026
Using doping and other materials science methods, capacitor suppliers are tackling DC bias derating in MLCCs, even as customers demand smaller packaging and higher capacitance.
A selection of electrolytic capacitors on a bronze PCB
Capacitor manufacturers are reacting to changing demand for lower ESR
By Avnet Staff   -   22/09/2026
Equivalent series resistance (ESR) is inherent in capacitors, and an unwanted parasitic. Manufacturers continue to work hard to reduce or even eradicate ESR, while end markets continue to determine future directions.
*Image alternate text (explanation of the image subject):   A closeup image of a small power supply on a PCB, showing a transformer and electrolytic capacitor
Capacitor innovations helping engineers manage ripple current effects
By Avnet Staff   -   22/09/2026
Ripple current is unavoidable, but it doesn’t have to be catastrophic. Lowering ESR, improving thermal paths and increasing operating parameters help. Designing around the problem can also be a solution.
operator sitting at a control station using a keyboard and electromechanical user interface
Meet the joystick that’s also a rotary encoder
By Philip Ling   -   02/07/2026
The Series 293 provides three controls in a single, compact solution. By combining a joystick, push-button switch and rotary encoder in one element, OEMs can build sophisticated software-defined user interfaces that are intuitive and innovative.
connectors used in computer water cooling
Beyond the datasheet: New connectors for liquid cooling
By Philip Ling   -   10/12/2025
Using liquids for heat exchange isn’t new in the industrial, aerospace and automotive industries. Now, as power dissipation in servers climbs above the 10s and into the 100s of kWs, it’s time to use the same approach for a different technology.
A collage of thermal management technologies
Thermal innovations keep high-performance electronics cool
By Avnet Staff   -   04/04/2025
Thermal management solutions are innovating rapidly to address the challenge of keeping electronic systems cool as they get smaller and faster, oftentimes used in combination to spread and transfer the heat.
connectors in rain
Connectors for harsh environments
By Avnet Staff   -   02/04/2025
The right connectivity solution for harsh environments depends on an understanding of the disruptive environmental factors and how they affect sensitive equipment. With this knowledge, engineers can select connectors
yellow medical device
Meeting the challenges of medical cable assembly design
By Avnet Staff   -   01/04/2025
Cable assemblies play a crucial role in the medical industry, providing the essential connection between medical devices, patients and healthcare professionals. These assemblies must meet stringent requirements to ensure patient safety while delivering re...
5G connectivity illustration
An introduction to mmWave connectors for 5G wireless networks
By Avnet Staff   -   16/07/2024
Addressing the challenges of mmWave for 5G networks requires careful system design and mmWave RF connector selection to help maximize link range, ensure link reliability and protect signal integrity.
Passive components glowing on a pcb
AI is impacting passive and interconnect design
By Avnet Staff   -   22/02/2024
Engineers selecting passive and power components must consider the needs of AI running in the cloud and on high-performance computers. Moving huge amounts of data around is also influencing interconnect design.
exploded-view-of-a-cellphone-showing-interconnect
Explore interconnect innovations that save space
By Avnet Staff   -   16/01/2024
Demand for electronic interconnect prioritizes smaller sizes and more connections. Delivering both without sacrificing reliability, usability or incurring higher costs are challenges.
EV charging devices
Passive components in EV chargers should be selected carefully
By Neil Willard   -   15/01/2024
Demand for EV fast charging stations means passive components that can tolerate the high power/high energy environment are also drawing attention. Components such as DC link capacitors and magnetics need to be carefully selected for the application.
surgeon checking a patient's monitoring equipment
Intro to Standard Molex Products and How They Are Integrated into Medical Applications
By Jamie Pederson   -   21/06/2023
Interconnect technology is designed for nearly every application imaginable including medical products. Molex designs and develops cutting-edge standard products with the quality and reliability that meet the rigorous needs of the medical industry.
A pcb with surface mount passive components
Crucial role of analog front ends, creating bridge to digital world
By Avnet Staff   -   29/04/2023
Analog front end, or AFE, is something every electronics engineer has heard of but may have difficulty defining. The design of these versatile circuits varies by application, making them essential even in a digital world.
Wide bandgap semiconductor material in its raw form
When GaN is too fast for your application, consider SiC instead
By Avnet Staff   -   24/04/2023
The best power converters are not always the ones that switch the fastest. Gallium Nitride (GaN) switches faster than other power transistors, but sometimes it is too fast. Silicon Carbide (SiC) MOSFETs may sometimes be a better option.
under the hood of an electric vehicle
Understand the sources of electromagnetic interference in electric vehicles
By Avnet Staff   -   24/04/2023
Electrical noise sources within vehicles fall into two types: electromagnetic inference (EMI) and electrostatic discharge (ESD). We explain these and the basic concepts of conducted and radiated EMI noise, with relevant examples.
Conceptual image of smart car in purple
Digital interfaces are driving data in the automotive sector
By Avnet Staff   -   03/04/2023
High-speed automotive networks link independent control units. This article compares the role and specifications of Ethernet, CAN and SPE, and explores recent network innovations enabling zonal network architectures.
graphic depicting different types of automotive connectivity
Solutions for transportation design pain points don’t have to be daunting
By Jamie Pederson   -   21/03/2023
Transportation engineers seeking solutions to overcome today’s most common design pain points can look to the industry’s long history of innovation for inspiration.
electric vehicle dashboard
What does the future of automotive technology look like?
By Jamie Pederson   -   09/05/2022
The automotive industry is becoming more technologically advanced at a fast pace from comfort and infotainment to advanced safety systems. This article explores the trends as vehicles become data centers on wheels.
engineer assembling connectors
What to consider when choosing a connector (interconnect solution)
By Jamie Pederson   -   21/04/2022
Selecting interconnect products for your project is a crucial step in the design process and there are several things to keep in mind when making those decisions. In this article we’ll discuss the most common considerations and how interconnect ma
electric vehicle dashboard
What is polarization, keying and color coding for interconnect?
By Jamie Pederson   -   10/04/2022
Establishing a properly aligned connection quickly is key in any assembly or installation process. Polarization, keying and color coding are primary means to ensuring connections are made quickly and safely. In this article we’ll discuss each of
digitally connected city
The 5G interconnect design challenges and their solutions
14/10/2021
Avnet spoke with Molex Global Product Manager Mike Hansen about the role copper interconnect is playing in the development of the next high-speed cellular network.
woman using mobile device in remote location
What to know about electromechanical interconnects for 5G systems
12/10/2021
High-performance radio frequency, input/output and board connectors are helping developers meet the challenge of 5G. Designed for mmWave and PAM-4 signals in the fronthaul of the network, engineers can use them to improve signal integrity.
Li-ion battery
To fight EV fires, focus is on early detection of battery cell thermal runaway
11/08/2021
Sensing solutions that focus on decomposition gases are being used to focus on early detection of battery cell thermal runaway.
Silicon carbide (SiC) and Gallium nitride (GaN)
The substantial benefits of silicon carbide (SiC) and gallium nitride (GaN) in power electronics
By Milan Ivkovic   -   08/03/2021
Silicon carbide (SiC) and gallium nitride (GaN) are two semiconductor materials that are creating a significant shift in the power electronics market.
person using tools
IP&E sourcing considerations for developers
08/08/2019
Designing with IP&E components comes down to more than just simple part selection.
Robotic arm industrial Internet of Things and Industry 4.0
Wired together: How automation systems power the Industrial Internet of Things
16/07/2019
From process control and automotive assembly, to robotics and the food and beverage industry, the concept behind Industry 4.0 touches all industries.
Results Per Page: