Article

How dielectric innovation is reshaping capacitor selection for high-power designs

Avnet A Frame
A power supply PCB showing electrolytic capacitors alongside power transistor heatsinks
The dielectric characteristics of capacitors dictate their performance in power supplies.
KEY TAKEAWAYS:
  • New dielectric materials tackle energy density, higher voltages and higher temperatures
  • EVs and other power stages increase the need for stable capacitance under extreme stress
  • The right capacitor can come down to dielectric type and its influence

Capacitors are evolving to meet the demands of higher-density, higher-voltage and higher-temperature electronics. For engineers, the most important changes are happening inside the component: in the dielectric materials and electrolyte systems that determine capacitance stability, lifetime, ripple performance and reliability under stress.

Capacitor manufacturers are responding to demand for components that deliver higher energy density, higher operating temperatures and higher voltage ratings. Much of that demand is coming from fast-growing applications, including EVs, wide bandgap power conversion and 5G infrastructure.

The pull from manufacturers in these emerging applications is driving the development of refined dielectrics and films used in, for example, new classes and grades of automotive-qualified multi-layer ceramic capacitors (MLCCs).

EV traction inverters, onboard chargers and advanced driver assistance systems (ADAS) use more capacitors operating under greater electrical and thermal stress. This is increasing demand for MLCCs with higher temperature ratings, higher voltage ratings and more predictable capacitance under DC bias.

Wide bandgap (WBG) power stages using silicon carbide and gallium nitride expose capacitors to faster voltage transitions, higher operating frequencies and demanding ripple-current profiles, so dielectric stability and lifetime under electrical and thermal stress become more important. For 5G, density is a major driver, requiring very small high-k dielectrics that remain stable over wide temperature ranges.
 

Developments in dielectric stability

Capacitor suppliers continue to refine materials that combine high relative permittivity, or k, with better dielectric stability and lower sensitivity to temperature and DC bias. In MLCCs, this typically involves doping the base material, usually barium titanate (BaTiO3). Although barium titanate has a naturally high relative permittivity, its crystal structure changes with temperature. It also behaves non-linearly, so capacitance can fall as voltage and temperature increase. Doping helps counteract these effects.

Dopants such as strontium, zirconium and calcium zirconate can shift or broaden the temperature range over which the crystal structure changes. Using dopants with different relative permittivity values can create two dielectric-constant peaks, helping to flatten the overall temperature response. Other dopants help neutralize oxygen vacancies that form during sintering or improve the sintering process itself.

These efforts are all in direct response to the demand for higher and more stable capacitance in smaller packages operating at higher voltages–driven by the automotive market but also the growth of 5G.

Polymer and hybrid aluminum electrolytics show that dielectric and electrolyte innovation is not limited to MLCCs. In automotive and industrial applications, these capacitor types have gained attention because they offer higher energy density, better high-frequency behavior and improved temperature performance compared with conventional liquid electrolytics.

For high-power switched-mode power supplies (SMPSs), hybrid aluminum capacitors that combine a polymer layer with liquid electrolyte achieve lower equivalent series resistance (ESR), high ripple capability and extended lifetimes at higher temperatures.

These changes are more evolutionary than revolutionary, but have materially improved performance envelopes, especially for parts used in DC-links in traction inverters and onboard chargers in the EV space.
 

What’s next for high-k dielectrics?

Organic high-k materials are an active area of research, including asymmetrically fluorinated polymers. Inorganic fillers such as silicon dioxide, combined with polymer matrices, have also shown promise and may move toward commercial use as processing, reliability and cost challenges are resolved.

Although these are still at the research stage, leading capacitor manufacturers are exploring materials like these, and they form part of their long-term roadmaps.

For design engineers, the practical question is not whether dielectric technology is improving, but which capacitor structure is best suited to a specific electrical, thermal and mechanical environment. Voltage derating, DC bias, ripple current, ESR, operating temperature, lifetime expectations and qualification requirements all affect the final choice.

Avnet maintains close relationships with its capacitor suppliers, helping its field application engineers understand how each technology is evolving and where it fits best. That gives customers access to guidance on dielectric type, package size, voltage rating, temperature performance, ripple capability, lifetime and qualification requirements when selecting capacitors for demanding applications.

About Author

Avnet A Frame
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Marketing Content Spots

Related Articles

Related Articles
A wireframe of an electric car showing the battery and key electrical components
How the EV drivetrain is moving toward function consolidation
By Avnet Staff   -   September 23, 2026
EVs present new opportunities for function consolidation, delivering lower cost and weight, and simpler wiring. But the shift comes with challenges when combining power, control and safety in a single platform. NXP is leading the evolution.
A printed circuit board showing power components
Six capacitor design takeaways for power supply engineers
By Avnet Staff   -   September 22, 2026
Power supplies are found in almost every electronic design, yet each one has different characteristics. Passive components may appear consistent, but their behavior changes with the application, too. Here’s how.

Related Events

Related Events

No related events found

how-dielectric-innovation-is-reshaping-capacitor-selection-for-high-power-designs