Avnet /IOTCONNECT at Embedded World 2024
Join Avnet and our supplier partners at Embedded World, Nuremberg, Germany. We will be showcasing several live, real-time demonstrations showing how working with Avnet and /IOTCONNECT™ make IoT simple, secure, and scalable.
Register today - use code ew24518150 for free entry!
How /IOTCONNECT delivers
/IOTCONNECT is the cloud-ready solution designed exclusively for OEMs. Avnet’s technology provides pre-enablement of IoT applications running on any hardware and the world’s leading cloud software. Avnet’s /IOTCONNECT is based on accelerator software packages that include dashboards and templates designed for easy configuration. Avnet has accelerators to match an OEM’s application, across all vertical markets. The /IOTCONNECT SDKs are optimized by Witekio, an Avnet company, to work with leading silicon supplier MCU and MPU low-cost development kits as well as the two top IoT cloud service providers: AWS and Microsoft Azure. Avnet developed /IOTCONNECT by working with silicon suppliers and the two leading IoT cloud platform providers – Microsoft Azure and AWS. /IOTCONNECT delivers pre-integrated, fully supported services to build production ready, scalable solutions. Join the OEMs deploying cloud connected IoT applications in high volume with the help of /IOTCONNECT.
What visitors to Embedded World 2024 will experience
This year, Avnet will have a diverse set of /IOTCONNECT-enabled demonstrations ranging from renewable energy management, AI-enhanced smart city infrastructures, Industrial Automation and crowd monitoring.
Exhibit #1
STM32 Security & Regulations: Hybrid Solar Inverter Demo
Reference links: GitHub | Avnet Collaborates with STMicroelectronics on Cloud-Connected Solutions
Hybrid solar inverters combine solar panels with a battery. They are relied on by many to deliver uninterrupted power. This demonstration, based on STM32Trust TEE Secure Manager on the STM32H5 discovery kit, shows how to effectively secure hybrid solar inverters in a cloud-enabled application.
/IOTCONNECT is used to monitor and control the power output of the inverter remotely, providing real-time data reporting and facilitating secure firmware OTA updates.
By integrating /IOTCONNECT, the solution demonstrates how to deliver a service that is fortified against unauthorized access. OEMs can build on this demonstrator to deliver safe, reliable and efficient energy systems, pivotal to sustainable infrastructures though building and maintaining public confidence and trust.
STMicroelectronics press release
Contact us: Talk to our team about this demo.
Exhibit #2
Edge AI for smart cities with AWS and /IOTCONNECT
Reference links: GitHub
Smart cities are using cloud-connected sensors to help manage and monitor public areas. This demonstration shows how applying AI takes that up a level.
The demo is built using the STM32U5 Discovery Kit for IoT Node with the STM32Cube.AI, leveraging AWS SageMaker for advanced model training. The solution can accurately detect and report the location of noises in an urban environment, such as breaking glass, a car alarm, or distressed voices.
/IOTCONNECT provides the mechanism for seamless firmware management and AI inference model retraining and deployment.
Press release: Avnet Partners with ST on IoT Smart City Application Powered by AWS
Contact us: Talk to our team about this demo.
Exhibit #3
LACROIX AI/ML Audio Event Classification for Urban Environments
Reference links: GitHub
EBV engineers are showing a proof-of-concept developed for its customer, LACROIX, a smart city solutions provider. The demo is built using the STM32U5 Discovery Kit for IoT Node with the STM32Cube.AI, leveraging AWS SageMaker for advanced model training.
The solution can accurately detect and report the location of noises in an urban environment, such as breaking glass, a car alarm, or distressed voices.
/IOTCONNECT brings indispensable value to LACROIX’s smart city solution by managing firmware updates and model retraining with its secure cloud management platform. It gives fine-grained control and confidence-based event filtering, and real-time location within a smart city environment.
Press release: Avnet Partners with ST on IoT Smart City Application Powered by AWS
Contact us: Talk to our team about this demo.
Exhibit #4
Smart Home Solution Reference Design by Indeema
Reference links: Indeema
Smart homes can do more with /IOTCONNECT, as this demonstration proves. EBV partner, Indeema, will showcase a smart home solution featuring Microchip and Espressif MCUs running /IOTCONNECT.
Come to the EBV booth to see how climate, security and device charging are all controlled through the smart home solution. /IOTCONNECT was instrumental in creating the seamless environment, providing secure and scalable middleware that runs on either AWS or Azure.
See firsthand how smart device management is simplified using /IOTCONNECT dashboards. The real-time data visualization enhances operational efficiency and the user experience. With its robust APIs into the world’s leading IoT cloud platforms, /IOTCONNECT enables rapid deployment of smart home applications.
EBV IoT – /IOTCONNECT Cloud Platform
Contact us: Talk to our team about this demo.
Exhibit #5
SPARK – Smart Parking AI-Driven RZBoard featuring Renesas’ RZ DRP-AI accelerator
Reference links: Avnet RZBoard V2L | GitHub
Using the Avnet RZBoard V2L, a custom CNN (convolutional neural network) model and /IOTCONNECT, Avnet Embedded engineers have created a demonstration that shows how simply smart image sensing can be added to public spaces to help drivers find somewhere to park in a smart city.
This real-time parking demonstration uses a live camera feed to identify occupied and free parking slots. Through /IOTCONNECT, that information can be relayed in real-time to drivers as they enter the city’s limits.
/IOTCONNECT provides the scalable backend for device management and data handling. The seamless integration with AWS and Azure makes the AI-driven insights available in real-time to the wider infrastructure.
/IOTCONNECT also supports Renesas 32-bit MCUs
Contact us: Talk to our team about this demo.
Exhibit #6
Complete IoT Solution with Arduino Pro, Avnet Silica Cellular Connectivity and /IOTCONNECT
Reference links: GitHub | Arduino PRO from Silica
Combining the Arduino Pro Portenta C33 board, a Pro Carrier Board and a 4G cellular connectivity module, Avnet Silica engineers show how Industrial IoT is becoming simpler and more secure to implement using /IOTCONNECT.
Avnet’s engineers have made it seamless to integrate /IOTCONNECT with the Arduino Pro Portenta C33 and Arduino framework. This integration provides device management middleware for cloud services running on AWS.
This demonstration not only shows the high-performance capabilities available in the Arduino ecosystem, but also the versatility and ease-of-use that /IOTCONNECT brings to Industrial IoT applications.
Get started today with /IOTCONNECT
Contact us: Talk to our team about this demo.
Exhibit #7
Panasonic People Flow Analytics with /IOTCONNECT
Reference links: Panasonic Bluetooth and WiFi modules from Abacus
See a dynamic people counter in action, using 40 networked sensors distributed around the exhibition halls 3 and 3A.
This demonstration is using /IOTCONNECT as the central hub, aggregating data from the sensors. It shows the distribution of visitors, plus environmental data captured by the sensors, including CO2 levels, temperature, and humidity – all in real time.
/IOTCONNECT is relaying sensor telemetry to a time-series database in AWS, enabling real-time visualization of hall occupancy and environmental conditions. This demonstrates the scalability and adaptability of /IOTCONNECT when managing complex IoT ecosystems.
Contact us: Talk to our team about this demo.
Exhibit #8
WITH: Yocto
Chip to Cloud EV Charging Solution
Reference links: GitHub | Avnet Embedded module featuring the NXP™ i.MX 8M Plus
This demonstration shows how home EV charging solutions can be enhanced with /IOTCONNECT, utilizing AWS services for optimal energy management.
Using /IOTCONNECT, the engineers behind this demonstration have integrated more than fourteen AWS services. The result is a secure and scalable user-friendly platform with real-time visualization and control of energy usage.
This device-first approach shows how /IOTCONNECT can deliver future-proof EV charging solutions that are ready to expand to include faster charging and the integration or renewable energy sources.
Get started today using /IOTCONNECT
Contact us: Talk to our team about this demo.
Avnet /IOTCONNECT at Embedded World 2024
Read our press release
Read NowGet Started using /IOTCONNECT Today
See how /IOTCONNECT is the fastest and most scalable way to securely connect your connected products to the cloud
Learn MoreGet the code
Download /IOTCONNECT code and run it on a range of development boards from our semiconductor supplier partners
Go To GitHub