Circuit Protection: Helping Drive Reliability and Longer Life

Display portlet menu

Circuit Protection: Helping Drive Reliability and Longer Life

yellow key imbossed on micromicrochip attached to circuitboard

The primary concerns of engineers designing mobile devices connected to the IoT remain device functionality, performance and feature set. With more devices connected to the IoT intended for long life, remote operation circuit protection increasingly takes a higher priority during the design cycle.

  • Mobile device users often interact with the device using touchscreens, push buttons, switches and connectors. These user interfaces can produce ESD events on the supporting circuitry. ESD protection devices – like ESD suppressors and TVS diodes – help protect against ESD failures.
  • Some mobile devices support higher data throughput in the Gbps ranges. Providing ESD protection at higher frequencies and higher data rates requires smaller device capacitance and faster response times. The circuit protection manufacturers consistently innovate to the needs of the market, and the current generation of ESD protection devices provide sub-picofarad channel capacitance and nanosecond response times.
  • Mobile devices also make use of a single or several RF signal chains. Because of increased signal gain demands and reduced RF transistor insulation layers, RF circuits are susceptible to ESD events. Many RF circuits have internal ESD protection, and these help protect the RF circuitry during manufacturing. Additional external ESD protection is required for use by end users in many applications.
  • Passive circuits are often used in applications, but ultra-low capacitance TVS multilayer varistors provide a single chip solution that replaces capacitors, passive filters and diode clamps. The reduction in component count and PCB space lowers installation costs, and the minimal insertion loss drives superior performance in these devices.
  • Another area where mobiles devices require circuit protection is the battery. Batteries are often hot-swappable, so they may be subject to overcurrent conditions such as short circuit or overloads. Resettable fuses from the leading circuit protection manufactures are often times a good approach in this application. Since most resettable fuses are usually made of conductive plastics, they enter a high-resistance state when a fault occurs. And, when the fault is removed, the resettable fuse enters its normal low-resistive state.
  • Low resistance resettable fuses are essential to longer battery life and higher power efficiencies in battery-powered applications. Circuit protection manufacturers continually increase conductivity of their resettable fuses to drive adoption into IoT nodes. Whatever circuit protection solutions are needed, Avnet and our suppler partners provide the right answer at the right time. Our factory-certified FAEs and our online resources keep engineers updated on the latest circuit protection needs

Related Articles
man using tablet computer
Specialists vs. end-to-end partners: the pros and cons for developers
March 27, 2019
Getting a product to market requires more than just the right idea; it also needs the right partner.
person holding superimposed globe with IoT symbols
Reimagining the ‘things’ of IoT
By Bill Amelio   -   February 28, 2019
While our collective vision for IoT’s impact on the future is grand in scale, it is still too easy for companies to get distracted by the minutiae of our present day IoT challenges.
Engineer participating in online community on desktop computer
In their words: Benefits of the world’s biggest engineering community
September 5, 2018
In the summer of 2018, Avnet celebrated a major milestone: 1 million community members across Hackster.io and element14. Here's the value of these communities from the members themselves.
Three people sitting around a coffee table playing a game with Spatial Gaming
Hardware Studio Helped Spatial Gaming Get Funding
August 15, 2018
If gaming 1.0 is analog board games and gaming 2.0 is video games, then Spatial Gaming is solidly 3.0—merging face-to-face interaction with high quality graphics using augmented reality.
Two young men and young woman looking at tablet computer in datacenter
IoT Technology 101
By Christian Curtis   -   March 6, 2018
Learn what’s in market today for IoT and what innovations are ahead.
Two men and woman reviewing technology products.
3 ways All Programmable SoCs create new opportunities for designers
March 2, 2018
In the growing market of embedded vision, there’s a need to not only rapidly scale to compete but to also be ready for machine learning’s effect on the space. That’s all while keeping up with lightning fast design cycles.
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
Using Programmable Logic to Build Power-Efficient Systems
March 8, 2017
The successful implementation of the Internet of Things (IoT) requires new thinking about how to power connected devices.
Related Events

No related events found