Article

Using digital twins for hardware component selection

Nishant Nishant
A base station in an industrial setting with a digital twin represented alongside
Digital twins are already used in cellular communications to monitor and control infrastructure. Those same models could help improve the design process.
KEY TAKEAWAYS:
  • Digital twins in RF development enhance hardware component selection
  • Real-world simulation of RF components improves decision making earlier in the design process
  • AI is being used to accelerate the simulation process, making scenario exploration faster

A digital twin is a virtual representation of a real-world component, system or process. Twins are intended to enable real-time operational data exchange and are used by mobile network providers to optimize operations.

During development, RF teams may use twins to explore architectures, channels and algorithms, but then switch back to datasheets, application notes and bench tests to pick parts. That separation can leave a great deal of value on the table. Teams define KPIs such as spectral efficiency, coverage probability, coexistence performance, and power budget, choose an RF architecture to hit them, and then narrow the hardware options. At that point, device selection usually falls back to familiar inputs such as noise figure, gain, 1dB compression point (P1dB), adjacent channel power ratio (ACPR), phase noise and reference schematics.

These figures rarely reflect the environment the part will see in the field. A regulator that appears unremarkable in isolation may become a dominant spur source when it interacts with the real power delivery network (PDN). A low-noise amplifier with excellent headline performance may collapse under blockers and self-interference in a crowded spectrum environment.

Digital twins close that gap by stressing each candidate device inside a realistic system model, enabling teams to ask not whether a part meets its published limits, but whether it preserves system-level margin under realistic operating conditions. The same models already trusted for link budgets and coverage can also reveal why one regulator, connector or RF front end is a safer choice than another once it sits in the actual system.

How digital twins can reduce risk

Many RF problems are rooted in layout or power-delivery behavior rather than in the RF silicon itself. A board-level digital twin helps expose those weaknesses early. Built from the stackup (PCB layer arrangement), routing, via structures, and package or connector models, it shows how the electrical behavior of the design changes once candidate parts are placed in context.

For high-speed digital interfaces feeding RF subsystems, this kind of twin makes it possible to compare connector families and interconnect choices against the real timing and loss budgets of the design. A connector that looks acceptable in isolation can become problematic once bends, vias and return-path discontinuities are included.

On the power side, PDN analysis reveals how regulators, decoupling and plane geometries behave under simultaneous switching loads. Two pin-compatible regulators with similar efficiency and ripple numbers can perform very differently when the actual board parasitics are present. One may inject spectral content into sensitive rails or exhibit control-loop behavior that degrades the RF chain, while another remains quiet and predictable. In that situation, the digital twin turns signal integrity (SI) and power integrity (PI) behavior into a decisive part-selection criterion.

Why thermal digital twins matter for RF performance

Thermal behavior is often treated as a reliability topic, but for RF systems, it is just as much a performance issue. Gain, noise figure, compression, oscillator stability, and beamforming calibration can all shift with temperature. In dense radio designs, the difference between a component that runs warm and one that runs hot often determines whether a system meets or misses KPIs in the field.

A thermal twin gives teams a way to quantify that risk in the context of the real-world product. By combining compact models of packages and modules with realistic PCB, enclosure and airflow conditions, the twin shows how heat spreads through the design during real transmit and receive duty cycles. That can change component choices quickly.

Two front-end modules may share a footprint and look nearly identical in a datasheet table, yet one may run significantly hotter once mounted near power devices or under a shield with limited airflow. The hotter part may suffer gain droop, reduced linearity or shortened lifetime even though it appears acceptable on paper. In that case, the digital twin justifies the choice of a less obvious device because it preserves RF performance more consistently over temperature and time.

The real shift happens when digital twins stop being viewed as verification tools and become selection gates. Instead of validating a nearly finished design, teams can define early in the architecture phase what a preferred component must prove in simulation before it is accepted.

Used this way, the digital twin becomes part of the decision process rather than a supporting document. It also improves supplier conversations. When teams ask for usable behavioral, S-parameter and thermal models instead of static PDFs alone, they make it clear that system context matters as much as peak datasheet numbers. That, in turn, encourages a more realistic and more resilient selection flow.

How AI will accelerate digital twin-based BoM optimization

The main obstacle to twin-driven part selection is usually effort. Detailed SI, thermal and RF simulations take time to build and run, especially when many candidate devices are under consideration. AI and machine learning are beginning to make that process lighter by supporting surrogate models, reduced-order twins, and smarter design-space exploration.

As those methods mature, teams will be able to explore broader sets of regulators, front-end modules and filters without rerunning every high-fidelity simulation from scratch. AI can help identify which scenarios are most informative, where margins are weakest, and which substitutions are least likely to break system KPIs. That does not remove the need for engineering judgment, but it does make digital-twin-based BoM optimization far more practical in normal development schedules. RF systems architects will see digital twins as a routine part of component convergence rather than an advanced technique reserved for the most difficult programs.

What value do digital twins provide in RF design?

Twin type Selection role Key factors Decision question answered Typical components

RF system twin

KPI-based selection

Coverage, throughput, coexistence, blocker response, nonlinear behavior, system margin

Which RF front-end preserves KPIs under real deployment conditions?

LNA, PA, mixer, filter, switch

Board-level twin

SI/PI screening

Stackup, routing, vias, return paths, PDN, parasitics → SI/PI-induced spurs, jitter, EVM

Which regulator or interconnect behaves cleanly in the actual board PDN and layout?

Connectors, interconnects, regulators, PDN design choices

Thermal twin

Temperature-aware selection

Heat spread, airflow, enclosure → gain drift, NF shift, linearity, calibration stability

Which components maintain RF performance across real thermal conditions?

FEMs, packages, power devices

Cross-domain workflow

Multi-constraint convergence / BOM gate

Electrical, RF, thermal interactions under deployment conditions

Which combination of components meets all system constraints simultaneously?

Regulators, FEMs, filters, connectors, packages

AI-assisted twin

Fast candidate pruning / design-space acceleration

Surrogate models, reduced-order models, scenario ranking, margin hotspot identification

Which candidates can be eliminated or prioritized without full simulation?

Regulators, FEMs, filters

Why RF engineers are linking digital twins to the BoM

When component choices are validated inside living models of the real design, teams are less likely to discover fragile behavior on first prototypes and less likely to waste spins on parts that were only “drop-in” on paper. More importantly, they gain a disciplined way to connect system intent with hardware reality. For RF systems architects, that is the real opportunity. Digital twins can do more than proving an RF concept can work. They should help decide which specific pieces of silicon, power hardware and interconnect technology will enable it to work robustly in the field.

About Author

Nishant Nishant
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Marketing Content Spots

Related Articles

Related Articles
A wirelessly connected battery-powered industrial sensor sits on top of an electric motor housing.
Rethinking RF and analog front ends for smarter edge AI
By Avnet Staff   -   July 2, 2026
This article treats RF and AI as one design problem, exploring how to partition RF/AFE, data conversion and edge processing across vibration, RF condition monitoring and low power sensing use cases, with a practical co design checklist.
industrial equipment communicating wirelessly
Maximizing multi-antenna performance in dense industrial deployment
By Avnet Staff   -   May 12, 2026
With multiple wireless channels becoming the norm rather than the exception, industrial IoT and smart building networks are like RF jungles. Here’s what engineers can do to mitigate the impact.

Related Events

Related Events
satellite in orbit
Space 2.0: AMD Technologies for New Space
Date: February 23, 2022
Location: Webinar

using-digital-twins-for-hardware-component-selection