Article

Stylish, powerful and ready for anything – our latest outdoor displays

Nishant Nishant
A row of digital signage on a pathway at night, with a person jogging in the distance.

Remember the world without outdoor displays? No, we’d rather not either. Painstakingly reading timetables at train stations? Seeing great offers on posters and discovering they’re out of date? Essential public information unreadable due to vandalism? No thanks.

By contrast, today’s outdoor displays are reliable, energy efficient and eye-catching. Stylish and durable, they can actually add to the look of the spaces they’re in. But, of course, there’s always room for improvement, which is why our new range of IP-Rated Outdoor Displays is an exciting development for us and our customers.

First off – horizontal or vertical, our new monitors are engineered to be ultra-slim and lightweight. The absence of bulky casing gives them a slick look that is ideal for outdoor menu boards and kiosks.

But don’t let ‘light and slim’ fool you because there is zero compromise in strength and reliability, and all our monitors exceed IP65-rated protection. This means that they are waterproof and weatherproof against sun, rain, snow and wind. Their advanced sealing also keeps dust out, so you only need to clean the exterior shell, minimizing maintenance.

Technical Specifications
Sizes 32”, 43”, 49”, 55”, 65”, 75”, 86”
Temperature Tolerance LCD area operates from -30°C to 90°C
UV Isolation 94% efficiency
Infrared Insulation Reduces heat buildup by 45%

But a great display is nothing without great visibility and this is where our new monitors truly deliver – even under direct sunlight. 4000 nits of brightness and IPS technology delivers clear images from nearly any angle, even though these are ultra-low power displays.

Of course, these displays aren’t exclusively for commercial environments. They are flexible and robust enough for industrial use, with a truly impressive temperature tolerance. As always, our designers and engineers are taking our display portfolio to the next level for the benefit of all our customers.

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact a Display Solutions Expert

About Author

Nishant Nishant
Stefano Rosato, Director, Technical Touch Technology, Avnet

Stefano Rosato is director of technical touch technology in the Display Solutions team at Avnet. Ste...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

 

Marketing Content Spots

Related Articles

Related Articles
Avnet display
Discover the multitool of modules that keeps everyone happy
By Stefano Rosato   -   July 6, 2026
Unprecedented is such an overused word, so it takes a lot for us to choose it when talking about products in our portfolio. However, we took an executive decision on this one, as we believe the TCXD050IBLON-173 5.0-inch TFT-LCD module deserves every  acco...
resistive keys
Performance under pressure: our new resistive keys are a touch different
By Stefano Rosato   -   June 1, 2026
In the industrial world, the capacitive touchscreen can be a sensitive soul. It performs beautifully under ideal conditions, but this is a luxury most industries can't afford.

Related Events

Related Events

No related events found

stylish-powerful-and-ready-for-anything-our-latest-outdoor-displays