Article

‘One and done’: The TFT display platform engineered to reduce time and costs

Nishant Nishant
TFT display

As you might have already figured, making things easier for our customers is something of an obsession for us. They come to us with a challenge, problem or just a really great idea and we do our very best to make it happen. Our latest TFT display is a great example – it needs no host processor, and developers can work directly to the display platform. Yes, it’s a self-contained intelligent system with display.

To make this possible, a powerful STM32 microcontroller with an integrated LCD-TFT Display Controller (LTDC) is built into the display itself, removing the need for an external CPU. This allows for application logic, graphical interfaces and I/O control to run directly on it. There are fewer components (so lower costs), development is quicker (getting your product to market faster) and the whole system is simpler.

And it’s been carefully designed with the demands of industrial and medical applications in mind, which becomes clear when you see the number of customization and connectivity options available:

  • Rich connectivity: With RS-485, RS-232 and dual CAN built in – plus expansion options for I²C, SPI, USB, and analogue GPIOs – it integrates smoothly into existing infrastructures.
  • Scalable display sizes: Ranging from 5.0” to 12.1”, with high performance driven by MCUs such as the STM32H7, so it fits easily into existing systems.
  • Advanced graphics capabilities: Using tools like TouchGFX, developers can rapidly build modern, responsive graphical user interfaces with ease.

For engineers, the removal of costly microprocessor units is just another layer of benefit on a solution which already delivers in a big way. It frees them to focus on application innovation over complex system integration. And the architecture of the display supports efficient rendering and data handling without continuous CPU involvement, so it’s well suited to applications that need high energy efficiency and real-time performance.

In short: It’s a platform that makes makes building responsive, good-looking interfaces a whole lot faster, cheaper and, most importantly, easier.

Our display solutions come in a range of form-factors, and our display experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact Us

About Author

Nishant Nishant
Stefano Rosato, Director, Technical Touch Technology, Avnet

Stefano Rosato is director of technical touch technology in the Display Solutions team at Avnet. Ste...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

Marketing Content Spots

Related Articles

Related Articles
tablet with a PCAP knob
Display on Display: a touch solution that’s instinctively precise and flexible
By Stefano Rosato   -   September 11, 2026
Touchscreens are indispensable to the modern world, but there are situations when we might need something a little more tactile.
Avnet display
Discover the multitool of modules that keeps everyone happy
By Stefano Rosato   -   July 6, 2026
Unprecedented is such an overused word, so it takes a lot for us to choose it when talking about products in our portfolio. However, we took an executive decision on this one, as we believe the TCXD050IBLON-173 5.0-inch TFT-LCD module deserves every  acco...

Related Events

Related Events

No related events found

one-and-done-the-tft-display-platform-engineered-to-reduce-time-and-costs