Article

Making the stack stick: bonding and DTCs

graphic of person
color palette

Like most things in life, displays change, evolve and, happily, improve. As classic displays and control elements are increasingly being replaced by modern display stacks (Display Touch Cover lens or DTC), naturally new processes will come into play to bond the cover glasses or DTCs into their housings.

As the word ‘stack’ might suggest, various parts of these displays are bonded together. Firstly, the cover glass is bonded over its entire surface with a touch sensor using a transparent adhesive. The cover glass touch unit is then bonded to the display module using the same method.

Either a damping or structural adhesive can be used for the subsequent bonding of the display stack into a frame or housing. Of course, we must add a brief caveat here, as the overall process depends on several factors: the application area, material, DTC design and construction requirements. Because bonding a display stack isn’t always as straightforward as it might seem and there are plenty of considerations and challenges to be taken into account at every stage.

For example, the bonds must be resistant to moisture, grease, chemicals and UV rays. Then, additionally, each material expands and contracts at different rates and the chosen adhesive must be able to compensate for this. This means that judgements must be made in the early stages to decide which kind of bonding is the most appropriate. Simply – it’s all about the pros and cons.

infographic of display touch cover lense layers

infographic of display touch cover lense layers

 
Double-sided tape bonding
Pros - ‘Easier’ bonding in the front frame
- Fast further processing of the assembly (DTC + front frame)
- Cost-effective solution
Cons - Visible gap between front frame and cover glass
- Dirt accumulation in the joint
 
Liquid Adhesive bonding
Pros - Gap between front frame and cover glass is filled, which contributes to better sealing
- Achievable protection class IP6X
- Ensures better stability between frame and DCT
Cons - The liquid adhesive takes longer to harden than the tape
- The further processing of the assembly takes longer
- High effort when dosing and positioning the parts
 

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

 

Contact a display solutions expert

About Author

graphic of person
Alexander Sommerfeld, Solution Manager Display Integration, Avnet Displays

After getting his diploma in mechatronics, Alexander entered the world of display solutions at MSC i...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

Marketing Content Spots

Related Articles

Related Articles
NFC
TFT + NFC = Simplicity: Our newest integrated technology
By Stefano Rosato   -   February 12, 2026
NFC technology began as a convenience-enabler. Now we expect to find it everywhere – even in displays. So, we’ve introduced TFT displays with fully integrated NFC antennas.
mid sized display
Mid-sized 12.1” display ready to rumble
By Frank Ploenissen   -   October 30, 2025
Extending the 12.1” display size offering, Avnet Displays adds another bright addition to the SimplePlus Touch Display family — combining trusted performance with an even broader choice for our customers.

Related Events

Related Events

No related events found

making-the-stack-stick-bonding-and-dtcs