Article

Leading-edge technology for power distribution in 12 V applications

 generic graphic of person
A transparent car showing the wiring loom and power distribution network
Auto-makers are moving to smart fuses to reduce power distribution complexity and increase system flexibility.

The industry is rethinking and redefining how power gets distributed in modern vehicles. There is a move away from old-school relays and melting fuses toward smart fuses that better support zonal architectures.

By switching to smart fuses, manufacturers cut down on wire harness weight, which means lighter cars and a direct bump in EV range, less charging and fewer emissions. Another thing to keep in mind is the real-time diagnostics and predictive maintenance these smart fuses bring to the table. It’s a leap in safety: not only do they prevent the classic “fuse blew, now what?” scenario, but they also keep drivers out of the loop for manual replacements.

Moving from a centralized body control module (BCM) to a zonal architecture makes the whole system more flexible and scalable. It’s easier for automakers to adapt to different models without re-engineering the wiring every time.

Through a business strategy lens, new smart fuses, pioneered by ST with its I2t programmable fuse devices, mean lower production costs, faster go-to-market and better alignment with sustainability goals. Smart fuse technology is a foundation for next-gen automotive platforms.

Let’s look at the prototyping side. ST has announced new evaluation boards: the STEVAL-PDUBV1 for primary (stage 1) system evaluation, and the AEK-POW-PDUMINI for satellite (stage 2) power distribution units. These come packaged with user manuals, GUIs, and are supported by AutoDevKit™ and SPC 5 Studio. These software kits require no license, so teams aren’t stuck waiting for IT approvals.

Taking a modular approach means development teams can mix and match microcontroller boards, rapidly prototyping without being locked into a single platform or board configuration. This flexibility makes it easier for teams to experiment and pivot if requirements change midstream.

The smart fuse features stand out, too. The I2t programmable curve lets engineers set precise current boundaries and trip times, protecting wire harnesses from overload. Reaction times are under 30 microseconds, which not only meets but exceeds regulatory demands for safety.

This software configurability lets OEMs use one design for multiple platforms. Plus, post-production changes, such as over-the-air updates, are also possible. That’s hugely significant for supporting new standards or unforeseen field issues.

 

Future-proofing zonal architectures

Now, stepping from prototyping into the real world. The newest parts to consider are shown in the table below.

Device STi²Fuse Family On resistance (RDSON) Current (nominal, programmable) Switching time (nominal, programmable) Current limit
VNF9D5SF Monolithic High-Side Drivers (HSDs) 2 x 5.9mΩ 4A to 15A 1s to 300s 75 A
VNF9D10SF Monolithic HSDs 2 x 10mΩ 2.5A to 10A 1s to 300s 67 A
VNF9Q20SF Monolithic HSDs 4 x 20mΩ 1.5A to 6A 1s to 300s 34 A
VNF9D1M5Q Hybrid HSDs 2x 1.5mΩ 8A to 27A 1s to 300s 120 A
VN9D1M2Q Hybrid HSDs 2x 1.2mΩ 10A to 33.5A 1s to 300s 145 A
VNF9D3Q Hybrid HSDs 2x 3mΩ 2A to 18A 1s to 300s 70 A

The list of main features is substantial. There’s the built-in self-test, capacitive charging mode to manage inrush current, and digital diagnostics with ADC integration. That means safer startup for high-capacitance loads and clearer fault isolation. Functional safety gets a boost, too, with direct input pin, emergency stop and diagnostics pin latch for microcontroller fault interrupts.   

Although both types of STi²Fuse devices offer enhanced functionality, Monolithic HSDs are tailored for low to moderate current scenarios, focusing on integrating multiple channels, programmable slope control, built in PWM engine, and providing accurate i²t protection suited for distributed automotive systems.

By comparison, Hybrid HSDs are designed for moderate to high current demands, featuring sturdy power stages, peak-current latch‑off, dedicated emergency stop circuits, and reverse-battery safeguarding to address safety‑critical operations and boost overall system reliability.

Using the ST L99SP08 alongside eFuse HSDs enables ultra‑low‑power Active Standby ON operation by supplying low‑current loads through integrated P‑channel FETs while keeping the main HSD off, significantly reducing system quiescent current in power distribution.  The device intelligently performs a fast self‑wake‑up, automatically enabling the HSD when load current exceeds the P‑channel capability, ensuring seamless power delivery without software intervention.  Highly accurate digital diagnostics and current sensing provide deep visibility into load behavior, improving system robustness and fault detection.  As part of the STi²Fuse family, the L99SP08 strengthens functional safety and is ISO 26262 ASIL‑B ready, making it ideal for safety‑critical automotive power architectures.

What matters here is that these new generations address technical gaps and are designed to reduce risk for both OEMs and their supply chains. Teams can focus on meeting regulatory targets, while the new hardware delivers better safety and operational reliability.

Now that we’ve mapped out the feature upgrades, let’s get practical. Where do these smart fuses make a difference in the field?

 

Smart fuse applications

The devices are relevant for everything from traditional power distribution to advanced battery management setups. That means high-current loads, relay and fuse replacement, and even parallel switch scenarios.

Transitioning to zonal power architectures

 

Smart fuses enable automakers to move from the classic power distribution model toward a smart power distribution architecture (Source: STMicroelectronics)

Automakers and system integrators have flexibility, whether they’re working on legacy platforms or next-gen EVs. But real innovation doesn’t just stop at product launch. Customer support and clear communication keep adoption on track.

Seeing where these smart fuses fit in real-world systems, the next question is often about positioning against discrete solutions. Weighing integrated e-fuse devices against piecing together discrete parts is where Avnet’s technical experts can dive deeper into a customer’s application before advising.

Smart fuses aren’t just the next step in automotive power distribution, they’re the foundation for lighter, safer and more adaptable vehicle platforms. With ST’s latest I²t programmable devices, OEMs can speed development, cut complexity and futureproof their zonal architectures. To explore how these solutions fit your next design, connect with Avnet’s technical team and turn smart fuse innovation into real world performance.

About Author

 generic graphic of person
Miguel Tapia, Transportation Supplier Corporate Account Manager

Miguel Tapia has over 25 years of experience in the semiconductor industry, currently serving as Avn...

Helpful Links

Marketing Content Spots

Related Articles

Related Articles
An electric scooter highlighting the critical electronic subsystems
Targeted solutions for e-mobility’s five critical subsystems
By Miguel Tapia   -   September 28, 2026
From efficient power conversion to connected rider experiences, bringing semiconductors, software, reference designs and system-level platforms together is accelerating e-mobility development.
A wireframe of an electric car showing the battery and key electrical components
How the EV drivetrain is moving toward function consolidation
By Miguel Tapia   -   September 23, 2026
EVs present new opportunities for function consolidation, delivering lower cost and weight, and simpler wiring. But the shift comes with challenges when combining power, control and safety in a single platform. NXP is leading the evolution.

Related Events

Related Events
airplane cockpit looking out on the runway
More Electrification in Aircraft
Date: October 11, 2022
Location: Virtual

leading-edge-technology-for-power-distribution-in-12-v-applications