Article

ePaper integration with PCAP

Nishant Nishant
person using a tablet

Electronic paper (also known as e-ink, electrophoretic display, or electronic ink) is a kind of electronic display that mimics the appearance of ink on paper. An electronic paper display reflects ambient light like paper, unlike conventional flat panel displays that emit light.

Lightweight and slim, ePaper displays offer high-resolution and no glare visibility, allowing users to view text and pictures at any angle, giving them paper-like readability – even outdoors and in bright sunlight, without the need for a backlight. This makes it the perfect choice for both indoor and outdoor displays, such as retail shelf labels, interactive museum signs, traffic signs, notice boards and passenger information boards.

But outside of usability, they are predominantly known for their durability, reliability, high data storage and low power consumption. It can hold static text and images for an indefinite time without the use of electricity and will continue to display content even in a power outage. This is because it doesn’t require power to display an image, only to change the content. Equally, the response time of ePaper displays is slower when switching between screens. This too makes them more suited to static image displays.

Their displays will use approximately 3 Ah for 2 seconds each time it updates its contents, giving full use of 36 mA or 12 mAh per day. Therefore, the display consumes only 0.008% of the power that a same-sized TFT LCD would require in a day and because there is no heat source, there is equally no heat dissipation. With the global focus on energy conservation, ePaper has a major advantage over traditional LCD screens and, as a result, the market demand is increasing.

Making ePaper smart

To make the ePaper smart, so that it can be used in ebooks, wearable electronics and others, it is necessary to add a PCAP.

The main challenge in optical bonding EPD and a PCAP is the very thin glass substrate. Excessive or uneven pressure applied during the bonding process can cause the glass to break. And the traditional liquid bonding may result in adhesive overflow, and the curing shrinkage of the adhesive can lead to Mura issues, irregularity or lack of uniformity.

To tackle these two pain points, we use solid OCA (silicone-based) for the optical bonding procedure. The pressure and debubbling pressure used in vacuum bonding are low, which, combined with our self-developed bonding fixtures, avoids excessive and uneven pressure. This also reduces the occurrence of stress-related Mura. To increase weather-resistance, we can incorporate anti-UV designs into the structure to prevent the LCD yellowing or cracking.

Smart ePaper displays are well suited to plenty of Smart City applications, as well as Public Information Displays, digital signage, electronic billboards and transportation vehicles, among others.

Value-added features of ePaper displays

We offer a variety of value-added features tailored to different applications, as well as customized integration services:

  • Ceramic printing on cover glass
  • Optional cover glass features: Anti-Glare (AG), Anti-Reflective (AR), Anti-Fingerprint (AF), and Anti-Virus coatings
  • Anti-UV design
  • Integration of a front light guide with light sensors and PWM dimming capability
  • Provision of ePaper driving boards, touch controllers, and backlight driving boards

Our PCAP technology is stable against noise, water, and humidity, thanks to the mutual differential technology and HW FFT to find the best low noise frequency.

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact a Display Solutions Expert

About Author

Nishant Nishant
Stefano Rosato, Director, Technical Touch Technology, Avnet

Stefano Rosato is director of technical touch technology in the Display Solutions team at Avnet. Ste...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

Marketing Content Spots

Related Articles

Related Articles
NFC
TFT + NFC = Simplicity: Our newest integrated technology
By Stefano Rosato   -   February 12, 2026
NFC technology began as a convenience-enabler. Now we expect to find it everywhere – even in displays. So, we’ve introduced TFT displays with fully integrated NFC antennas.
mid sized display
Mid-sized 12.1” display ready to rumble
By Frank Ploenissen   -   October 30, 2025
Extending the 12.1” display size offering, Avnet Displays adds another bright addition to the SimplePlus Touch Display family — combining trusted performance with an even broader choice for our customers.

Related Events

Related Events

No related events found

epaper-integration-with-pcap