Article

Electronic component selection for very low Earth orbit satellites

Avnet A Frame
Satellites in orbit around the earth
Very low earth orbit satellites provide an increasingly important role in modern communications and earth observation, creating opportunities for manufacturers.
KEY TAKEAWAYS:
  • VLEO is a demanding environment for electronics, with specific characteristics. It is not just a lower LEO variant
  • Classify each system function by mission criticality before selecting components and protection measures
  • Calculate qualification and derating parameters on mission-specific environmental data

Very Low Earth Orbit (VLEO) missions place stringent demands on electronics, requiring radiation-aware design, thermal robustness and contamination tolerance, both for dedicated VLEO satellites and for low‑altitude demonstrators in nearby LEO regimes. This parts-oriented guide connects environmental conditions to component selection, highlighting trade-offs between commercial off-the-shelf (COTS) and space-grade parts, along with appropriate qualification and derating strategies.

Low Earth orbit (LEO) typically spans altitudes from approximately 160 km to 2,000 km, but the lower portion of this band behaves differently from what is often treated as “standard” LEO. In the 180–400 km range, commonly described as very low Earth orbit (VLEO), residual atmosphere, drag and atomic oxygen become dominant design drivers. Electronics for satellites operating in this band must withstand a harsh, dynamically varying environment.

Height ranges of commercial, very low, and low Earth orbits

Infographic of height ranges of commercial, very low, and low Earth orbits

Relative heights of aircraft and low-earth-orbit satellites. While the specific figures vary, the consensus is that VLEO extends to around 400 km above sea level, before LEO takes over.

VLEO space environment for satellite electronics

From an electronics perspective, the radiation environment in VLEO is nuanced rather than benign. The total ionizing dose (TID) accumulated over a multi year mission is often lower than in higher LEO or medium Earth orbit because of increased geomagnetic shielding and shorter path lengths through the trapped particle belts. However, single event effects (SEEs) remain a significant concern. Trapped protons and heavy ions can induce single event upsets in digital logic and memory, triggering destructive latch up in power and mixed signal devices.

Radiation drives a design strategy tailored to the mission profile. A blanket approach in which all devices are radiation‑hardened is rarely economical for VLEO. Yet flying uncharacterized COTS devices at their data‑sheet limits also carries unacceptable risk. A more effective methodology is to model the mission radiation environment, estimate SEE rates for candidate components, characterize critical devices where data are lacking, and then decide where architectural mitigation (such as scrubbing, redundancy or watchdog‑based recovery) is sufficient and where radiation‑tolerant parts remain essential.

Thermally, VLEO missions are characterized by high cycle counts and significant temperature excursions. A circular orbit at a few hundred kilometers altitude has a period of roughly 90 minutes, and spacecraft typically experience one warm and one cold phase per orbit. Over a year, this results in thousands of temperature cycles. Seasonal effects, attitude changes, payload duty cycles and servicing maneuvers mean some structures and boards experience several tens of thousands of cycles over mission life.

The intensity of these cycles can be substantial. External surfaces balance direct solar input, albedo, Earth infrared and deep space, while internal assemblies are subjected to localized heating from transmitters, high‑power payloads or electric propulsion. Without careful thermal design, board‑level temperature swings of 40–80 °C between hot and cold states are realistic. Repeated excursions of this magnitude drive thermo‑mechanical fatigue in solder joints, underfills, vias, wire bonds and connectors. Coefficient‑of‑thermal‑expansion (CTE) mismatches between semiconductor packages, PCB laminates and mechanical supports become primary reliability concerns rather than secondary layout details.

Atomic oxygen (AO) is a defining feature of VLEO. At altitudes below roughly 300 km, the flux of energetic oxygen atoms is markedly higher than at the 500–700 km altitudes associated with many traditional LEO missions. AO reacts with numerous organic materials, eroding polymers and coatings, roughening surfaces and altering thermal‑control properties such as emissivity and absorptivity.

Although most electronics are housed within the spacecraft, AO exposure is not confined to external panels. Harnesses, multilayer insulation, antennas, radiators and apertures are directly exposed, and AO‑generated species can penetrate internal cavities through gaps and vent paths. In parallel, organic materials release gases trapped in the material (outgas), particularly early in life or during warm phases. In vacuum, outgassed molecules condense on cooler surfaces, forming thin films on optics, radiators and printed‑circuit assemblies. Depending on composition, these films can be insulating (affecting charging and optical performance) or slightly conductive (modifying leakage paths and noise characteristics).

Plasma conditions in VLEO differ from those at higher altitudes. Even if absolute surface potentials are modest, differential charging between illuminated and shadowed surfaces and between dissimilar materials can generate transient currents, particularly along long harness runs and into sensitive analog or RF circuits. During close‑proximity operations between multiple spacecraft, interactions between their plasma sheaths introduce additional pathways for unexpected transients.

Design philosophy for VLEO electronics

Given these conditions, an effective design philosophy for VLEO electronics rests on three elements.

The first is functional criticality classification. Not all functions are equally important to mission success or safety, so classifying electronics by the consequences of failure allows differentiated parts policies and margins, rather than a uniform and often inefficient approach.

The second element is selective use of COTS and space‑grade components. Space‑grade and radiation‑tolerant parts remain the default choice for safety‑critical and mission‑critical functions, but screened and appropriately mitigated COTS devices can be used in many other roles to gain performance and cost advantages.

The third element is quantified qualification and derating. Environment predictions for radiation, temperature extremes and cycles, atomic oxygen exposure and contamination are translated into explicit test levels and derating factors for devices, assemblies and subsystems so that margins are based on data rather than assumptions.

The next article in this series introduces a four‑class criticality model for organizing functions and parts policies across VLEO and LEO missions.

Qualification and testing of VLEO satellite electronics

Qualification involves converting orbital parameters, expected lifetime and maneuver profiles into total ionizing dose (TID) and single‑event effect (SEE) spectra, thermal ranges and cycle counts, AO fluxes and contamination risks. These envelopes are allocated to subsystems according to their physical location and operational role. A converter mounted near an external panel, for example, may be assigned higher thermal and AO exposure than a controller located deep within the structure.

Once candidate COTS devices are identified, a structured screening flow reduces risk:

  1. Data‑sheet screening and lot control. Selection is restricted to devices with at least industrial temperature ratings and sufficient margin between intended operating points and absolute maximum ratings. Lot traceability is established so that test results are directly applicable to flight builds.
  2. Total ionizing dose testing. Representative devices are subjected to step‑stress TID tests to at least twice the predicted mission dose, with functional and parametric monitoring during and after irradiation. Devices exhibiting abrupt degradation before the test limit are rejected or restricted to lower‑criticality applications.
  3. Single‑event characterization. For digital logic, memories and power devices, SEE testing is used to characterize upset and latch‑up behavior and to derive event‑rate estimates for the mission environment. These data inform the assignment of devices to criticality classes and determine the need for mitigation such as scrubbing or current limiting.
  4. Thermal‑vacuum and power‑cycling tests. Devices mounted on representative boards are cycled in thermal‑vacuum over a temperature range encompassing expected board temperatures, with at least 1.5–2X the expected number of mission cycles. Realistic power profiles, including cold starts, hot restarts and maximum‑load operation, are applied to reveal latent weaknesses.
  5. Failure analysis and design feedback. Any failures or suspicious parametric shifts are analyzed, and the findings are fed back into component selection, circuit protection and layout.

Board‑level testing verifies power integrity, signal integrity and the effectiveness of conformal coatings and AO‑protection measures under thermal and mechanical stress. Assembly‑level testing adds vibration, shock and extended thermal‑vacuum exposure to uncover harness issues, connector problems and mechanical‑thermal interactions.

System‑level testing exercises integrated hardware and software in scenarios that mirror expected operations: safe‑mode entry, power cycling during eclipses, thruster‑driven attitude changes and complex attitude or configuration changes.

Derating guidelines for VLEO satellite electronics

Derating provides a bridge between environment predictions, qualification data and operational constraints. By operating components below their absolute ratings, designers build margin against wear‑out mechanisms, manufacturing variability and uncertainties in environment modeling.

On the electrical side, typical starting points are:

  • Operating voltages between 50-80% of absolute maximum ratings, with Class‑A devices closer to the lower bound.
  • Average currents between 50-75% of device ratings, particularly for parts located in high‑temperature regions.
  • Junction temperatures limited to approximately 95–110 °C depending on device type and grade, even if data‑sheet limits are higher.
  • Capacitors in critical locations used at no more than 50-60 % of their rated voltage.
  • Resistors and other dissipative components sized to operate well below their power ratings in continuous service.

Environmental and mission parameters can also be derated. Designing subsystems to at least twice the predicted TID provides margin against variability in solar conditions. Qualifying hardware for 1.5-2X the expected number of thermal cycles reduces sensitivity to modeling uncertainties. Operational rules that restrict high‑stress activities, such as high‑power downlinks or complex attitude maneuvers, during periods of elevated environmental risk further reduce exposure.

Table 1: VLEO design summary

Aspect Typical VLEO servicing figure Design implication Preferred parts policy
Altitude and regime
  • 180–400 km circular
  • 90 min orbits
  • high drag
  • Frequent orbit maintenance
  • Strong atomic-oxygen exposure
  • Short intervals between eclipses
  • Lightweight structures
  • Atomic-oxygen resistant external materials
  • Thorough thermal cycling test on electronics
Radiation dose Often around 1–5 krad(Si) behind modest shielding over 3–5 years Modest total dose but non-trivial single-event effects from trapped particles
  • Space-grade or rad-tolerant parts for mission-critical functions
  • Screened COTS with single-event mitigation for other functions
Thermal cycling Thousands of day/night cycles
Local board-level temperature variations: 40–80°C
  • Solder joint fatigue
  • CTE-mismatch
  • Connector fretting
  • Use -40 to +105°C parts
  • Qualify for 1.5 to 2× mission cycles
  • Conservative junction temperature margins
Atomic oxygen and contamination Atomic-oxygen flux at <300 km significantly higher than at 500–700 km, so atomic oxygen can enter internal cavities
  • Erosion of polymers and coatings
  • Emissivity changes
  • Films on high-impedance circuits from AO-driven and outgassed species
  • AO-resistant or coated polymers
  • Low outgassing material selection
  • Conformal coatings and filtered feed-throughs matched to AO/UV exposure
Electrical derating
  • Voltage typically limited to 50–80% of absolute maximum
  • Current to 50–75%
  • Junction temperature to 95–110°C
Additional margin where COTS data are sparse or failure consequences are high
  • Tighter derating and more extensive test for mission-critical functions
  • Relaxed limits for non mission-critical hardware isolated from critical buses

Design criteria for VLEO

Very low Earth orbit missions expose electronics to a combination of modest total dose, significant single‑event activity, high thermal‑cycle counts and pronounced atomic‑oxygen and contamination effects. Treating all functions with a single parts policy is either unnecessarily conservative or insufficiently robust.

A more effective approach classifies functions by criticality, applies an appropriate mix of space‑grade and COTS components and underpins those choices with environment‑derived qualification and risk‑based derating. With this framework, designers can exploit modern terrestrial electronics while still meeting the reliability expectations of VLEO platforms.

In the second article of this series, we build on this foundation by proposing a four‑class criticality model and exploring how it supports VLEO business opportunities in Earth observation, communications and drag‑compensation research.

Read Part 2 in the series:  A 4-class model for space components

About Author

Avnet A Frame
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Marketing Content Spots

Related Articles

Related Articles
Two satellites orbit the earth, representing LEO and VLEO
A four-class criticality model for VLEO satellite electronics
By Avnet Staff   -   June 25, 2026
Very low Earth orbit (VLEO) missions create new business opportunities in Earth observation, communications and drag compensation research. A criticality scheme balances COTS and space grade components across VLEO and LEO platforms.
aircraft technical drawing
Beyond cost: Why supply chain trust will define defense & aerospace competitiveness by 2030
By Carolyn O'Connor   -   March 10, 2026
Geopolitical volatility, rare-earth materials constraints, complex compliance demands and escalating cybersecurity requirements are demanding innovation across the most established defense and aerospace supply chains.

Related Events

Related Events
airplane cockpit looking out on the runway
More Electrification in Aircraft
Date: October 11, 2022
Location: Virtual
satellite in orbit
Space 2.0: AMD Technologies for New Space
Date: February 23, 2022
Location: Webinar

electronic-component-selection-for-very-low-earth-orbit-satellites