Demonstrating the cross-vendor smart home experience
- Enable zero-touch onboarding of smart devices using AWS provisioning
- Multi-protocol device control
- Unified dashboards across third-party clouds
- Provide a customized and branded end-user experience
Smart home technology continues to evolve, but interconnectivity remains a known challenge. Diversity at the device level ripples upstream, all the way to the cloud platforms that control them. Bringing disparate ecosystems for lights, cameras, actuators, and sensors together has become an imperative.
AWS (Amazon Web Services) provides the building blocks to do that, allowing providers to develop solutions that remove these barriers to consolidation. Avnet has partnered with AWS to help extend that technology all the way to the edge and simplify interoperative connectivity between multiple smart home device manufacturers.
Avnet’s /IOTCONNECT™ integrates with AWS solutions and complements two key elements: AWS IoT Greengrass, and AWS IoT Device Client. The table below outlines these technologies and how they cooperate.
AWS IoT Greengrass
Type: Edge runtime
- Runs on capable edge devices (Linux or Windows)
- Connects to AWS IoT Core directly
- Main focus is local processing, offline operation, component and lifecycle management
- Experience is built by the smart device OEM or solution provider
AWS IoT Device Client
Type: Device-side helper app
- Runs on Linux devices
- Connects to AWS IoT Core directly
- Main focus is simplified access to Jobs, tunneling, and shadows
- Experience is built by the smart device OEM or solution provider
Avnet /IOTCONNECT, powered by AWS
Type: Solution acceleration platform
- Runs on SDK or on device; cloud services in Avnet-managed AWS tenant
- Leverages AWS IoT Core, AWS IoT Greengrass, AWS Lambda, and related AWS services
- Main focus is rapid solution delivery: onboarding, templates, OTA, dashboards, analytics, multitenant management tenant
- Avnet provides a pre-built operational UX (dashboards, rules, analytics) plus APIs to accelerate delivery
Each technology listed above provides specific functionality:
- AWS IoT Greengrass Core Software is an edge runtime for Linux-based devices. It provides a local MQTT broker, component framework for AWS Lambda containers and local functionality (such as machine learning inferencing) and synchronizes with AWS IoT Core.
- AWS IoT Device Client is a ready-to-go Linux application that connects with AWS IoT Core using secure tunneling. It can provide basic metering and fleet provisioning.
- Avnet /IOTCONNECT is a solution accelerator platform built on AWS services, including AWS IoT Core, AWS IoT Greengrass, and AWS Lambda. It adds dashboards and essential features including a rules engine, over-the-air (OTA) updating, lifecycle management, and analytics. By packaging common AWS IoT patterns into a repeatable, multi-tenant solution, OEMs can deploy without rebuilding dashboards, OTA flows, and lifecycle logic for every product line.
C2C (cloud-to-cloud) connects cloud platforms
More recently, AWS released Managed Integrations for AWS IoT Device Management, a software framework that simplifies controlling different smart home devices from multiple manufacturers. The objective was to extend the smart home environment to multiple providers without putting the burden of integration on the homeowner.
Managed Integrations can be used to automate device setup workflows and support interoperability across devices, regardless of the vendor or their connectivity protocol.
The cloud-to-cloud connector is a vital piece of the solution. It gives manufacturers a structure for accessing device controls through APIs (application programming interface). This establishes a connection between Managed Integrations and the vendors’ cloud, which can be passed along to /IOTCONNECT to create a single pane of glass for the end user.
At CES 2026, Avnet demonstrated how this works in practice, using its Smart Home Demonstration Case. The demonstration uses Managed Integrations, edge intelligence, and wireless connectivity. The control plane is /IOTCONNECT with AWS IoT Core as the messaging backbone, showing how multiple devices with their own on ramps converge into a single user experience.
The architecture of the demonstrator comprises:
- Managed Integrations for AWS IoT Device Management for cameras and smart lightbulbs
- AWS IoT Core deployed on edge hardware
- AWS IoT Greengrass
- AWS IoT Core for LoRaWAN sensors
The Avnet /IOTCONNECT Smart Home Demonstration Case

Devices in the Smart Home Demonstration Case include:
TP-Link Tapo cameras
(indoor and outdoor)
- Connected over WiFi through the Tapo cloud and to /IOTCONNECT via dedicated C2C connector
- Provided live video streaming on the /IOTCONNECT dashboard
- Commands include ON/OFF
Philips Hue Smart Light Bulbs
- Connected over Zigbee through Hue Bridge to Hue Cloud, then to /IOTCONNECT via dedicated C2C connector
- Commands include ON/OFF, brightness, cloud connection state
Door Sensor
- Connected over Zigbee to Home Assistant, then to /IOTCONNECT Bridge
Secure Smart Contact Sensor
- Connected over Zigbee to Home Assistant, then to /IOTCONNECT Bridge
- Telemetry includes battery voltage, firmware, Open/Closed and tamper
Outdoor Motion Sensor
- Connected over Zigbee to Home Assistant, then to /IOTCONNECT Bridge
- Telemetry includes battery, motion sensitivity, occupancy, temperature
Smart Temperature and Humidity Sensor
- Connected over Sub-1GHz to Tapo Hub, then WiFi to Tapo Cloud, to /IOTCONNECT using Home Assistant or C2C
- Telemetry includes humidity, temperature, signal level and cloud connection
Power Meter
- Connected over WiFi to Home Assistant, then to /IOTCONNECT Bridge
- Telemetry includes energy (kWh), firmware status
Smart Water Detector
- Connected over Sub-1GHz to Tapo Hub, then WiFi to Tapo Cloud, to Home Assistant and /IOTCONNECT Bridge
- Telemetry includes battery, leak alerts, moisture level, signal strength
Conclusion
The smart home experience should be seamless, allowing agentic-like control over connected devices. Reacting intelligently to changing and variable conditions should be the default mode of operation. That scenario is now closer thanks to AWS Managed Integration and /IOTCONNECT. Bringing the key pieces of technology together, as demonstrated by Avnet, provides a platform for greater integration and market adoption. /IOTCONNECT consumes Managed Integrations APIs and presents them in a unified dashboard, without needing to directly integrate each vendor cloud. If your company is considering integrating C2C connectors for smart home solutions, Avnet can help.