Article

A monitor with a three-in-one cable? Pure simplicity.

Nishant Nishant
USBC

There are two words guaranteed to make us sigh loudly: cable management. Now, don’t misunderstand us, we know the unique satisfaction of well managed cables, but that feeling is entirely derived from the knowledge that they often need a lot of wrangling.

Take monitors, for example. There are plenty of situations where having multiple cables attached to a monitor can be obstructive and problematic. On medical devices, where additional cables mean more cleaning to maintain high levels of hygiene. Or kiosks and Point of Sale systems, where a streamlined look and zero public obstruction is essential.

See? Cables matter. So much that our customers have been asking us for help.

And, of course, our design experts were all too happy to spring into action, doing what they do best, and have solved the cable conundrum with a new USB-C Monitor Series that is a single cable dream. In your traditional monitor setups, you would expect to have separate cables for power, touch functionality and a video data cable, such as an HDMI.

Our new USB-C Monitor Series needs only a single cable to handle all three.

The range covers display sizes from 10.1” to 21.5”, sizes we know to be popular in commercial, medical and industrial environments. And, because our team think of everything, the monitors also support VCP (Virtual Control Panel) commands over USB-C, so you can monitor and adjust brightness, contrast and color. Commands can be sent directly from the host device without needing physical buttons or complex control setups, allowing for easier configuration and remote adjustments.

Plus, the maximum cable length of three meters means that the monitor can easily be positioned further away from the host system, while maintaining signal integrity. This is ideal for industrial and commercial setups where the monitor and controlling system may not be directly next to each other.

It all comes down to one thing: simplification. Our new USB-C Monitor Series cuts through the complexity of traditional setups with a single cable, making these monitors perfect for today’s demanding industrial and commercial environments.

Avnet USB-C Monitors: Technical Features
High Brightness: 1000 cd/m² brightness makes them suitable for both indoor and outdoor use, even in environments with strong ambient light.
Durable: These displays can withstand harsh environments, making them perfect for industrial or rugged applications.
Capacitive Touch Technology: 10-point capacitive touch supports both finger and capacitive stylus interactions, this means precise and responsive user input across multiple applications.
OSD: On Screen Display Controls for quick adjustments, while the main controls can still be driven via USB-C commands for remote access.
Energy Efficient: Suitable for continuous operation in power-sensitive environments.

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact a display solutions expert

About Author

Nishant Nishant
Stefano Rosato, Director, Technical Touch Technology, Avnet

Stefano Rosato is director of technical touch technology in the Display Solutions team at Avnet. Ste...

Additional Information

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

Marketing Content Spots

Related Articles

Related Articles
TFT Displays
Not such a narrow margin: New TFT displays that are borderline genius
By Stefano Rosato   -   August 26, 2025
Our customers’ great tech needs space to shine, so we’ve introduced a new Narrow Border TFT solution in partnership with industry leader and global Tier 1 display manufacturer IVO.
development board and tablet with balloons on screen
Big, bright, built for engineers: New Display Kits for ST Discovery Boards
By Frank Ploenissen   -   June 30, 2025
Size does matter. At least it does when it comes to our new MIPI DSI displays. We’re upscaling your options with new 7” and 10.1” display kits, designed to fit seamlessly with STMicroelectronics’ STM32F769I and STM32H747I Discovery kits.

Related Events

Related Events

No related events found

a-monitor-with-a-three-in-one-cable-pure-simplicity