202608-when-motors-learn-to-think

202608-when-motors-learn-to-think

When Motors Learn to Think: Three Key Links Between Agentic AI and Industrial Control

Integration of Multiple Technologies Heralds a New Era in Smart Healthcare

At home, a robotic vacuum can navigate around a pair of slippers. But in a factory, what happens when an expensive servo motor begins to show signs of bearing wear? In most cases, the answer is: nothing. It keeps running until the problem becomes a failure. 

Traditional motor control is like a soldier that only follows commands. Even when bearing noise, abnormal temperature, or current harmonics begin to reveal early signs of trouble, the control system may not proactively understand what those signals mean. The issue is not unwillingness, but capability: its “brain” is usually built around deterministic PID control logic, without the ability to interpret context or make autonomous decisions. 

Bringing Agentic AI into embedded control architectures is emerging as an important trend that could reshape the underlying logic of industrial control. This is more than an upgrade to intelligent control. It adds decision-making, self-adjustment, and contextual awareness on top of real-time control, giving control systems a brain that can truly “think.” 

As a bridge between semiconductor manufacturers and industrial customers, Avnet is committed to turning this forward-looking concept into deployable system-level solutions, especially in response to the large-scale manufacturing upgrade needs across Asia Pacific. From chip selection and architecture design to model deployment, Avnet helps industrial customers build motor control platforms that can think. In practical terms, this transformation can be understood through three technical moves. 
 

From Rule-Driven to Goal-Driven: Beyond Commands, Toward Objectives 

Traditional control is largely rule-driven: IF temperature > 80°C, THEN reduce speed. Generative AI has made human-machine interaction more natural, but many applications remain reactive: if you do not ask, it does not act. 

The core difference of Agentic AI lies in autonomy. Instead of giving it a single instruction, the user gives it a goal, such as “maximize production-line efficiency while ensuring safety.” Agentic AI can break that goal into sub-tasks: continuously monitor sensor data, analyze vibration trends, predict remaining bearing life, determine whether preventive speed reduction is needed, generate a maintenance work order, and select an appropriate downtime window. 

The key is that Agentic AI does not need to take over the entire control system. It can manage only a defined subset, such as assisting with energy-efficiency optimization under normal operating conditions, while falling back to deterministic control when abnormalities occur. This model of limited autonomy is exactly the balance industrial environments need: smart enough to add value, but bounded enough to remain safe. 
 

Creating an “AI Budget” Inside Microsecond-Level Control Loops 

In responsive computing and control applications, AI inference faces a very practical constraint: AI needs CPU resources, and so does the motor control loop. When both compete for the computing power of the same MCU, this becomes one of the hardest engineering challenges for embedded AI. 

Take motor FOC, or field-oriented control, as an example. Each cycle requires intensive matrix multiply-accumulate operations such as Park and Clarke transforms, as well as complex trigonometric calculations for rotor angle estimation. If a conventional MCU relies mainly on software libraries to perform these calculations, CPU cycles are heavily consumed, leaving very limited “thinking space” for AI. 

Avnet partner Infineon’s PSoC™ Control C3 family offers one example of how this challenge can be addressed. Its built-in CORDIC accelerator speeds up angle calculation and trigonometric function generation, while DSP instructions accelerate matrix transformations. Together, these capabilities save CPU cycles and reserve more computing room for Agentic AI. 

The core logic is not to add a separate chip just for AI. Instead, it is to make deterministic control faster and more efficient inside the same MCU, then use the freed-up resources to support AI. 
 

Bringing Intelligent Control to Life: Slimming Large Models Down for the Chip 

Agentic AI typically relies on large language models, or LLMs, for reasoning and planning. Yet industrial MCUs usually have only a few hundred KB to 1 MB of memory. Fitting a multi-billion-parameter model into an MCU may sound unrealistic, but engineers are moving toward practical deployment through three approaches. 

First is weight quantization. By reducing model parameters from 32-bit floating point to 8-bit, memory requirements can be significantly reduced while keeping accuracy loss within an acceptable range. A more advanced approach uses mixed precision: higher precision is preserved for critical layers, while more aggressive quantization is applied to less critical layers. 

Second is the use of compact models. Lightweight models such as TinyLlama and SmolLM are designed for edge applications. Their parameter sizes are much smaller than those of large models, yet they can still deliver sufficient accuracy for specific industrial tasks. 

Third is edge-cloud collaborative inference. A local lightweight model can generate a preliminary result first. In most cases, local inference is sufficient for real-time decisions and does not require network connectivity. Only when a more complex scenario appears does the system call on a cloud-based large model for validation and refinement. 

With these three methods, mainstream industrial MCUs such as Arm Cortex-M33-based devices can potentially run a lightweight local loop of “sense, decide, and act.” Decisions can be completed at millisecond speed, without relying on the cloud, and the system can continue operating even when disconnected. 
 

Safety: The Boundary Intelligent Control Must Not Cross 

No matter how intelligent Agentic AI becomes, industrial control has one non-negotiable boundary: functional safety. In practice, a layered architecture is a more reasonable approach. The AI layer is responsible for “thinking”, including analysis, recommendations, and prediction. The deterministic control layer is responsible for “doing”, such as executing PID control and switching modes. The functional safety layer provides the final safeguard, including overcurrent protection and emergency shutdown. 

Infineon’s MOTIX™ TLE9954 family reflects this design philosophy. Its SiP package integrates a three-phase bridge driver, OptiMOS™ power devices, and an Arm® Cortex®-M core. It complies with ISO 26262 ASIL B functional safety requirements and includes an integrated current-sense amplifier and 12-bit ADC. In other words, the basic data Agentic AI needs for decision-making can be collected by the chip itself. 
 

Conclusion 

The journey from a motor that simply rotates to a motor that can think requires hardware accelerators to free up computing budget, model optimization techniques to compress large models into MCU-friendly forms, and functional safety architectures to protect the boundaries that cannot be compromised. 

This is the capability Avnet and partners such as Infineon are working to build together: aligning chip selection, architecture design, and model deployment so intelligent control can move from concept into real factory environments. When motors learn to think, every rotation becomes more meaningful. 

 

 

202608-when-motors-learn-to-think

202608-when-motors-learn-to-think

Related Articles
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
From Assistive Tool to Real-Time Collaborator: AI Ultrasound Ushers in a New Era of Edge Intelligence
November 1, 2026
As AI moves from cloud-based assistance to real-time participation at the edge, it is becoming genuinely embedded in clinical workflows and helping clinicians reduce cognitive burden.
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
When AI Clusters Reach 1.6T: Look Beyond GPUs - IP&E Is the Data Center’s “Hidden Bus”
October 1, 2026
Compute silicon defines the performance ceiling, but IP&E determines whether the system can remain stable under extreme load.

202608-when-motors-learn-to-think

Related Events
Avnet/ Renesas AI webinar
Date: July 15, 2020
Location: Webinar