传输与切换

A transmission and switching IC mainly finds applications in a telecommunication network. Transmission provides the transport of a signal from an end-user source to the destination such that the signal quality at the destination meets certain performance criteria and switching selects the route to the desired destination that the transmitted signal travels by the closing of switches either in the space domain or the time domain or some combination(s) of the two.

传输与切换 - 子类别

PHY

1

传输与切换 - 制造商