KIOXIA

KIOXIA, which officially started operating on October 1, 2019, after rebranding from Toshiba Memory, is a world leader in memory solutions, dedicated to the development, production and sale of flash memory and solid-state drives (SSDs). In April 2017, its predecessor Toshiba Memory was spun off from Toshiba Corporation, the company that invented NAND flash memory in 1987. KIOXIA is committed to uplifting the world with memory by offering products, services and systems that create choice for customers and memory-based value for society.
KIOXIA's innovative 3D flash memory technology, BiCS FLASH™, is shaping the future of storage in high-density applications, including advanced smartphones, PCs, SSDs, automotive and data centers.

产品类别

NAND flash memory solutions with integrated controller

KIOXIA offers NAND Flash Memories that integrate a controller in the same package. These NAND solutions provide ECC and other control functions, optimized by KIOXIA for each NAND technology generation.

A handshake between two robotic hands

Single Level Cell (SLC) NAND Flash Memory

KIOXIA‘s SLC NAND flash memory products offer wide line-up of capacity and package type. SLC NAND is adopted in a wide range of applications from consumer use to industrial use because of its high Read and Write speed and high reliability.

A handshake between two robotic hands