Custom Meta Tags

5G - hero banner

5G Solutions

5G solutions - main title

5Gの世界に向けた設計

5G intro - MM

これから2030年にかけて、5Gは世界最先端のセルラー技術として圧倒的な地位を築き、それを維持するでしょう。今後10年間にわたり、OEMは、より高速で広範囲かつ信頼性の高い接続需要に対応し続けるために、常に設計を刷新させ、繰り返さなければなりません。

今こそ、5Gの設計の道のりを加速させる時です。 5Gは、インフラからエンドポイントまで、企業および個人の生活のあらゆる側面に浸透するでしょう。 この道のりを加速化するために最も相応しい場所が、アヴネットの 5Gソリューション・ページです。

 

5G articles title - LC

5G関連記事

5G Articles Teaser

communication towers
The future of 5G RedCap powers device expansion
By Benjamin Alvarez   -   2024年8月6日
Market adoption of 5G wireless networks has been slower than expected outside smartphone applications. The Reduced Capability standard was introduced to accelerate 5G expansion in markets where interest has been limited.
記事を読む(英語)
cityscape with radio waves
How to evaluate 5G mmWave Phased Array Antenna Modules
By Steven Fireman   -   2024年5月29日
Faster 5G development requires hardware and software with proven compatibility, plus precision instruments and interconnects to ensure the stability and accuracy of test and simulation results.
記事を読む(英語)
Woman riding in self-driving car.
Bringing mm-wave beamforming to new applications
By Steven Fireman   -   2024年4月9日
With 5G rolling out and the help of phased array antennas, the 30 to 300 GHz, and specifically the millimeter-wave bands, of the RF spectrum are making their way into applications like autonomous driving.
記事を読む(英語)
An-image-showing-various-modules-from-3G-4G-and-5G-implying-5G-is-faster
What’s new in mmWave and 5G SoCs and modules?
By Avnet Staff   -   2023年8月24日
This article looks at recent developments in mmWave and 5G modules and systems-on-chips (SoCs), and the benefits they represent to product development teams working at both the board level and system level of design.
記事を読む(英語)
The Avnet RFSoC Gen 3 with the Phased Array Antenna Module (PAAM) from Fujikura
How modelling and simulation support mmWave design integration and delivery
2023年6月6日
5G mmWave system design is too complex to approach at a component level. Engineers need to take full advantage of software in all its forms to bring new solutions to market and provide full lifetime support.
記事を読む(英語)
electric vehicle dashboard
What is polarization, keying and color coding for interconnect?
By Jamie Pederson   -   2022年4月10日
Establishing a properly aligned connection quickly is key in any assembly or installation process. Polarization, keying and color coding are primary means to ensuring connections are made quickly and safely. In this article we’ll discuss each of
記事を読む(英語)
A graph of standing waves occur in transmission lines when there is an impedance mismatch.
The double edge of standing waves
By Philip Ling   -   2022年4月1日
A standing wave occurs when the reflected signal is in phase with the source. When it happens in a transmission line, it is normally unwanted because it results in emitted radiation. However, it is exactly that radiation that maximizes the signal’s streng...
記事を読む(英語)
person holding 5g device
How 5G will deliver more for less
2021年12月2日
From improved timing algorithms and sleep modes to the modernization of network hardware and new network protocols, 5G employs several power reduction strategies to manage network energy consumption.
記事を読む(英語)
digitally connected city
5G相互接続の設計上の課題とそのソリューション
2021年10月14日
次の高速セルラーネットワークの開発において銅配線が果たしている役割について、モレックスのハンセン氏に話を聞きました。
記事を読む(英語)

5G knowledge library - RRD

5Gナレッジ・ライブラリ

5Gがどのように状況を変化させ、設計においてどのように部品を選択すべきかに関して、Avnet Abacusのコンテンツライブラリを参照する。

詳細はこちら

ビームフォーミングの基礎(英語)

ビームフォーミングの基礎(英語)

フェーズドアレイシステムのビームフォーミング理論とザイリンクスZynq®UltraScale+™RFSoCでの実装について説明します。

ホワイトペーパーを読む

ウェビナーシリーズ(英語)

ウェビナーシリーズ(英語)

シングルチップ無線プラットフォームであるザイリンクスRFSoCを使用して、5Gの実用的な設計手法を学びます。

詳細はこちら