the-same-but-different-the-new-simpleplus-6-95-twins

the-same-but-different-the-new-simpleplus-6-95-twins

The same, but different: the new SimplePlus 6.95” twins

Nishant Nishant
A close-up shot of a rectangular black display with a dark gray screen, showing a thin black bezel and a visible orange ribbon cable on the bottom right, against a plain white background.

The SimplePlus family just keeps growing – and this time we’re welcoming twins! By popular demand, we’re introducing two new 6.95” touch displays which might look similar on the surface but, like all twins, have quite different personalities.

But first, let’s look at what they have in common. Touch functionality, of course, and a wide viewing angle, which is always welcome for its clear view of the display from many different positions. Ever reliable and flexible, both can operate in temperatures ranging from -30 to 80° Celsius. Their data connection is via a 24-bit LVDS interface, and both have their LED drivers on board. A regular coverlens with a black border print protects their touch sensor with USB interface.

So, how on earth do we tell them apart?

Well, in short, one display enjoys a shady spot and the other sings in the sun. In technical terms, this means that the first offers 500 nits TFT brightness – ideal for indoor environments where overhead lighting or bright ambient light is available. Think offices, retail, medical settings, factories and warehouses. It’s sibling, however, loves the great outdoors, offering 1200 nits of beautiful brightness which is perfect for anywhere there is intense or direct overhead lighting, such as outdoor kiosks, construction sites, dashboards and more.

As with all our SimplePlus touch displays, a plug-and-play display interface card is optional.

Product Code AMA-695A03-DU2511-G010
Size 6,95” wide (1024x600 pixel resolution)
Viewing Angle 170°/170°
Capacitive Touch? Yes
Coverglass 1.1 mm with decorative black border print
Brightness 500 cd/m² TFT, LED driving circuit on board
Interface LVDS
Contrast 1000:01:00
Operating Temperature -30° to +80°C
Compatibility ACC-THV65-AMA-695A03 Driving Board
Product Code AMA-695A04-DU2511-G010 (for outdoor applications)
Size 6,95” wide (1024x600 pixel resolution)
Viewing Angle 170°/170°
Capacitive Touch? Yes
Coverglass 1.1 mm with decorative black border print
Brightness 1200 cd/m² TFT, LED driving circuit on board
Interface LVDS
Contrast 1000:01:00
Operating Temperature -30° to +80°C
Compatibility ACC-THV65-AMA-695A03 Driving Board

Our Avnet Displays come in a range of form-factors and our display-experts are on hand to guide you in the creation of display or touch solutions that meet your requirements. Find out how Avnet Displays can propel your product innovation and get in touch today.

Contact a Display Solutions Expert

关于作者

Nishant Nishant
Frank Ploenissen

After getting his diploma in electrical engineering, Frank entered the world of display solution and...

附加信息

Avnet’s Displays team solves product design challenges for OEMs looking to build the perfect display technology into their products. Our in-house team works directly with businesses to solve all the challenges of integrating a display into a product design, from tiny wearables to massive outdoor screens. We design, build and deliver display solutions all over the world for established household brand names and industry disruptors alike.  If you need a display designed and integrated into your product, our team is here to help. Get in touch today to tell us about your challenge.

 

the-same-but-different-the-new-simpleplus-6-95-twins

the-same-but-different-the-new-simpleplus-6-95-twins

相关文章
Avnet display
Discover the multitool of modules that keeps everyone happy
By Stefano Rosato   -   2026年7月6日
Unprecedented is such an overused word, so it takes a lot for us to choose it when talking about products in our portfolio. However, we took an executive decision on this one, as we believe the TCXD050IBLON-173 5.0-inch TFT-LCD module deserves every  acco...
mid sized display
Mid-sized 12.1” display ready to rumble
By Frank Ploenissen   -   2025年10月30日
Extending the 12.1” display size offering, Avnet Displays adds another bright addition to the SimplePlus Touch Display family — combining trusted performance with an even broader choice for our customers.

the-same-but-different-the-new-simpleplus-6-95-twins

相关活动

未找到相关活动