the-future-of-5g-redcap-powers-device-expansion

the-future-of-5g-redcap-powers-device-expansion

The future of 5G RedCap powers device expansion

Benjamin Alvarez
communication towers

Powering the expansion of 5G devices

What's Next Magazine

Market adoption of 5G wireless networks has been slower than expected.

In fact, outside of the high-bandwidth applications around smartphones, 5G interest is still quite limited due to the high costs, limited coverage and lack of a need for some advanced features.

To accelerate the expansion of 5G into the industrial, medical, home and buildings, and security markets, 3GPP introduced the Reduced Capability (RedCap) standard in 2021. 3GPP stands for the 3rd Generation Partnership Project, which brings together seven telecom standards development organizations.

block diagram

5G relies on three main pillars all running inside the 5G Core: enhanced Mobile Broadband (eMBB), ultra-Reliable Low Latency Communication (uRLLC) and massive Machine Type Communication (mMTC). 5G RedCap addresses applications that fall between these extremes. (Source: 3GPP)

The move to 5G

5G RedCap, also known as 5G NR-Light or New Radio-Lite, is a lighter version of the 5G standard, bridging the gap between 4G and 5G. It targets use cases with minimum hardware requirements, where high data rate, ultra-low latency or even extremely low power are not critical, but there is a need for reasonable throughput.

A RedCap device is much simpler compared to baseline 5G devices defined by the 5G Release 15 standard. The silicon is less complex and, in the end, less expensive.

A RedCap device with the least complexity can work with a single receiving antenna rather than two, making for easier integration and lower cost. Some low-power features are also supported like radio resource management (RRM) relaxation (Micro Sleep State) and extended Discontinuous Reception Mode (eDRX). It will enable new cases including static objects, devices that are mainly uploading data to the cloud that will benefit from these power-saving modes.

Coming soon: Enhanced Reduced Capability (eRedCap), all the benefits of RedCap with a smaller throughput using the same 5G SA network.

Why should semiconductor manufacturers and OEMs pay attention?

RedCap and eRedCap technologies are the future generation of mid-end cellular IoT connectivity. They will replace respectively LTE Cat 4 in the coming years and LTE Cat 1 later. Industrial, medical and automotive markets are looking for longevity, so it’s still too early to discuss 4G sunset. But it is time to say that from a cellular network and chipset point of view, new evolutions on 4G are over.

RedCap increases the addressable 5G market because it solves the functional “middle ground” between high-performance 5G and low-end cellular communication like LTE-M and NB-IoT. Some use cases are already well known and covered by LTE; new ones are coming.

5G RedCap presents an exciting opportunity for OEMs and semiconductor manufacturers to innovate, diversify their product offerings, and contribute to the growing ecosystem of efficient IoT connectivity.

Market opportunities

5G RedCap technology addresses emerging market use cases that are not adequately served by existing advanced 5G standards: NB-IoT, Cat-M1 and of course 4G.

5G RedCap chipsets are already available and poised for growth. According to the some forecasts, 5G RedCap modules will constitute 18% of total cellular IoT module shipments by 2030, showing a significant market potential, particularly in developing nations where the cost is key to wide technology adoption for digital transformation.

Designed with a focus on mid-tier IoT devices such as gateways and industrial sensors, RedCap technology delivers reduced data flow and dependable connectivity while providing power consumption optimization, which provides a substantial extension in device battery life.

5G RedCap’s flexibility and network advantages, including lower latency, higher speeds and power optimizations compared to previous LTE generations, position it as a superior choice for future mass IoT deployment.

Benefits for IoT

5G RedCap offers several benefits for IoT applications, including:

  • HIGHER PEAK DATA RATE: 5G RedCap can support peak data rates three times higher than LTE Cat 4. This means that 5G RedCap can support applications that require more data throughput.
  • LOWER LATENCY: 5G RedCap offers comparable latency to existing 4G LTE technologies. This means that 5G RedCap can support applications that require near real-time data communication, such as industrial automation and smart grid applications.
  • IMPROVED POWER CONSUMPTION: 5G RedCap can help to improve the power efficiency of IoT devices, which can extend the battery life of these devices.

Use cases

  • Smart wearables (smart watch, low-end XR glasses)
  • Video surveillance
  • Medical devices, health monitors
  • High-end wireless
  • Utility/smart grid/industrial gateways

Conclusion

5G RedCap is a new 5G standard that is designed to address the use cases between the high-speed enhanced mobile broadband (eMBB), the ultra-reliable low latency communications (uRLLC) and the low throughput and battery efficient Massive Machine-Type Communication (mMTC) technologies.

5G RedCap is well-suited for a wide range of IoT applications and will play a significant role in future IoT deployments. For the time being, LTE Cat 1, LTE Cat 1 bis and Cat 4 are the most suitable for those IoT scenarios.

The first RedCap chipsets are available, offering the most advanced RedCap features and LTE fallback and they are not sold in similar quantities compared to LTE chips. RedCap modules are de facto a bit more expensive than traditional Cat 4 modules. As we discussed earlier, it will change in the coming years with the large availability of standalone 5G.

5G RedCap’s flexibility and network advantages, including lower latency, higher speeds and power optimizations compared to previous LTE generations, position it as a superior choice for future mass IoT deployment.

关于作者

Benjamin Alvarez
Benjamin Alvarez

Benjamin is a wireless connectivity and RF field applications engineer for EBV, an Avnet Company. Be...

Helpful Links

the-future-of-5g-redcap-powers-device-expansion

the-future-of-5g-redcap-powers-device-expansion

相关文章
5 men
Roundtable discussion: For today’s supply chain, it’s all about resilience
By Valeri Oliver   -   2025年12月9日
The modern supply chain is always evolving, whether due to geopolitical upheaval, natural disasters or other factors. Hear straight from three of Avnet’s supply chain experts about the latest trends in supply chain resilience, data mapping and more
cargo vessel moving through icy waters
Resilience by design: The supply chain’s new imperative
By Robert Cowan   -   2025年12月8日
The instinct to react quickly in a crisis is human. But in the supply chain world, speed without strategy can be futile. Use a counterintuitive approach: strategic patience. Sometimes the smartest move is to slow down.

the-future-of-5g-redcap-powers-device-expansion

相关活动

未找到相关活动