taking-a-sustainable-approach-to-making-sustainable-products

taking-a-sustainable-approach-to-making-sustainable-products

Taking a sustainable approach to making sustainable products

man
Office building
For a good example of sustainable manufacturing, look no further than Avnet Embedded’s new Eschbach, Germany factory.

What's Next Magazine

Sustainability is not just a buzz word. It is becoming more relevant and important for companies and for consumers. Companies are rated according to how sustainably they manufacture their products. Consumers are looking for products that are designed to be sustainable.

The raw materials used to make a product are important too. It matters how much the manufacturer leverages recycling and whether the materials they use come from sustainable sources. This is complicating supply chains, as it is hard and often expensive to locate and monitor the origin of all materials.

It matters how the goods are produced. Does the manufacturer use renewable energy? Do the processes used create air or water pollution during production? What kind of labor is used and what are the working conditions? The excessive use of resources, exploited labor and poor working conditions are clear red lines for sustainable production.

Indeed, as Avnet’s responsible value chain approach explains, the production cycle is long, convoluted and involves many partners.

Then there are various logistical considerations like transportation, packaging and distribution of the products, as well as how the product is disposed of at the end of its lifecycle. Whether the product is recyclable or it becomes waste defines how environmentally friendly a product is.

Another consideration is the amount of energy the product is designed to consume over its operational lifetime. Quality has a profound impact on sustainability. If the product is designed to be energy-efficient and have a long lifetime, its replacement will not be necessary for a long time.

E-waste is the fastest growing source of waste worldwide. The Circularity Gap Report 2023 suggests the global economy is now less circular than it was in 2020 and in 2018. View Report

What is green production?

When production happens close to the point of use, it has the potential to be greener. The time when manufacturing was outsourced to the region with the lowest cost seems to be coming to an end. There are several factors pointing to this.

Globalization is clearly returning to localization, partly due to tensions in the global economy. Artificial intelligence (AI) and automation are making production less labor intensive, reducing demand for a low-cost workforce. New manufacturing technologies are making it easier to mass customize products locally.

Factories that adopt a greener approach to production will also make greater use of solar and other renewable energy sources, like ground source heat pump systems. These factories have the potential to be net positive in terms of energy consumption. They will also be able to sell excess energy to the grid, which will benefit the local community.

The materials used to build these factories are selected to have a low environmental impact and where possible they will be recycled and recyclable. The carbon footprint will be neutral or even positive. This can be achieved by having plants growing on the roofs and around the factory.

When can you call a product sustainable?

A sustainable product is one that has a minimal impact on the environment. This ranges from the raw materials selected, the emissions generated during production, and the energy used throughout its operational lifetime. The raw materials selected should come from sources that conform to relevant sustainability standards. All the materials used should be recorded to provide traceability.

All products that use energy should be designed to consume the lowest possible energy. Products must also be designed for durability and longevity, so they can remain in service for as long as possible, even several decades. When the product is eventually retired it must be designed for recyclability. Recirculating products can create further value with minimal environmental impact. Designs based on a platform that allows upgradability of the product is also a good approach, as it can extend the product lifetime.

With more products now defined by software, it is also necessary to think about how software can improve sustainability. Updating software when the product is in service using over-the-air (OTA) update technology is now impacting product lifecycles and supporting sustainability.

manufacturing cell

Integrated circuits can potentially function as intended forever. In practice, operating conditions, manufacturing flaws and exposure to natural elements will degrade an IC and may cause it to malfunction.

A factory for the future

For a good example of sustainable manufacturing, we need look no further than our own Avnet Embedded. Avnet is currently building a new factory that will be carbon-neutral, in the heart of Europe. Located in Eschbach, Germany, the new facility will replace an existing building and offer a three-fold increase in manufacturing capacity but with a much lower environmental impact.

Like the existing factory, the new facility will be located close to many of Avnet Embedded’s customers, reducing the impact of transporting finished products. Photovoltaic panels fitted to the roof will make good use of solar energy to power the factory. It will also be equipped with a heating/cooling system that draws energy from the ground. The factory will only use materials and machines that are recyclable and from sustainable sources. It will have plants on the roof as well around the factory. These efforts ensure it will be far more sustainable than the old factory even with a higher manufacturing capacity.

Avnet Embedded’s compute modules are a good example of sustainable products. They are designed using sustainable materials which are recyclable. Energy efficiency is core to product design. Avnet Embedded’s production facilities, where its compute modules are manufactured, are highly automated.

warehouse

What’s next for sustainable product design?

Component selection is fundamental to lowering active energy. More of Avnet’s global suppliers appreciate this and are developing technologies that support ultra-low power operation. This includes microprocessors and microcontrollers. Power semiconductors that have lower switching losses are becoming more affordable, meaning they can be used to replace less efficient power solutions.

Avnet’s FAEs are helping OEMs optimize their designs for sustainability. If you need advice or design guidance, contact your Avnet representative today.

关于作者

man
Tiitus Aho

With a career spanning 25 years in the embedded computing and display market, Tiitus Aho is one of t...

taking-a-sustainable-approach-to-making-sustainable-products

taking-a-sustainable-approach-to-making-sustainable-products

相关文章
industrial equipment communicating wirelessly
Maximizing multi-antenna performance in dense industrial deployment
By Avnet Staff   -   2026年5月12日
With multiple wireless channels becoming the norm rather than the exception, industrial IoT and smart building networks are like RF jungles. Here’s what engineers can do to mitigate the impact.
electric cars charging with wind turbines in distance
Wide bandgap continues to disrupt
By Philip Ling   -   2025年12月15日
The supply chain for wide bandgap (WBG) solutions is now maturing, which means we’re seeing consolidation, acquisition and even some attrition. This turbulence is both predictable and surmountable.

taking-a-sustainable-approach-to-making-sustainable-products

相关活动

未找到相关活动