behind-the-datasheet-vision-systems

behind-the-datasheet-vision-systems

Behind the Datasheet: Vision systems

Philip Ling
documents

Image sensors are highly integrated devices, often with multiple operating modes and configuration parameters. Far from being a drop-in device, they need to be carefully integrated into the hardware, and require strong support from the system’s embedded software.

As with all system-level components, there needs to be a robust and flexible interface between the hardware and the software. This typically means using a driver: a software component that acts as the counterpart to the hardware element. The driver provides the system’s software a way to access the features of the hardware component. As such, drivers are often specific to a particular component, at least at some level.

Generic drivers can be used, and these do provide a good starting point for developers, particularly if the hardware component uses industry-standard interfaces. Drivers are often — not always — developed and provided by the hardware component manufacturer. To compound the issue, drivers are also normally specific to the operating system being used (if any).

One of the reasons why Linux is now so popular is because it comes with a lot of drivers. The community is also very good at developing and sharing drivers. Periodically, stable drivers may be integrated into the latest Linux distribution. If a Linux driver exists for the hardware component, it can save the engineering team a lot of time and effort.

This isn’t always obvious to developers when they begin the process of selecting an image sensor for their embedded vision application.

In this interview, Avnet Technical Marketing Engineer Mario Bergeron explains what engineers need to think about both before and after selecting an image sensor.

關於作者

Philip Ling
Philip Ling

Philip Ling is a Technical Content Manager with Avnet. He holds a post-graduate diploma in Advanced ...

behind-the-datasheet-vision-systems

behind-the-datasheet-vision-systems

相關文章
electric cars charging with wind turbines in distance
Wide bandgap continues to disrupt
By Philip Ling   -   2025年12月15日
The supply chain for wide bandgap (WBG) solutions is now maturing, which means we’re seeing consolidation, acquisition and even some attrition. This turbulence is both predictable and surmountable.
two young men and two young woman working with computers
New insights into design practices using development kits
By Philip Ling   -   2025年12月11日
Development kits offer a fast and affordable way for engineers to explore new technologies and for managers to assess project viability. Discover how to select the ideal kit for your project.

behind-the-datasheet-vision-systems

相關活動

未找到相關活動