The Hidden Factor Limiting Edge AI Performance: Why the Analog Front End Matters
When industrial equipment predicts failures through vibration sensors, smartwatches monitor health through electrocardiogram (ECG) signals, or security cameras detect anomalies through sound recognition, most people credit these breakthroughs to increasingly powerful AI algorithms and digital processors. However, an often-overlooked fact is that all real-world signals—vision, sound, vibration, temperature, and bioelectric signals—are inherently analog in nature. The bridge between the physical world and the digital brain—the Analog Front End (AFE)—plays a vital role in determining the quality of the data fed into AI models, ultimately influencing system accuracy, reliability, and decision-making performance.
As edge AI moves from proof-of-concept deployments to large-scale implementation, AFE design is facing unprecedented challenges. In applications where power consumption, silicon area, latency, and feature extraction efficiency are tightly constrained, traditional data-acquisition-centric design approaches are no longer sufficient. Optimizing the analog front end for AI-driven workloads is rapidly becoming a key area of innovation.
New Design Considerations for AI-Optimized AFEs
Traditional AFEs are designed to produce clean, well-conditioned digital signals. However, in machine learning applications, subtle variations that were previously considered noise may actually contain valuable indicators of equipment failures, health conditions, or environmental changes. As a result, engineers must rethink conventional design practices and balance signal conditioning with the need to preserve AI-relevant information.
Preserve Signal Features by Avoiding Over-Filtering
AI models interpret data differently from traditional digital signal processing systems. Aggressive low-pass or high-pass filtering may generate signals that are easier for humans to analyze but may inadvertently remove subtle features that are valuable for AI inference. Whenever possible, preserving the original signal characteristics and performing filtering later in the digital domain can help maintain flexibility for both AI processing and other downstream applications.
Minimize Distortion and Track Gain Changes
Introducing artificial signal artifacts during data collection can negatively impact model training and inference accuracy. For wide dynamic-range signals, automatic gain control (AGC) can help optimize signal quality. However, gain adjustments should also be communicated to the digital processing chain and synchronized with sensor data so that they can be properly incorporated during model training and analysis.
Ensure Precise Timing Synchronization
Multi-sensor AI systems rely heavily on accurate timing relationships between signal sources. Variations in filter depth, signal paths, or digitization latency can introduce group delay differences that alter the relationships among signals. These timing discrepancies can significantly degrade the performance of multimodal AI models.
Adopt Hierarchical Architectures to Improve Energy Efficiency
Edge devices frequently operate in ultra-low-power, always-on modes. In many cases, low-precision signal acquisition can be used to detect potential events while the AI accelerator remains inactive. Only when specific thresholds are exceeded does the system activate higher-precision data acquisition and AI processing. Additional nano-watt-level monitoring circuits can further reduce overall energy consumption by minimizing the time that full AI subsystems remain active.
Support Multiple Data Paths for Different Use Cases
As applications transition from IoT to AIoT, sensor data often serves dual purposes: enabling traditional data analytics while simultaneously feeding AI models in real time. Establishing dedicated data paths for different workloads can help prevent conflicts and ensure optimal performance across both functions.
From Components to Complete Solutions
Addressing these challenges requires more than selecting individual high-performance components. Modern AFE designs must operate reliably across multiple voltage domains, support diverse sensor interfaces, and deliver high levels of integration and robustness. Success depends on creating optimized end-to-end signal chain solutions rather than focusing solely on individual device specifications. Such complexity places greater demands on engineering teams as well as on technology partners capable of providing broad product portfolios and extensive technical expertise.
As a leading global technology distributor and solutions provider, Avnet helps engineers address these challenges through its extensive supply chain network and technical resources. Avnet offers nearly 1,800 analog switches and multiplexers from 13 leading suppliers, enabling customers to quickly identify the right components for both development and production while reducing design risks and supply chain challenges.
Learn More
To explore Avnet's Analog Switches and Multiplexers portfolio, scan the QR code or visit:

Analog Switches & Multiplexers
View Product Portfolio
Avnet and onsemi: Building a Reliable Foundation for Edge AI
Avnet's long-standing partner onsemi offers a comprehensive portfolio of logic and signal-management solutions that support the development of highly reliable AFEs. In multi-sensor systems, onsemi's analog switches and multiplexers feature low on-resistance, high bandwidth, and low crosstalk, helping maintain signal integrity during channel switching.
In addition, onsemi provides extremely compact packaging solutions as small as 0.62 mm × 0.32 mm², making them ideal for space-constrained applications such as wearable devices. These products help engineers simplify designs, reduce component counts, improve system reliability, and support the stringent signal integrity requirements of edge AI applications.

Conclusion
As semiconductor technology continues to advance, improving edge AI performance is no longer solely a matter of increasing compute capability. Instead, success depends on optimizing the entire signal chain—from sensing and data acquisition to processing and execution. The Analog Front End (AFE), as the critical interface between the physical and digital worlds, is becoming increasingly important. By establishing a strong foundation for signal processing at the source, engineers can provide AI systems with higher-quality data, enabling more reliable, intelligent, and impactful applications across industries.