IoT Security: Real Problems and Solutions

IoT Security: Real Problems and Solutions

IoT Security: Real Problems and Solutions

Guillaume Crinon Headshot
diagram of smartphone and connected devices

Introduction

“IoT security” is a popular topic these days, and there is not a single week without a conference featuring a paper or a keynote about security, without an announcement from hardware or software companies introducing new solutions and without an article in the specialized press. Avnet Silica would certainly not miss such an opportunity to participate in the discussion.

This paper aims at defining the real issues behind “IoT security”, the real challenges for our customers both from hardware and embedded / server software aspects and of course solutions as we envision them for the next 6 to 8 years, until our world becomes all IPv6 and 6LoWPAN.

We could start like many others, explaining how connected devices are at risk, how hackers can ruin business-models and how much everyone should look into cryptography. We will not.

Surprisingly or not, the main problem our customers face is the cost of personalizing the devices they manufacture with unique IDs, MAC addresses, keys and certificates, either on the production line or during field deployment. Surprisingly or not, technical solutions for personalization very often provide an additional toolset enabling the highest level of security at no additional cost.

We will demonstrate how the security architecture of the Internet of Things should leverage the security architecture of the Internet as we have been building it for more than 20 years. We will explain the challenges of properly provisioning and securing low-power non IPv6 connected sensors and devices.

In the past 15 years, enterprise Information Technology (IT) architects have successfully upgraded their security schemes from an all-wired world based on desktop computers to all-wireless-mobile laptop and smartphone fleets without compromising on security and even improving it. A similar evolution is happening now: beyond laptops and smartphones, industries are looking to connect many devices, machines and objects to application servers through private and public networks, as shown here.

What needs to be solved

The cost of personalizing connected devices

Regardless of the application and the security scheme associated with it, there is always a point in the life of a device connecting to another or to a distant server when someone needs to program unique identifiers and secret keys into a memory.

This process is called personalization. This is a hurdle, often a burden and always a cost in the manufacturing process or for the end-user.

Let us take a straight-forward example: adding a WiFi printer to a home network. At some point, you will need to associate manually the printer with the router so that they can share the same pass-key. Whether you do it manually, via NFC, or with a USB cable, the printer needs to know the secret key. In this case, the burden is not supported by the printer manufacturer but by you, the end-user.

The same thing applies in the business world but on a larger scale. One example from building automation is an alarm-system. This comprises a central unit and several peripherals communicating locally via an RF protocol, and may be sold individually or bundled. Someone, whether the manufacturer, the installer, or the end-user in DIY mode needs to “pair” or “associate” the peripherals with the central unit, and then register the central unit with the global surveillance service.

In all these cases, someone has to bear the cost of going through these personalization and pairing processes, either the manufacturer of the device, the service provider or the end-user himself at the expense of a true out-of-the-box experience.

The complexity of these processes often makes them a weakness in the security of such networks. How often do you renew your home WiFi pass-key? Probably never because it is too much of a hassle. How often are secret AES keys renewed in many systems? Not often and possibly never for exactly the same reason.

Networking and security: the importance of “end-to-end”

Link and network security are being addressed by every single communication and networking technology at different levels of the protocol stacks such as IPsec for IP, WPA for 802.11, 802.15.4, Bluetooth, and so on. However they should not be mistaken for end-to-end application security.

Indeed, having a WPA-secured WiFi connection to a local router is definitely not sufficient to “http” privately into a distant server, bearing in mind that most local network keys are hardly ever renewed for the reason explained above.

As illustrated below, it is fairly common that the data generated by a sensor or a machine will be conveyed through many different networks of different sorts belonging to a variety of service providers before reaching the targeted application server:

Each leg is only responsible for its own security, and is unaware of the legs behind or in front of it. As a consequence, the data has to be decrypted and re-encrypted within each gateway, from one leg to the next. It is often said that the security level of a whole system is defined by its weakest link. Therefore the need to trust several connectivity providers as well as the gateway manufacturers interconnecting them is clearly a weakness.

If the data are carried over IP all the way, there is an option of “tunneling” from the sensor to the application server. However this is the only possibility that comes close to “end-to-end” security in this scheme.

The solution is an extra level of end-to-end device-to-server security taking care of:

  • Device authentication to server
  • Server authentication to device
  • Secure session key establishment
  • Data integrity
  • Data confidentiality if needed

Solutions

End-to-end security in the IP world

SSL (Secure Socket Layer)
It is now more than 20 years since Netscape released in 1995 the initial public version of SSL (numbered 2.0 as 1.0 was never released because of flaws).

The idea was simple: how could Internet clients communicate securely and privately end-to-end with applicative remote servers delivering email, banking, e-commerce services through the public Internet regardless of their HW/SW platform and OS (Operating System)?

“Securely and privately end-to-end” meant the client being able to authenticate the server, not exposing passwords and confidential information to any third party including Internet Service Providers (ISP’s) and Telecom Operators. It also had to keep eavesdroppers and hackers at bay.

The easiest answer to this problem was to use the same unique secret key on both sides of the communication channel.

The main problem then became: how to distribute this unique secret key without exposing it?

Using an alternate channel could be a solution: After all, banks send us Visa/Mastercard PIN codes in a separate mail, and some websites use our email account to send us a provisional password when registering for a new service or requesting a password reset. Nevertheless, this was no lightning-fast process and certainly not practical for renewing session keys on a regular basis in a seamless and user-transparent way.

The real breakthrough came from the use of asymmetric cryptography.

This technology involved a fundamental transaction invented 20 years previously between 1973 and 1977 by asymmetric cryptography pioneers Clifford Cocks, Whitfield Diffie, Martin Hellman, Ron Rivest, Adi Shamir and Leonard Adleman. Theyhad devised methods for computing a unique shared secret key between two entities communicating over a public channel without exposing any secret information. Simply brilliant! Any acronym bearing RSA (Rivest, Shamir, Adleman) or DH (Diffie-Hellman) refers to these mathematicians. Since Cocks was working for the British secret services, his work and name were kept secret until recently, but he nonetheless deserves the recognition.

Asymmetric cryptography (RSA, ECC) being powerful but requiring much more processing power to encrypt and decrypt data compared with symmetric algorithms (DES, AES), it was therefore not very efficient to use it to encrypt and decrypt every single packet exchanged over the internet. For this reason, its use has been mostly restricted to the exchange and computation of symmetric session keys used to encrypt and decrypt the streams of data exchanged over the Internet.

Back in 1995, it was therefore possible for a client to securely authenticate a server and compute a shared secret session key used to exchange data:

Need for certificates

As is illustrated here, servers do not send their public key as is; they send certificates embedding their public key.

Why not sending a public key directly?

Because the client needs to be able to differentiate the genuine web site it wants to connect to from a fake one. How to differentiate between www.mybank.com and www.my-bank.com if the latter one wants to impersonate the real bank in order to capture account credentials?

Both will have a public key, but the client needs to check which one corresponds to www.mybank.com

In order to do this, the world relies on Certificate Authorities (CA) who are trusted independent corporations issuing digital certificates that certify the ownership of a public key by the entity named in the certificate.

Let us assume that www.mybank.com wants to issue a public key. Mybank will first send it to a Certificate Authority (CA) along with its credentials and proof of its identity. The CA will check that www.mybank.com is the owner of the public key and issues a digital certificate (complying with the X.509 standard) comprising [www.mybank.com ‘s public key, the name of mybank.com and its other credentials, validity dates] signed with CA’s private key.

This digital certificate will then be sent back to www.mybank.com who will share it with web clients requesting a connection.

Upon reception, the client will check the signature of the certificate using the CA public key (which is usually preloaded into the web-browser). In this way thus authenticate the certificate and therefore trust that the public key inside the certificate belongs to www.mybank.com which is the website it is asking to connect to.

In spite of many ongoing reflections on ways to improve the system, this architecture is the one currently securing the Internet:

TLS (Transport Layer Security)

After a few flaws and weaknesses discovered in SSL2.0 and SSL3.0, SSL has evolved to TLS1.x based on improved algorithms for signing, authenticating and encrypting which will not be detailed here.

In particular Elliptic Curve Cryptography (ECC) often replaces RSA, as it provides much shorter keys and less calculation complexity along with a higher level of security.

Embedded sensors and IPv6

Whereas the tremendous growth in the expected number of Internet-connected devices has led to migrate the addressing space from 32-bit in IPv4 (4.3B unique addresses) to 128-bit in IPv6 (3.4x1038 unique addresses!), the billions of sensors and devices being deployed are not yet natively IP-compliant.

Indeed, most of these devices are likely to communicate wirelessly and in many cases to run on batteries without maintenance for 5 to 15 years depending on the use cases.

Although a few IP-friendly wireless technologies such as 802.11 and cellular 3G/4G have been around for years they still fail the battery life test.

Instead, battery-friendly wireless technologies tend to favor small payloads, extended sleep time, asynchronous behavior and asymmetric communication, very often connecting to gateways with LAN (Local Area Network) connectivity such as Bluetooth, ZigBee, WmBUS, Z-Wave, Enocean, KNX, ioHomeControl, 802.15.4 or more recently without gateways with LPWAN (Low-Power Wide Area Network) technologies such as SIGFOX, LoRaWAN, NB-IoT to name a few.

Although recent implementations of 6LoWPAN (low-power wireless IPv6) have emerged such as Thread and Bluetooth 4.2, it is expected that a vast quantity of sensors and devices that will be deployed under the IoT banner will actually NOT be IP-friendly until 2025 at least for reasons of backward compatibility and legacy with existing products.

This means that these billions of devices, from smart meters to industrial sensors will not be able to use the Internet Protocol standard to establish a TLS session with the server they will be connecting with.

End-to-end security outside the IPv6 world

Is this the end of our story? Certainly not!

We are looking for a way to implement this green layer of end-to-end security that sits on top of the other security legs:

We have at least one leg which is not IP, probably low power, low data rate acting as a bottleneck on the whole path (remember if we are IP all the way, go to the previous paragraph, problem solved).

There is a simple answer: if genuine IP TLS is too heavy with too much overhead for this bottleneck, let us tailor a derivative of TLS bearing:

  • Cryptography algorithms with shorter keys (ECC) rather than longer ones (RSA)
  • Smaller certificates
  • Extended session key validity
  • A simple capability for a sensor to check a server certificate off-line if needed
  • A secure and cheap way to personalize and store certificates together with session keys in the sensor or device
  • Certificate Authority services enabling the issuance and checking of custom certificates

This TLS derivative should perform the same functions as the real TLS:

  • Mutual authentication
  • Very simple and automated provisioning of a sensor/device into a distant application
  • Mechanisms for revocation of a sensor/device from a distant application
  • Secure AES session key derivation and secure exchange
  • yielding message integrity and encryption

Secure elements

Although many MCUs boast low-power cryptographic engines, they miss the real problems:

  • Someone still needs to personalize them at some point, and this has a cost
  • They are not secure and secret keys can be read from their memory or computed from dynamic supply currents or even from their electro-magnetic emissions.

This is the reason why Visa and SIM card chips are not standard Cortex-M3 hardware.

This is the reason why such things as secure elements are useful.

Secure elements are tiny components connecting as peripherals to host MCUs/MPUs and featuring:

  • Personalized certificates
  • Secure hosting of secret keys
  • Handling of cryptography primitives

In short, they are part of the solution together with secure personalization logistics.

Bottom line: personalizing a connected device
Our initial problem was lowering the cost and the burden of personalizing and provisioning connected devices, sensors, machines to local or remote servers. By regrouping the technologies mentioned above, we now have a full set of solutions:

  • TLS or TLS-like stacks and APIs capable of mutual authentication, distribution and renewal of session keys
  • Secure elements able to host certificates and handle TLS primitive functions
  • Secure logistics in order to personalize secure elements before device manufacturing eliminating the need to personalize the device itself
  • Trusted Certificate Authority services for issuing and checking custom certificates during the 15-year life of the connected product

Gateway

A gateway typically bridges between a Local Area Network (LAN) and the application server through the Internet (IP network). It therefore needs to securely authenticate to the server and securely authenticate the server it is connecting with.

Since the link between the gateway and the server is IP-based, this can be handled with a TLS protocol over any IP connection, whether WiFi, Ethernet or 3G/4G.

A recommended implementation will be our Avnet-Silica-personalized secure element as a companion chip to the main processor running our UbiquiOS stack in the gateway seamlessly handling the TLS with the server running our APIs and performing the task of provisioning the gateway with HTTPS or MQTTS.

IP or 6LoWPAN sensor

As seen above, sensors are often battery-operated and need to operate light stacks. 6LoWPAN is the low-power version of IPv6, typically used by the Thread™ networking protocol. In this case, it will be possible to establish a TLS directly between the sensor and the server as explained earlier.

A recommended implementation will be our Avnet-Silica-personalized secure element as a companion chip to the sensor microcontroller running our UbiquiOS stack seamlessly handling the TLS through a provisioned gateway with the server running our APIs and performing the task of provisioning the sensor securely with HTTPS or MQTTS.

Non IP sensor

If the sensor is neither IP nor 6LoWPAN-based, it will be necessary to establish a TLS derivative tailored to the local networking technology directly between the sensor and the server.

A recommended implementation will be our Avnet-Silica personalized secure element as a companion chip to the sensor microcontroller running our UbiquiOS stack seamlessly handling Avnet Silica’s proposed TLS derivative through a provisioned gateway with the server running our APIs and performing the task of provisioning the sensor with the best balance of security and power consumption in accordance with the mechanisms in use with HTTPS and MQTTS.

Conclusion

Avnet and its partners enable customers to benefit from their depth and breadth of expertise in addressing personalization and security schemes for IoT projects.

The company represents several secure element manufacturers, including Infineon, ST Micro, NXP, Maxim, Microchip/Atmel and Morpho/Trusted Objects.

Avnet is also currently developing its own stacks and APIs. These will be able to handle TLS derivatives and easy provisioning schemes running on various radio links, together with UbiquiOS Technology and Avnet Services.

Avnet is also establishing certification authority services with a trusted partner for customers who do not wish to invest in a full public-key infrastructure themselves.

關於作者

Guillaume Crinon Headshot
Guillaume Crinon

Guillaume Crinon is the Global IoT Strategy Manager at Avnet, responsible for security and connectiv...

IoT Security: Real Problems and Solutions

IoT Security: Real Problems and Solutions

相關文章
young woman giving presentation
Adding AI and machine learning to IoT
By Jennifer Skinner-Gray   -   2025年12月12日
Avnet is helping more manufacturers integrate more types of AI and machine learning into more products. Multimodal AI and agentic AI will be crucial developments if artificial intelligence is to become seamlessly integrated into our lives.
coffee machine with embedded intelligence
Transitioning from IoT to edge AI system development
By Avnet Staff   -   2025年10月29日
Rapid developments in machine learning and artificial intelligence present challenges for embedded system engineers charged with bringing AI to edge devices. How should design teams address these challenges?

IoT Security: Real Problems and Solutions

相關活動

未找到相關活動