Your essential guide to edge AI terminology
Edge AI is the driving force behind a new generation of smart devices. Instead of relying on central servers, edge AI moves intelligent decision-making onto devices themselves, transforming everyday objects into instant problem solvers.
Edge AI is a trend reshaping industries, from healthcare to manufacturing, automotive to consumer electronics. AI comes with a fresh vocabulary for expressing these innovations.
This essential guide provides in-depth explanations of key edge AI terms, enriched with the context behind their introduction and illustrated with practical uses.
Spiking Neural Networks (SNNs): digital brains inspired by nature
Spiking Neural Networks represent a leap forward in emulating the workings of biological brains. Rather than maintaining a steady electric signal, these systems operate by sending quick electrical spikes, similar to neurons firing in the brain.
The intensity of the spike is comparable to the weight of connections in other types of neural networks. Pioneers in spiking neural networks say this results in higher computational efficiency, enabling devices to tackle complex recognition tasks while consuming very little power. High computational and power efficiency are crucial traits demanded by manufacturers of mobile wearables and distributed sensors.

Context and applications
SNNs began as theoretical concepts among neuroscientists who imagined computers that could recreate thought. The last decade's hardware advances have unlocked their real-world potential, enabling engineers to develop robots that react to speech and hand gestures in real time.
Neuromorphic processors designed for SNNs are now allowing drones, prosthetics and ambient sensors to function for weeks on limited batteries.
Neuromorphic computing: bridging organic and machine intelligence
Digital chips excel at repetitive calculations, but adapting to new situations has historically been a challenge. Neuromorphic computing solves this by structuring silicon pathways to mimic animal neural networks.
Sending data in irregular, responsive pulses instead of rigid, predictable patterns reduces energy usage. It also empowers rapid learning and adaptation.
Developers have built neuromorphic platforms that can interpret sights and sounds locally, without relying on distant servers. Industrial sensors, for instance, detect faults or anomalies and improve themselves with every new observation.
This approach is a foundational technology for autonomous robotics, which requires flexible adaptation to dynamic environments.
Context and applications
The concept of neuromorphic computing dates back to pioneering work in the 1980s. Today, it is flourishing, as real-time edge intelligence finds widespread commercial use.
TinyML: big learning, shrinking footprints
Like edge AI, TinyML describes running advanced machine learning algorithms on extremely compact, energy-efficient chips. In this case, those chips are typically microcontrollers (MCUs) or sensors with some on-device processing logic.
Rather than sending information to the cloud, edge-based techniques like TinyML focus on processing data locally and immediately, providing faster responses while maintaining data privacy.
Context and applications
The term “TinyML” predates the label “edge AI,” but both are predated by the concept of edge computing. The impact of TinyML has been particularly significant in consumer health. Wearable monitors can track irregular heartbeats and deliver instant feedback, keeping sensitive data on the device at all times. Environmental sensors also benefit, using TinyML to recognize pollution or hazardous conditions on the spot—a critical capability for public safety.
The discipline surged after the launch of the TinyML Foundation in the late 2010s, fueling innovation in everything from hearing aids to industrial automation. The Foundation changed its name in 2024 to the Edge AI Foundation, reflecting the direction of travel in the technology’s roadmap.
Neural Processing Units (NPUs): creating instant responses for complex tasks

Neural Processing Units are chips designed for lightning-fast neural network computation, while also optimizing battery life. Originally available only in top-tier smartphones and early IoT modules, NPUs are now widespread, supporting such features as instant facial recognition, augmented reality overlays and seamless voice-guided navigation.
Context and applications
As soon as NPUs reached mainstream devices in the 2010s, they became an essential standard across phones, edge cameras and portable assistants. This caused a surge in chip design competition, with manufacturers now aiming to create ever-faster NPUs, supporting complex tasks such as real-time language translation and advanced image analysis.
LiteRT (formerly TensorFlow Lite): streamlining AI for resource-limited devices
LiteRT (the RT stands for run-time) is a development toolkit that supports multiple framworks. Using LiteRT, AI applications run smoothly on devices with minimal computing power.
Originating from TensorFlow Lite, LiteRT helps developers compress and optimize models, so tasks such as gesture recognition and voice interpretation can happen directly on smartphones, microcontrollers and smart cameras.
LiteRT also includes support for hardware accelerators, enabling speed and efficiency that was previously impossible for edge-based AI.
Context and applications
TensoFlow Lite appeared in 2017, but Google changed its name to LiteRT in 2024, signaling a shift toward making AI both portable and lightning-quick, even for severely constrained platforms. Typical application examples include security cameras. Using LiteRT, cameras can analyze footage and detect threats locally, rather than depending on cloud servers to review every image.
Orchestration: seamless AI management across devices
Widespread adoption of edge devices brings new challenges in managing and updating their capabilities. Orchestration is the practice of automating and coordinating machine learning tasks over networks.
Orchestration between sensors, cameras and embedded devices using frameworks allows businesses in retail, logistics and security to deploy software updates and AI models on hundreds of devices simultaneously.
Context and applications
Orchestration forms the backbone of enterprise-scale edge deployments, ensuring that models are always optimized. For example, retailers can instantly update surveillance algorithms across all locations, responding to evolving threats in real time.
Inspired by DevOps automation techniques, orchestration for AI deployment gained traction in the early 2020s, enabling scalable and resilient operations outside traditional IT infrastructure.
Containerization and secure enclaves: reliable, private AI deployment
Containerization solves distribution challenges by packaging all software dependencies together with AI models, ensuring consistent updates and smooth operation across a variety of hardware. This modular method makes rapid updates and simple maintenance possible, which is essential for diverse edge environments.
Alongside this, secure enclaves give an extra layer of privacy, by isolating sensitive processing and user data in dedicated memory regions.
Context and applications
Secure enclaves are now nearly universal in wearables and mobile authentication devices that rely on biometric data. Containerization was first seen in enterprise IT in 2013. Secure enclaves have now become a central technology in edge applications, and commonplace in consumer devices.
Good to know:

Model compression a technique to reduce the size of the model so it requires less memory to store and run neural networks. Fewer memory read/writes speeds up workloads for small chipsets.
Quantization describes reducing the precision of the numbers used for calculations, saving memory and energy without noticeable losses in inference accuracy.
Knowledge distillation refers to small models “learning” from their larger counterparts, retaining skills with fewer resources.
Latency management a method employed to ensure responses to triggers are rapid and reliable. As an example, triggers could be voice commands or safety alerts.
These techniques and others now emerging represent a major departure from legacy, cloud-based machine learning. Edge AI enables real-time intelligence from everyday devices.
Final Thoughts: navigating the Edge AI revolution
Edge AI is changing the way machines learn, adapt and solve problems. Today’s innovations range from bio-inspired networks and learning silicon to advanced software that manages and protects intelligence in billions of devices.
The rapidly evolving language of edge computing equips designers, engineers and business leaders to create and leverage the next wave of intelligent devices.