how-to-choose-nics-for-ai-data-centers

how-to-choose-nics-for-ai-data-centers

How to choose NICs for AI data centers: Bandwidth, latency and offload explained

Nishant Nishant
network switch in data center
Choose NICs for AI data centers that balance bandwidth, latency, offload and PCIe.

KEY TAKEAWAYS:
  • NICs critical to AI performance
  • Balance bandwidth, latency
  • Match NIC features to workloads

Network interface cards (NICs) used to be the quietest line in a server bill of materials. In AI data centers, they have become headline devices. As GPU clusters grow from a handful of boxes to multi-rack training “pods,” the NIC turns into a pacing item for throughput, latency and how much useful work operators squeeze out of expensive accelerators.

AI is distributed computing at scale. Training jobs fan out across dozens or hundreds of nodes, each iteration triggering a storm of east-west traffic as gradients are exchanged, parameters synchronized and checkpoints pushed to storage. Inference workloads may not saturate the fabric as aggressively, but they are merciless about latency and jitter when user-facing service-level agreements (SLAs) are at stake. The NIC sits between the GPU and the top-of-rack switch, translating peripheral component interconnect express (PCIe) transactions into packets and offloading work that once belonged to the CPU. When that layer underperforms, the result is stalled iterations and blown latency budgets, even if the GPUs look fine on paper.

Why NICs dictate AI cluster performance

Speed is the first specification everyone reaches for, but in AI environments, it is only the beginning. A dense 8-GPU training server can justify 200 or 400 Gb/s of aggregate NIC bandwidth to keep collective operations from becoming the bottleneck. Smaller inference boxes might live at 100 Gb/s so long as tail latency remains under control and the fabric is not heavily oversubscribed.

Port configuration adds nuance. Dual port cards often split traffic across fabrics, one port into the AI network and another dedicated to storage, or provide redundant paths into a pair of leaf switches. The practical question is not “How fast can I go?” so much as “How much bandwidth per GPU do I need so that the accelerator, not the network, sets the pace?”

Latency and congestion behavior are just as important. Many training jobs are synchronous, so the slowest node dictates the cadence of the cluster. The numbers that matter live in the p99 and p999 columns of a benchmark spreadsheet, not in the averages on a datasheet. Small message performance is revealing because collective primitives often move tens or hundreds of bytes, not large Ethernet frames. Under load, the way a NIC interacts with congestion control, data center bridging and switch buffers determines whether the fabric degrades gracefully or periodically hiccups, sending engineers hunting for ghosts.

A card with slightly higher nominal latency but tight distribution under load is often a better choice for training than a part that looks great in microbenchmarks but suffers when queues build.

Offload engines and PCIe topology

NICs have evolved into packet-processing engines with PCIe interfaces. High-end devices for AI and high-performance computing lean on off-load features such as:

  • Remote direct memory access (RDMA) paths that bypass the CPU for memory-to-memory transfers
  • Direct GPU-to-NIC pipelines that avoid extra copies through system RAM
  • Programmable flow steering that routes packets to the right queue or virtual function with minimal software intervention

In multi-tenant AI clouds, offload for tunnel encapsulations and overlays keeps virtual networking from becoming a tax on every packet. These capabilities add silicon area and firmware complexity, but together they can reclaim CPU cores per rack or allow a smaller CPU footprint without starving the accelerators.

The PCIe fabric that feeds the NIC matters just as much. A 400 Gb/s card on a heavily shared PCIe switch that also serves eight GPUs may never reach its theoretical throughput. Non-uniform memory access (NUMA) placement adds another layer of complexity. When the NIC that feeds a group of GPUs is attached to the wrong CPU socket, cross-socket traffic can quietly erode performance, especially if the host is also busy with data preprocessing or orchestration. Architects increasingly model the NIC, PCIe topology and accelerator complex as a single subsystem with shared bottlenecks, rather than three independent blocks.

Operational requirements: telemetry and security

Once deployments reach hundreds or thousands of nodes, operational details come to the fore. An AI cluster running near line rate all day leaves little room for improvisation when something goes wrong.

Telemetry and manageability features move from nice-to-have to essential. Per queue statistics, hardware timestamps, congestion counters and integration with observability stacks turn the NIC into both a sensor and an interface. Security and isolation features such as single root I/O virtualization (SR IOV) for slicing cards between tenants, signed firmware and on-card crypto engines are hard requirements in hosted environments where multiple customers or departments share a fabric. Firmware lifecycle management becomes a project because rolling out a new image without interrupting in-flight training runs demands careful staging and robust hardware.

Matching NIC bandwidth and latency to GPU workloads

How these parameters are weighted depends on whether the cluster is dominated by training, inference or data engineering work.

Large synchronous training jobs are brutally honest about the network. Because every worker must participate in each collective operation, even modest congestion can stretch iteration times. Designers here focus on high per-node bandwidth, tight latency distribution, and strong RDMA and GPU direct support, and often choose NICs with explicit congestion control hooks and predictable behavior under load.

Inference-heavy environments put more emphasis on tail latency and predictable quality of service (QoS). Online recommendation systems and conversational models may send only a few kilobytes per request, but they do so constantly and cannot tolerate jitter. Priorities include fine-grained traffic shaping, support for multiple priority queues, and the ability to keep latency-sensitive inference traffic insulated from background jobs such as model refreshes or log shipping.

Data-hungry feature pipelines and storage-heavy workloads introduce another profile. These jobs often push large sequential reads and writes to distributed file systems or object stores. They benefit from high throughput and storage-specific offloads such as non-volatile memory express (NVMe) over Fabrics, but can accept higher latency. Many designs dedicate NIC ports on a separate storage fabric, which simplifies QoS at the cost of more aggregate I/O per node.

Decoding NIC datasheets: PCIe, RDMA, queues and telemetry

NIC datasheets usually present the same core elements: bandwidth and port counts, host interface, latency figures, feature tables, and power or thermal data. Each item maps directly to design decisions in an AI data center.

The “ports and speeds” section lists configurations such as “2 × 200 GbE” or “1 × 400 GbE,” along with interface types like QSFP56, OSFP, or SFP and sometimes qualified optics and DACs. For AI deployments, read this in terms of how ports map to fabrics and whether all ports can operate at line rate simultaneously on the target server.

The PCIe interface is given as lane width and generation, for example “PCIe 5.0 x16.” This defines the maximum host-side bandwidth the NIC can consume. A high-speed port on an undersized or oversubscribed PCIe connection will be bottlenecked regardless of switch capacity in the network.

Latency entries often quote round-trip numbers for packet sizes. Small packet and RDMA latency figures are most relevant for AI training and inference, but they should be treated as best-case minima, not guarantees for p99 or p999 behavior.

Feature tables enumerate protocol and offload support: RDMA variants, SR IOV and other virtualization schemes, NVMe over Fabrics, overlays such as VXLAN or GENEVE, and security options like IPsec, MACsec, and secure boot. For AI clusters, priority typically falls on RDMA and GPU direct paths, rich flow steering and queueing options, and any storage-specific offloads in use.

Telemetry and management sections summarize per queue and flow-level statistics, sensors, timestamping and management protocols. These capabilities determine how easily operators can diagnose congestion and firmware problems at scale. Power and thermal specifications, including typical and maximum power, airflow direction and temperature range, feed directly into rack-level power and cooling budgets, which are already tight in GPU-dense systems.

Once you understand the datasheet's language, you can normalize the different parts against one another. Simple comparison tables help by lining up candidate NICs against throughput class, supported offloads and natural workload “home.”

NIC classes chart

Example NIC classes for AI data centers shows typical bandwidth, off-load capabilities and best fit workloads.

Designing NIC strategy for GPU pods and spine leaf networks

Technical choices around NICs play out against changing deployment patterns. Many operators now organize infrastructure around GPU pods, racks or half racks of accelerator-dense servers homed on a redundant pair of top-of-rack switches. Within a pod, most traffic is east-west as training nodes synchronize with their neighbors. This stresses NIC capabilities such as link aggregation, failover and flow distribution across multiple uplinks.

A separate storage fabric is increasingly common, carrying NVMe over Fabrics or object store traffic on dedicated ports so that checkpointing and data ingest do not compete directly with gradient exchange. At the broader fabric level, leaf spine architectures move most traffic horizontally through multiple spines. NICs must coexist gracefully with ECMP hashing and traffic engineering, handling many similar flows without collapsing into hot spots when a popular model or service dominates the cluster.

Turning specs into a design checklist

In practice, NIC selection reduces to a few questions. Which workloads dominate: synchronous training, latency-sensitive inference or data-heavy pipelines? How much bandwidth per node and per GPU do you need today, and what margin will you want for the next accelerator generation? Which offloads are mandatory given your software stack and CPU budget? How mature are the drivers and firmware on the platforms you deploy? NICs are now design-in components for AI infrastructure, not interchangeable plumbing that can be swapped at the last minute. As models grow and clusters become more intricate, the network interface is where many of the most consequential system-level decisions land.

Avnet Networking and Communications Solutions

About Author

Nishant Nishant
Avnet Staff

We use Avnet Staff as a collective byline when our team of editors and writers collaborate on the co...

Helpful Links

how-to-choose-nics-for-ai-data-centers

how-to-choose-nics-for-ai-data-centers

Related Articles
AI data center
Tackling data center latency for AI: Why intra-DC microseconds matter as much as WAN milliseconds
By Avnet Staff   -   March 11, 2026
Within the data center, latency is a critical consideration for large-scale training and high-throughput inference setups. Leading AI training clusters are engineered for microsecond class communication.
Man working in modern data center
How communications networks in high-performance data centers are evolving
By Avnet Staff   -   March 10, 2026
Data center networks evolved rapidly over the past decade, driven by the need to handle growing data volumes efficiently while managing power, space and cost. Learn about the technologies making the advancements possible.