Custom Meta Tags

Category Page Switcher

APAC Nav and Training Switcher

培訓與活動
未找到相關活動

Category Attributes

工業

  篩選條件   工業 RSS FEED
令人振奮地是,工業設備和基礎設施的投資和創新正在振興。 從設計、構建並將您的工業應用推向市場,請瀏覽我們的工業知識庫或閱讀有關新技術以及其工程和流程的信息。

Featured

Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
看不見的它,正改變著人們的生產效能和生活體驗
2025年4月15日
面對環境隱形智慧領域的發展契機,安富利推出的AVT9152 模組結合了BLE(低功耗藍牙技術)、LTE-M、NB-IoT和GPS技術,非常適合低功耗和小尺寸物聯網應用,
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
安富利推動多功能機器人賦能工業自動化與智慧未來
2025年2月15日
隨著技術的不斷進步,我們有理由相信,多功能機器人將在未來的工業和生活中發揮更加重要的作用。
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
邊緣AI來襲:安富利幫助工業設備 “獨立思考”
2024年12月16日
邊緣AI作為推動工業智慧化轉型的核心力量,正在以驚人的速度嶄露頭角,成為實現更高效、智慧化生產的關鍵引擎。
Integration of Multiple Technologies Heralds a New Era in Smart Healthcare
工業數位化?低功耗、高性能、超強連接才是“超能力”!
2024年7月15日
全球約有1000萬家以上的工廠,總價值46萬億美元,因此,工業數位化對於製造業創新是極其重要的。低功耗、高性能和連接三大技術趨勢在工業運營數位化轉型中發揮了關鍵作用。
gas sensor device
Breathe easy: How electrochemical sensors safeguard air quality
By Avnet Staff   -   2024年4月29日
Design engineers seeking to develop more sustainable devices can turn to electrochemical gas sensors for a variety of applications that reduce carbon emissions, protect the environment and safeguard human health.
Conceptual image of smart car in purple
家用儲能系統:走向綠色能源的關鍵一步
2024年2月15日
隨著技術的不斷進步和市場的逐漸成熟,我們可以期待家用儲能系統在未來發揮更大的作用,推動全球能源向更清潔、更高效、更可持續的方向發展。
Conceptual image of smart car in purple
協作機器人:工廠自動化的“新寵”
2024年1月15日
協作機器人強調與人類工人的互動與協同,它們是工業自動化領域的一股清新之風,代表了自動化技術的一個新方向。
Conceptual image of smart car in purple
一路狂奔的專用5G網路有多強?
2023年9月15日
5G在大量資料處理以及設備連接方面的增強,使其可以支援從高品質影片流到即時資料分析等各種應用。
Conceptual image of smart car in purple
工業儲能:讓美好明天更可持續
By Avnet Staff   -   2023年8月15日
能源是氣候挑戰和可持續發展的核心,也是解決問題的關鍵。 能源存儲,是能源產生和使用鏈中最關鍵的部分,也是影響能源效率最大,技術發展最快的部分。
工業雲端平臺,提升品質增加效能的引擎
工業雲端平臺,提升品質增加效能的引擎
2023年4月15日
隨著人們日益增長對產品和服務個性化的需求,以及企業數位化進程的加速和對生產效率的追求,工業雲端平臺逐漸成為一個市場熱點
An engineer looks closely at an embedded system
Yes, you can get to market fast in IoT
By Mark Josewski   -   2023年1月9日
The IoT is giving OEMs new ways to serve customers. With these new products come new business models. Bringing a new solution to market takes effort. Where should you put your resources?
Two robot arms face each other in a clean room
Why you should be turning on to brushless DC motors
By Avnet Staff   -   2022年11月22日
For most applications, brushless DC motors are the more flexible and efficient choice.
mand holding testing equipment
穩健性測試對碳化矽供應鏈來說不可或缺
2022年11月10日
在高可靠性、高可用性的應用中,SiC半導體被視為新興技術。本文不僅介紹了SiC的優勢,還詳述了含有穩健性測試的端到端供應鏈,穩健的供應鏈使得SiC的品質更安全可靠。
hand reaching out
您知道碳化矽優值係數(Figures of Merit)的重要性嗎
2022年11月10日
碳化矽半導體在電力轉換設備中正變得無處不在,特別是在電動汽車、太陽能和儲能系統領域。本文通過分析各種應用,細緻探討了可用於比較器件的優值係數(Figures of Merit)。
generator
Why should you consider a smart monitoring system for your diesel generator?
By Philip Ling   -   2022年8月17日
The IoT is changing the way we manage and maintain essential assets. Smart sensors, cloud-based analytics and remote management are coming together to increase productivity, efficiency and reliability.
two buisiness people exchanging handshake with SiC icons overlayed
近距離觀測碳化矽的品質
2022年6月27日
碳化矽製造建立在現有的生產方法之上,但需要全新的工藝。提高產量和降低成本,有賴於在生產過程的每個階段保證最高品質。
An engineer is standing at a desk, using a computer. His hands are on a keyboard and a mouse, and he looks intently at the screen.
無程式碼設計如何加速工業物聯網的發展
By Philip Ling   -   2022年1月14日
為工業物聯網解決方案開發大量新的和多樣化的設備可能會挑戰您的工程資源。 使用無程式碼設計開發方法可以減少挑戰的規模和復雜性。
A group of colleagues working in a computer security room having a discussion
工業自動化發展如何,派個無人機去偵查!
2021年12月1日
工業自動化技術就是一種運用控制理論、儀器儀表理論、電腦資訊技術,對工業生產過程實現檢測、控制、優化、調度、管理和決策,實現增加產量、提高品質、降低消耗、確保安全等目的
Cleanroom tech with wafer
借助 SiC 技術,實現三大設計自由
By Milan Ivkovic   -   2021年4月17日
儘管 SiC 技術的性能和潛力無庸置疑,但一些設計人員最初可能仍然會猶豫不決,無法下定決心使用 SiC 技術來處理新專案
lab techicians
與Si 相比,SiC 技術優勢無庸置疑
By Milan Ivkovic   -   2021年4月16日
目前,碳化矽 (SiC) 技術發展到了引爆點,它的明顯優勢推動著實際應用的廣泛採用。
Circuit board
FPGA、GPU 與 CPU – 人工智慧應用程式的硬體選擇
2021年3月31日
現場可程式設計閘陣列 (FPGA) 為人工智慧 (AI) 應用帶來了許多優勢。圖形處理單元 (GPU) 和傳統的中央處理單元 (CPU) 相比,孰優孰劣?
Graphic of a digital eye with Avnet 100 year anniversary logo at the bottom right corner
利用人工智慧開發機器視覺系統可能存在的十大陷阱
2021年3月31日
機器視覺 (MV) 和人工智慧 (AI) 為各類前沿應用程式提供了寶貴的檢測和分析功能。與所有先進技術一樣,該領域也存在一些陷阱,需要小心防範。
A group of colleagues working in a computer security room having a discussion
時間敏感型網絡(TSN):一次性對乙太網的“改造”
2020年8月1日
工業4.0以及工業物聯網(IIoT)的興起,讓人們踏上了一條對乙太網進行深度“魔改”之路,作為這次“魔改”成果的TSN正在前面向我們招手,現在是時候加快腳步,向著這個目標衝刺了。
Two robotic arms
縮短工業物聯網的設計時間
2019年4月23日
目前工業市場的相關討論,大多聚焦於工業物聯網 (IIoT) 的龐大的市場潛力。其驚人的創新潛能,預期可大幅提升生產力、作業效率和利潤,但前提是必須由能兼顧可靠性、穩定性和長效
Graphic of iris recognition
智慧製造,需要什麼樣的工業之“眼”?
2017年8月18日
在市場需求驅動下,近年來工業視覺市場一直保持較快的增速。據高工產業機器人研究所(GGII)預測,中國工業驅動的機器視覺市場規模預計到2020年將超過120億元,2017-2020年均增速將達15
First1 Last  Results Per Page: 30 6090All