Zynq SoMs Decrease Customer Development Times and Costs

Display portlet menu

Zynq SoMs Decrease Customer Development Times and Costs

Display portlet menu

Zynq SoMs Decrease Customer Development Times and Costs

lab tech in cleanroom gear holding up micrchip

Xilinx’s Zynq®-7000 All Programmable (AP) System-on-Chip (SoC) provides a new paradigm for embedded system design, blurring the line between traditional processors and FPGAs. These devices combine the software programmability of a processor with the hardware programmability of an FPGA. The Zynq AP SoC provides unrivaled levels of system performance, flexibility and scalability while providing system benefits in terms of power reduction, lower cost with fast time to market.

Customers agree that Zynq SoCs can potentially revolutionize embedded system design. Alan Boate, CEO of Canada-based Ajile Light Industries, says he “sees the future of embedded design based on the combination of Zynq PS (Processing System) and PL (Programmable Logic).” John Battles, founder of New Mexico-based Mountain Storm Instruments, LLC, chose Zynq SoCs for their high-speed performance and open source software community that “leverages existing development tools, libraries, programming languages, and applications.”

While the Zynq AP SoC simplifies embedded system design at the architecture level, developing a Zynq-based chip-down solution poses many design challenges. All Zynq-based designs require enabling circuitry to function properly. This usually includes DDR3 SDRAM, Ethernet, USB, UARTs and power regulation. Each enabling circuitry requires nuances to make Zynq work properly.

 

“Avnet’s customers have found unique homes for SoMs in cable set-top boxes, various avionics applications, and medical devices.”

 

As an example, designing the high-speed DDR3 interface for Zynq requires a deep understanding of transmission line theory. The PCB layout calls for matching trace lengths, controlling impedances and using proper termination. If designed improperly, several PCB spins and months of development times can be wasted.

Similarly, the power regulation requirements of Zynq can be tricky for designers. All Zynq AP SoCs have multiple voltage rails that require multiple voltage levels. Voltage levels must fall within tight tolerances for optimal performance. Power supplies must start-up and sequence appropriately while accommodating varying current loads and transients.

Electrical design engineers continuously meet technical challenges ensuring working circuitry. However, designing and debugging Zynq-enabling circuitry takes both time and money. Jeremy Gribben, CTO at Ajile Light Industries, relates that Ajile consumed three costly months developing and testing the interface between Zynq and LVDS-enabled CMOS imagers and displays.

Sensing the need to lessen the technical challenges of designing Zynq-based systems while shortening customer design cycles, Avnet has developed a series of Zynq-based system-on-modules (SoMs). All Avnet SoMs provide core Zynq functionality including memory, configuration, Ethernet, USB, and power. Additionally, Avnet’s SoMs provide customers a migration path, from evaluation and development to production, using the same hardware solution.

One of the first Zynq-based SoMs that Avnet produced was MicroZed™. Its unique design allows it to be used as both a stand-alone evaluation board or combined with a carrier card as an embeddable SoM. MicroZed contains two I/O headers that provide connection to two I/O banks on the programmable logic (PL) side of the Zynq-7000 AP SoC device. In stand-alone mode, these 100 PL I/Os are inactive. When plugged into a carrier card, the I/Os are accessible in a manner defined by the carrier card design.

For more information on MicroZed, please visit microzed.org/product/microzed.

 

In response to customer feedback for smaller, ruggedized and cost-effective SoMs, Avnet recently released PicoZed™. This device offers designers the flexibility to migrate between the 7010, 7015, 7020, and 7030 Zynq-7000 AP SoC devices in a pin-compatible footprint. PicoZed contains the common functions required to support the core of most SoC designs and provides easy access to over 100 user I/O pins through three MicroHeaders on the backside of the module. The MicroHeaders also support access to dedicated interfaces for Ethernet, USB, JTAG, power and other control signals, as well as the GTP/GTX transceivers on the 7015/7030 models. The transceiver based 7015 and 7030 versions of PicoZed are a superset of the 7010/7020 version, adding four high-speed serial transceiver ports to the I/O connectors. Designers can simply design their own carrier card, plug-in PicoZed, and start their application development with a proven Zynq-7000 AP SoC sub-system.

For more information on PicoZed, please visit microzed.org/product/picozed.

 

Avnet’s first Zynq SoM to market, the Xilinx Zynq®-7000 AP SoC Mini-Module Plus (MMP), supports the 7045 and 7100 Zynq AP SoCs. The Zynq MMP SoM, when combined with a MMP Baseboard II and a MMP Power Supply, provides an out-of-box development system ready for prototyping. The Zynq MMP boasts various I/O options including 132 user I/O pins, 8 GTX transceivers, USB 2.0, Gigabit Ethernet, PCI Express, and DisplayPort. Additionally, the Zynq MMP SoM can be placed on a user created carrier card for customized applications targeted for production.

For more information on Zynq MMP, please visit microzed.org/product/zynq‑mmp.

 

In addition to simplifying hardware design, Avnet jumpstarts Zynq-based software, firmware and HDL development by providing the necessary tools to get started. MicroZed, PicoZed and Avnet’s entire portfolio of Zynq-based SoM have board support packages (BSPs) available. Industry-leading operating systems have been ported to these SoMs. Reference designs and tutorials familiarize engineers to Xilinx’s development tools.

 

“Customers agree that Zynq SoCs can potentially revolutionize embedded system design.”

 

Avnet’s MicroZed and PicoZed are targeted at many applications including test and measurement, motor control, and software-defined radio (SDR). Avnet’s customers have found unique homes for SoMs in cable set-top boxes, various avionics applications, and medical devices. MicroZed, in particular, has been adopted by many customers to quicken time to market and save resources.

Mountain Storm Instruments, LLC (MSI) designs and manufactures Flexible Sensor Platforms (FSP) and Intelligent Sensor Platform (ISP) targeted at remote wireless sensing. While previous versions of its solutions were based on16-bit and 32-bit MCUs, the company chose Zynq for its next generation designs due to the peripherals, integration, high-speed performance and open source ecosystem.

Instead of designing a chip-down solution, MSI chose Avnet’s MicroZed SoM. John Battles says, “Avnet has built a flexible Zynq platform that eases the Zynq design process. It hits the sweetspot in the market and provides a unique solution.” He continues, “The microzed.org community site helps lower the support burden. MicroZed has been designed for OEM use in real products. For small start-ups, order size flexibility is essential when the market demand is unknown.”

MSI’s SmartDAQ 1000 ISP uses Avnet’s MicroZed for its Zynq Sub-system. For more information, please visit mtnstormdaq.com.

After investigating chip-down Zynq solutions, Ajile Light Industries was looking for a simpler way to utilize Zynq across its high-speed, high-definition image sensor and DMD display designs for applications in industrial inspection, 3D metrology and medical devices. Jeremy Gribben recounts that MicroZed was adopted because it “improves the development time of a company our size.” He continues, “The training, tutorials and reference designs provided by Avnet were helpful to get us up and running. The support documentation is at a higher level than other similar solutions.”

Xilinx’s Zynq-7000 AP SoC solutions are quickly changing the industry in embedded system design. Avnet continues to drive market adoption of this differentiated technology by providing a growing family of Zynq-based SoMs that minimize design effort, reduces time to market and developments costs, and allows customer to focus on their core competency. For more information on all of Avnet’s Zynq SoM solutions, please visit www.microzed.org.

Zynq SoMs Decrease Customer Development Times and Costs

Display portlet menu

Zynq SoMs Decrease Customer Development Times and Costs

Display portlet menu
Related Articles
Business people around a table in a meeting about IoT security
Customization comes with a competitive edge—and security challenge
By Guillaume Crinon   -   September 6, 2018
Whether you have an in-house team or are exporting the building of infrastructure to a trusted partner, make sure the team is asking the right questions when it comes to implementing and deploying IoT solutions.
Graphic depicting the world globe with a transparent computer screenshot of the world map overlaid to the right of it
Fueling Up On Smart Maps – Mapping Technology In Oil And Gas
March 22, 2019
It’s a political hot topic, a major export and even the reason wars have been fought. It touches almost every aspect of our lives.
man in red flannel shirt at workstation
In their words: Benefits of the world’s biggest engineering community
September 5, 2018
In the summer of 2018, Avnet celebrated a major milestone: 1 million community members across Hackster.io and element14. As a project-based site, Hackster enables anyone to jump feet first into hardware through knowledge sharing, as well as contests
Alex Glow
From hacker spaces to Hackster.io: Alex Glow owes her career in hardware to communities
July 17, 2018
Exposure to engineering as a kid helped Alex Glow fall in love with hardware. But it was communities that gave her confidence to turn her hobby into a career.
Kitty Yeung, maker, kittyyeung.com
Model behavior with microcontrollers: Kitty Yeung’s intersectional engineering spans art, science
July 6, 2018
“Current established industries don't often leverage people's multiple talents and passions. But the forthcoming generations of the workforce are getting more interdisciplinary and they need opportunities to develop and grow.”
Young woman wearing safety gear standing in tunnel
Element14 allows Sneha Nidhi to continue a lifetime of learning
June 22, 2018
Sneha Nidhi always comes from a community of engineers. Her first was her family.
Young man standing in front of monitors
How one engineer found both confidence and community in element14
June 22, 2018
Tracking Santa Claus changed the track of Frederick Vandenbosch’s life.
man standing and stretching while looking at his tablet on the desk
Standout Product Keeps Employees from Sitting Too Much
June 1, 2017
You’ve probably heard in the news lately how unhealthy sitting can be. According to WebMD, sitting for long hours has been linked to mental health problems, obesity, death from heart disease and cancer, and other conditions.
IoT concept icons over building
Red Hat and Eurotech Partnership: Paving Way for End-to-End Architecture for IoT
April 26, 2017
Red Hat Inc., in its March 2016 press release, announced its collaboration with Eurotech, a leading M2M and IoT solution provider based out of Italy.
timelapse image of sunset with vehicle lights
Mobile Asset Tracking With Bing Maps: Keeping Your Fleet Fleet
April 4, 2017
You can have a fleet of things, like vehicles. Or you can be fleet, as in fast. OR, in the case of transportation logistics, it could mean both.
dollar bill folded into an arrwo and placed upon a world map
Maps For Your Business: It's More Than You Think
April 2, 2017
If you run a business, then you want to be found. It seems like a no-brainer right? Customers have to be able to find your store to be able to make a purchase. So you put your address and a map of your locations on your website.
pills in the shape of a map
Mapping For Senior Care: The Potential of Bing Maps In A Growing Industry
April 1, 2017
It’s hard to admit it, but we’re all getting old. With the huge population of Baby Boomers all entering their senior years, the number of senior Americans is higher than it’s ever been.
A billboard with the graphic of a cloud connected city on it
Not Your Father’s Billboards – Bing Maps Brings The Out-Of-Home Industry Into the Digital Age
March 31, 2017
When you hear the words “Outdoor Advertising” you might think of dusty highway billboards and smiling realtors on bus stop benches. 20 years ago, that was probably pretty close to accurate. Today, it’s a different story.
Graphic of a person using IoT for several applications
Going Up? Elevators, Windows 10 And The Internet Of Things
March 30, 2017
People are excited about the Internet of Things for a variety of reasons. It’s already made us more connected. And as more and more things are connected, a number of industries are poised to become faster, more efficient and more reliable.
2D image of a brown cat holding a Microsoft flag and riding a flame breathing white horse
One Windows to Rule Them All
March 20, 2017
Unless you’ve been on an extended vacation on a remote tropical island you know Windows 10 was released on July 29. And the hype is huge.
yellow map with orange navigation icon
Setting a Course For A Golf Course With Bing Maps
March 13, 2017
With more than 25 million regular players worldwide, there’s no doubt that golf is one of the most popular past times on the planet. And it’s a sport that’s growing every year.
business man standing on small rowboat in the ocean
What To Do With All That Data
March 6, 2017
Just as important as the hardware and the data it collects in an Intelligent System are the tools we need to process and analyze information. Otherwise, an Intelligent System does nothing to serve our purposes.
Woman clicking on a map on a large touch screen
Bing maps V8 control brings exciting upgrades for developers
March 2, 2017
For developers, being able to pack more features into apps is definitely a plus. And that’s exactly what Microsoft is trying to help you with.
5 kids looking at a laptop
Bing Maps Is Bringing The World To The Classroom
March 2, 2017
You’ve heard about Bing Maps for business, right? Companies in a wide variety of industries are using Bing Maps to drive sales, increase efficiency and save money.

Zynq SoMs Decrease Customer Development Times and Costs

Display portlet menu
Related Events

No related Events found