Custom Meta Tags

MSe SHARED Embedded Software Hero (HBv2)


Embedded Software

MSe Win10 IoT E 2021 text (LC)

Windows 10 IoT Enterprise 2021

Windows 10 IoT Enterprise 2021 is a new operating system offering for embedded and IoT devices. Microsoft delivers enterprise-class power, security, and manageability to the Internet of Things in addition to new features and capabilities. Premium features such as advanced protection against modern security threats and comprehensive device management, app management, and control capabilities are added. Windows 10 Enterprise LTSC 2021 includes the cumulative enhancements provided in Windows 10 versions 1903, 1909, 2004, 21H1, and 21H2.

Windows 10 Enterprise LTSC 2021 has a 5 year lifecycle, but Windows 10 IoT Enterprise continues to have a 10 year lifecycle.

Microsoft Edge Browser support is now included in-box and Microsoft Edge kiosk mode is available for LTSC releases starting in Windows 10 IoT Enterprise 2021 LTSC. Microsoft Edge kiosk mode offers two lockdown experiences of the browser so organizations can create, manage, and provide the best experience for their customers. 

WPA3 H2E standards are supported for enhanced Wi-Fi security.


There are no changes in the pricing model
It is based on the type/performance of processors used in your hardware.

Subject to change – please contact microsoft[at]avnet.eu for the actual CPU to license matching. The license prices vary depending on the type of processor you are using. We are happy to send you an offer, based on your specific need and/or Tier level.

From the technical standpoint, there is no difference in between the 3 license options. It´s the same installation media without any feature restriction.

There are two update models available, covered under the following licensing options:

SAC
The SAC - Semi Annual Channel. Twice a year the OS will receive feature updates and regularly security and other updates. The feature updates in H1 and H2, which means the first and the second half of a calendar year can change the OS up to a complete new OS version. In the past these updates took place in March and September (1803 and 1809 indicate the versioning).
Windows 10 IoT Enterprise SAC is a complete Windows 10 Enterprise version.

LTSC
As an alternative to the Semi Annual Channel (SAC) version, Microsoft offers a LTSC (Long Term Servicing Channel, formerly LTSB - Long Term Servicing Branch) version.
For example, there is no Microsoft Store and Cortana in this version. So the updates can be controlled and there is no must to install them.

MSe Win10 IoT E 2021 more (GBLS)

MSe Contact Box for Modal (html)

Contact Us Image

Contact Us
 

Need local assistance for your Microsoft Embedded Solution? Let us know!
 

CONTACT OUR EXPERTS

 

 

MSe Win10 IoT E 2021 links downloads (GBLS)

Links & Downloads

Partner for training:

IT Consulting Swiontek
Rudi Swiontek
(CEO / Trainer)
e-mail: rs[at]it-swiontek.de
Website: http://www.it-swiontek.de/

MSe SHARED Contact Modal

Contact us

Please let us know how we can assist you by filling in your details below and clicking on 'Submit'.

 
 

MSe Win10 IoT E 2021 table (LC)

Enterprise and IoT LTSB/LTSC editions

Version Servicing Option Date of availability Mainstream support end date Extended support end date
21H2     Long-Term Servicing Channel (LTSC) 2021-11-16 2027-01-12 2032-01-13 (IoT Enterprise only)
1809     Long-Term Servicing Channel (LTSC) 2018-11-13 2024-01-09 2029-01-09 (IoT Enterprise only)
1607     Long-Term Servicing Branch (LTSB) 2016-08-02 End of servicing 2026-10-13 (IoT Enterprise only)
1507 (RTM) Long-Term Servicing Branch (LTSB) 2015-07-29 End of servicing 2025-10-14

https://docs.microsoft.com/en-us/windows/release-health/release-information

Windows 10 Enterprise LTSC 2021 builds on Windows 10 version 21H2 adding premium features designed to address the needs of large and mid-size organizations), such as:

  • Advanced protection against modern security threats with System Guard, Attack surface area reduction  and Windows Security App
  • Full flexibility of OS deployment with SetupDiag and the latest ADK/MDT
  • Updating and support options
  • Comprehensive device and app management and control capabilities through Windows Sandbox and Microsoft Defender Application Guard

For more details please have a look at https://docs.microsoft.com/en-us/windows/whats-new/ltsc/whats-new-windows-10-2021

Note: Not all features in an update will work on all devices. A device may not be able to receive updates if the device hardware is incompatible, lacks current drivers, or is otherwise outside the original equipment manufacturer’s (OEM) support period.
Source: https://support.microsoft.com/en-us/help/13853/windows-lifecycle-fact-sheet

 

MSe Win10 IoT E 2021 Back to Top