Custom Meta Tags

Hero Banner

Pressure Sensors: The Design Engineer's Guide

Long Copy

Piezoelectric pressure sensors

What are piezoelectric pressure sensors?

Piezoelectricity is the charge created across certain materials when a mechanical stress is applied.

Piezoelectric pressure sensors exploit this effect by measuring the voltage across a piezoelectric element generated by the applied pressure. They are very robust and are used in a wide range of industrial applications.
 


When force is applied to a piezoelectric diaphragm, a
voltage proportional to the pressure is generated

Working principle

When a force is applied to a piezoelectric material, an electric charge is generated across the faces of the crystal. This can be measured as a voltage proportional to the pressure (see diagram to the right).

There is also an inverse piezoelectric effect where applying a voltage to the material will cause it to change shape.

A given static force results in a corresponding charge across the sensor. However, this will leak away over time due to imperfect insulation, the internal sensor resistance, the attached electronics, etc.

As a result, piezoelectric sensors are not normally suitable for measuring static pressure. The output signal will gradually drop to zero, even in the presence of constant pressure. They are, however, sensitive to dynamic changes in pressure across a wide range of frequencies and pressures.

This dynamic sensitivity means they are good at measuring small changes in pressure, even in a very high-pressure environment.
 

Function

Unlike piezoresistive and capacitive transducers, piezoelectric sensor elements require no external voltage or current source. They generate an output signal directly from the applied strain.

The output from the piezoelectric element is a charge proportional to pressure. Detecting this requires a charge amplifier to convert the signal to a voltage.

Some piezoelectric pressure sensors include an internal charge amplifier to simplify the electrical interface by providing a voltage output. This requires power to be supplied to the sensor.

An internal amplifier makes the sensor simpler to use. For example, it makes it possible to use long signal cables to connect to the sensor. The amplifier can also include signal-conditioning circuitry to filter the output, adjust for temperature and compensate for the changing sensitivity of the sensing element.

The presence of the electronic components does, however, limit the operating temperature to not much more than 120ºC.

For higher temperature environments, a charge-mode sensor can be used. This provides the generated charge directly as the output signal. It therefore requires an external charge amplifier to convert this to a voltage.

Care is required in the design and implementation of the external electronics. The high impedance output of the sensor means the circuit is sensitive to noise caused by poor connections, cable movement, electromagnetic and RF interference.

The low frequency response of the sensor is determined by the discharge time of the amplifier.
 

Construction

The piezoelectric effect requires materials with a specific asymmetry in the crystal structure. This includes some natural crystals, such as quartz or tourmaline.

In addition, specially formulated ceramics can be created with a suitable polarisation to make them piezoelectric. These ceramics have higher sensitivities than natural crystals. A useful output can be generated with as little as 0.1% deformation.

Because the piezoelectric materials are rigid, only a very small deflection of the material is required to get a usable output signal. This makes the sensors very robust and tolerant of over-pressure conditions. It also means they respond rapidly to changes in pressure.

The pressure sensor can be affected by any external force on the piezoelectric element, for example, by forces caused by acceleration or noise.

Microsensors can be constructed using thin films. Zinc oxide was one of the first materials used. This has largely been replaced by ceramics made from materials such as lead zirconate titanate (PZT) because of their larger piezoelectric effect.

Micoelectromechanical systems (MEMS) can be created by combining piezoelectric thin films with micromachined silicon membranes.

Piezoelectric materials are also used in some other types of MEMS sensors. For example, the inverse piezoelectric effect is used to generate surface acoustic waves through a diaphragm. The distortion of the surface under pressure can then be detected by the changes it causes in the waves that are received by another piezoelectric element.
 


 A cross-section of a piezoelectric presure sensor construction

Design

Piezoelectric pressure sensors are often constructed in a threaded tube (as shown in the diagram below) to make it easy to mount them in equipment where pressure is to be monitored. Care is needed when installing these because over-tightening can affect the output sensitivity.

In some of the typical applications of piezoelectric sensors, they may be exposed to thermal shock (a sudden change in temperature) caused by either radiant heat or the flow of hot gases or liquids past the sensor.

This can cause changes to the output due to heating of the crystal, the diaphragm or the casing of the sensor. Note that this is not the same as the static temperature sensitivity of the sensor.

The effects of thermal shock can be minimised by the design of the enclosure and mounting the sensor to provide isolation.
 

 

Sensitivity

The output is linear over a wide range, typically 0.7 KPa to 70 MPa (0.1 to 10000 psi) with an accuracy of about 1%.

Ceramic sensors are subject to a loss of sensitivity over time. But this is usually quite small; typically less than 1% per year.

There may also be a small loss in sensitivity when first exposed to high pressure and temperature. The effects of this can be avoided by cycling the sensor through the maximum expected pressure and temperature before deploying them.

The frequency response of a piezoelectric sensor drops off at low frequencies because the generated charge cannot be retained.

At high frequencies there is a peak corresponding to the resonant frequency of the piezoelectric element. The sensor is normally used within the flat region of the response curve between these two extremes (see below).


The frequency response of a piezoelectric sensor

Applications

The robustness, high frequency and rapid response time of piezoelectric pressure sensors means they can be used in a wide range of industrial and aerospace applications where they’ll be exposed to high temperatures and pressures.

They are often used for measuring dynamic pressure, for example in turbulence, blast, and engine combustion. These all require fast response, ruggedness and a wide range of operation.

Their sensitivity and low power consumption also makes them useful for some medical applications. For example, a thin-film plastic sensor can be attached to the skin and used for real-time monitoring of the arterial pulse.
 

Advantages and disadvantages

One of the main advantages of piezoelectric pressure sensors is their ruggedness. This makes them suitable for use in a variety of harsh environments.

Apart from the associated electronics, piezoelectric sensors can be used at high temperatures. Some materials will work at up to 1,000ºC. The sensitivity may change with temperature but this can be minimised by appropriate choice of materials.

The output signal is generated by the piezoelectric element itself, so they are inherently low-power devices.

The sensing element itself is insensitive to electromagnetic interference and radiation. The charge amplifier and other electronics need to be carefully designed and positioned as close as possible to the sensor to reduce noise and other signal errors.

Piezoelectric sensors can be easily made using inexpensive materials (for example quartz or tourmaline), so they can provide a low cost solution for industrial pressure measurement.

Want to learn more about the other core technologies used in pressure sensors? Click the links below to jump to the section you're interested in.


Looking for more on pressure sensor technology? Check out the further chapters of this guide below, or if you're pressed for time you can download it in a PDF format here.

Pressure Sensors Contact GBL

Need some advice on pressure sensors?

Our pressure sensor experts are on hand to help you make the right choice for your application.

Right Rail Card Dark

Webinar

Discover the keys to designing pressure sensor applications with this 30-minute technical presentation and Q&A with Nicholas Argyle, Applications Engineer EMEA, TE Connectivity.

Watch On Demand

Right Rail Card Dark_1

White paper

Need a more digestible introduction to pressure sensors? Download the white paper, 'Pressure sensors: Design considerations and technology options'.

Download

Right Rail Card Dark_2

Sensor solutions brochure

Discover the latest sensor solutions available from Avnet Abacus.

Download

Right Rail Card Dark_3-RB

Sensors linecard

Explore our pan-European sensor suppliers and their products and solutions.

Learn More

Right Rail Card Dark_3-KI

New products

Discover the latest product announcements from our sensor suppliers.

Learn More

Pressure Sensors Chapter 1 GBL

Chapter 1

How pressure sensors work

An introduction to pressure sensors covering the different types, how they work, their function, construction, and what to consider in your design choices.

Pressure sensors chapter 1 graphic

Pressure sensors chapter 5 GBL

Chapter 5

Types of pressure measurement

What’s the difference between absolute, gauge and differential pressure sensors? And how do you know which one to use?

Pressure sensors guide chapter 5 graphic

Pressure Sensors Chapter 2 GBL

Chapter 2

Pressure sensor applications

Discover the recent innovations in pressure sensor technology that are enabling smarter, safer, and more environmentally friendly electronics for businesses and consumers alike.

Pressure sensor guide chapter 2 graphic

Pressure sensors chapter 7 GBL

Chapter 7

Pressure sensors for different media types

An in-depth guide to pressure sensors for different media types. Learn about the technology, applications, different options, their specifications and their limitations.

Pressure sensor guide chapter 7 graphic

Pressure Sensors Chapter 3 GBL

Chapter 3

The different types of pressure sensors

Discover how pressure sensors vary according to the type of pressure measurement, sensing principles, output signal, media, MEMS technology, mounting and more.

Pressure sensor guide chapter 3 graphic

Pressure sensors chapter 8 GBL

Chapter 8

Pressure sensing in harsh environments

An in-depth guide to pressure sensors for harsh environments - designing for extreme temperatures, high pressure, and corrosive and dynamic environments.

Pressure sensor guide chapter 8 graphic

Pressure sensors chapter 4 GBL

Chapter 4

Pressure sensor output signals

Sensors, transducers, or transmitters? The right selection is important for your application. So what's the difference and how do you choose between them?

Pressure sensor guide chapter 4 graphic

Pressure sensors chapter 9 GBL

Chapter 9

Understanding specifications

Explore the datasheet and the different factors affecting the accuracy of pressure sensor readings. Discover how to make the right choice for your application.

Pressure sensor guide chapter 9 graphic

NPI Product Table

New products

ImageProductNew
Amphenol Advanced Sensors LCIS media compatible pressure sensors
Amphenol Advanced Sensors NovaSensor division LCIS media-compatible pressure sensors feature a high stability SenStable® backside MEMS piezo-resistive chip placed in a board-mountable package. The ceramic button pressure port isolates on-board elect
 
Bourns BPS125 series ultra-low pressure digital pressure sensor
Bourns' BPS125 series pressure sensor is based on Microelectromechanical Systems (MEMS) technology. The BPS125 is 3.3V capable and is calibrated for pressure ranges from 250Pa to 1PSI. Designed for advanced sensor needs in industrial automation, ener
 
ALPS HSPPAD143A series water proof pressure sensor
The Alps Alpine HSPPAD143A series single sensor measures air and water pressure, and features low current consumption with a dedicated ASIC.   Features Broad measurement range from 9,000 metres altitude to 10 metres underwater1.8µA low current con
 
Bourns BPS140 series environmental sensors
Bourns Sensors & Controls Product Line is introducing a new series of environmental sensors based on Microelectromechanical Systems (MEMS) technology. Designed for the advanced sensor needs in Industrial Automation, Energy, Building & Home Control a
 
Amphenol Advanced Sensors NPA low pressure mount pressure sensors
The NPA product series is provided in a miniature size as a cost effective solution for applications that require calibrated performance. Packaged in a SOIC14 pin surface mount, the NPA-Low Pressure Series is available in Gauge or Differential press
 
Amphenol Advanced Sensors NPA series surface mount pressure sensors
The NPA Series of Surface-Mount Pressure Sensors is provided in a miniature size as a cost effective solution for applications that require calibrated performance. Packaged in a SOIC14 pin surface mount, the NPA Series is available in gauge, absolut
 
TE Connectivity MS5840-02BA pressure sensor
TE Connectivity (TE) introduces the MS5840-02BA pressure sensor; one of the lowest profile micro altimeters in the market. This ultra-compact gel-filled pressure and temperature sensor is optimized for both altimeter and barometer applications and is
 
Bourns BPS110, BPS120, BPS130 and BPS230 series environmental sensors
Bourns Sensors & Controls Product Line is introducing a new line of environmental sensors based on Microelectromechanical Systems (MEMS) technology. The initial products offered in the Bourns® Precision Sensor (BPS) line are three pressure sensor mod
 
OMRON 2JCIE-BU01 series USB type environment sensors
OMRON has launched a USB type version of its 2JCIE environment sensor, designed to sense a range of environmental conditions. Featuring network connectivity via USB or Bluetooth, the sensor combines VOC, humidity, light, barometric pressure, and soun
 

Static HTML