Custom Meta Tags

Category Page Switcher

APAC Nav and Training Switcher

Training & Events
No related Training & Events found

Category Attributes

5G

  Filter By   5G RSS FEED
The 5G mobile network standard is now being widely deployed, but it’s only the beginning of the story with work on 6G already underway. Whether you’re designing 5G infrastructure or end products, dive into the latest information from Avnet on evolving technologies, trends, applications, and solutions.
Woman riding in self-driving car.
Bringing mm-wave beamforming to new applications
By Steven Fireman   -   April 9, 2024
With 5G rolling out and the help of phased array antennas, the 30 to 300 GHz, and specifically the millimeter-wave bands, of the RF spectrum are making their way into applications like autonomous driving.
Computer board, laptop and test equipment
Private 5G networks are becoming fundamental to enterprises
By Avnet Staff   -   January 27, 2023
Cellular networks are no longer the exclusive domain of traditional telecom operators. If you are looking for guaranteed service levels, you should consider a private 5G network. The key is to master mmWave and MIMO technologies.
two combines in field
How 5G networks support precision agriculture
By Avnet Staff   -   January 9, 2023
Modern farming faces many challenges, but technology holds the key. Precision agriculture uses the latest technologies, enabled by 5G networks. Drones and robots have joined tractors and harvesters, becoming the hardware of farming.
bus, greenhouse, satellite, auto manufacturing
Explore some real-world examples of private 5G networks
By Avnet Staff   -   January 6, 2023
There are increasing examples of private 5G networks, but many more at the trial-and-test bed stage. Find out why all kinds of industries are building private 5G networks rather than using public 5G networks.
cityscape
More industries seek performance benefits of private 5G networks
By Avnet Staff   -   January 6, 2023
We have waited 10 years for public 5G networks. While real-world implementations of private networks are in their infancy. Owning one means you don’t have to wait any longer. You also get exclusive access to the performance 5G offers.
satellites in low Earth orbit
Putting 5G in space for the massive IoT
By Philip Ling   -   January 4, 2023
5G cellular networks and the massive IoT are a natural fit. Putting 5G cell towers in space is taking massive to a new level. To learn more, Avnet spoke with Sateliot Chief Business Officer Gianluca Redolfi, one of the pioneers in this area.
electric vehicle dashboard
What is polarization, keying and color coding for interconnect?
By Jamie Pederson   -   April 10, 2022
Establishing a properly aligned connection quickly is key in any assembly or installation process. Polarization, keying and color coding are primary means to ensuring connections are made quickly and safely. In this article we’ll discuss each of
The double edge of standing waves
By Philip Ling   -   April 1, 2022
A standing wave occurs when the reflected signal is in phase with the source. When it happens in a transmission line, it is normally unwanted because it results in emitted radiation. However, it is exactly that radiation that maximizes the signal’s streng...
person holding tablet computer
Putting the smarts into building automation
March 21, 2022
Smart building automation can augment the capabilities of today’s building management systems and create new data flows that reveal insights about how a building is functioning and used. It can also enable new revenue streams for building managers.
person holding 5g device
How 5G will deliver more for less
December 2, 2021
From improved timing algorithms and sleep modes to the modernization of network hardware and new network protocols, 5G employs several power reduction strategies to manage network energy consumption.
antenna tower
Remote testing gives RF engineers a short-cut to mmWave application development
November 17, 2021
For RF engineers working on mmWave applications, limited access to hardware and test equipment can mean delays, cost and complexity. Remote testing over a secure internet connection lets engineers jump directly to application development.
digitally connected city
The 5G interconnect design challenges and their solutions
October 14, 2021
Avnet spoke with Molex Global Product Manager Mike Hansen about the role copper interconnect is playing in the development of the next high-speed cellular network.
100GHz+ sign with digital globe in the background
Beyond millimeter wavelengths, the terahertz domain awaits
October 13, 2021
Realizing the potential of terahertz frequencies will require enormous advances in technologies from semiconductors through network design.
woman using mobile device in remote location
What to know about electromechanical interconnects for 5G systems
October 12, 2021
High-performance radio frequency, input/output and board connectors are helping developers meet the challenge of 5G. Designed for mmWave and PAM-4 signals in the fronthaul of the network, engineers can use them to improve signal integrity.
skull with 5G around it
No, millimeter-wave 5G is not ‘dead’
October 12, 2021
5G will require a new network design in which smart repeaters, advanced software and algorithms, digital beamforming, and other techniques allow millimeter-wave signals to permeate RF-restrictive environments.
waves in the sky
The future of 5G depends on software-defined radio
October 11, 2021
5G is a technological moving target. If designers had to rely only on hardware to make those changes, it’s possible that 5G would be far too expensive or technically impossible to deploy. That’s where SDR comes in.
heavy traffic
How 6G networking will solve your city’s traffic problems
October 11, 2021
6G networking and self-driving cars could make traffic congestion a thing of the past.
woman's face profile view and digitial face profile view
As 5G evolves, 6G takes aim at Internet of Everything
October 8, 2021
Work on 6G is already underway to define what the standard will do and how it will do it. If 5G is about enabling the Internet of Things (IoT), 6G is about enabling the Internet of Everything – including you.
First1 Last  Results Per Page: 30 6090All