minized-speedway-design-workshops

Display portlet menu

MiniZed SpeedWay Design Workshops™

01 Nov 2017 - 30 Jun 2018

Multiple Dates / Locations


Avnet LogoXilinx logoTE ConnectivitySpeedWay
 

The MiniZed SpeedWay Design Workshops help engineers jump start the development of single-core Xilinx® Zynq®-7000 All Programmable SoC devices using the Avnet MiniZed Zynq SoC development board, a cost-optimized prototyping platform for embedded vision and Industrial IoT systems.

These one-day instructional programs will train customers on the latest design flows using Xilinx’s Vivado® Design Suite through a mix of lecture and interactive labs.

For designers new to Xilinx SoC technology and tools, or those looking to brush up their skills, Avnet will offer two introductory courses: Developing Zynq Hardware and Developing Zynq Software.

More experienced designers can choose from two advanced course offerings: Integrating Sensors on MiniZed with Petalinux and A Practical Guide to Getting Started with Xilinx SDSoC Development Environment.

online courses chalkboard

 

Event Agenda

Developing Zynq Software

In the Developing Zynq Software Speedway, you will be introduced to Xilinx SDK and shown how it offers everything necessary to make Zynq software design easy. This class will cover these capabilities, including BSP creation, built-in drivers, example C code, interrupts, debugging, flash programming, I2C interface between a TE connectivity Pmod, and where to get more help.

Developing Zynq Hardware

In the Developing Zynq Hardware Speedway, you will be introduced to the single ARM Cortex –A9 Processor core as you explore its robust AXI peripheral set. Doing so you will utilize the Xilinx embedded systems tool set to design a Zynq AP SoC system, add Xilinx IP as well as custom IP, run software applications to test the IP, and finally Debug your embedded system.

Integrating Sensors on MiniZed with PetaLinux

From within an Ubuntu OS running within a virtual machine, learn how to install PetaLinux 2017.1 and build embedded Linux targeting MiniZed. In the hands-on labs learn about Yocto and PetaLinux tools to import your own FPGA hardware design, integrate user space applications, and configure/customize PetaLinux. Use Xilinx SDK tools to develop/debug user applications and use example application code to capture data from a TE Connectivity HTU21D I2C sensor. Where service is available, an Internet of Things (IoT) application will be used to publish the sensor data periodically to the cloud using the MQTT protocol. Source code for the user applications are included with the hands-on labs for you to leverage as a launch point in your custom design.

A Practical Guide to Getting Started with Xilinx SDSoC

Using proven flows for SDSoC, the student will learn how to navigate SDSoC. Through hands-on labs, we will create a design for a provided platform and then also create a platform for the Avnet MiniZed. You will see how to accelerate an algorithm in the course lab. This experience should give you the background to assist you in developing custom platforms with custom algorithms, accelerated by SDSoC.

North American Locations

Location: Multiple locations

Time: 8:30 A.M. - 4:30 P.M.

Novi, MI

  • Developing Zynq Software 6/6
  • Developing Zynq Hardware 6/7
 

Events

On-line
Asia Pacific - coming soon
Europe – EBV - coming soon

Europe – Avnet Silica

 

Prices & Information

Full-day workshop, MiniZed board and TE Connectivity Pmod: $155.
Additional full-day workshops, or a full-day workshop for attendees who have a MiniZed board*: $59.

*For attendees who have a MiniZed board, the TE Connectivity Pmod will be provided at the first course they attend. Attendees must have a laptop, MiniZed board and TE Connectivity Pmod to participate in the workshop labs. Prices may vary across regions.

Please click on Register for more information.

 

Register

Register

minized-speedway-design-workshops

Display portlet menu

RELATED EVENTS

What Can I Do with Programmable Logic?

22 Aug 2018 - 22 Aug 2018
Webinar

Join element14 and learn how programmable logic can be useful, powerful, and flexible for circuit applications.

Xilinx, Avnet, Webinars

Design Made Easy with Xilinx

11 Jul 2018 - 11 Jul 2019
Webinars

The IoT Data Journey: Connecting the points from the Edge to the Cloud

19 Jan 2017 - 19 Jan 2018
Webinar

The fundamental requirement for enabling the promise of the Internet of Things (IoT) are interoperable connections between the various sensors at the edge to a gateway and up to and back from the cloud. This Avnet IoT University course is designed to help you make sense of it all.