minized-speedway-design-workshops

Display portlet menu

MiniZed SpeedWay Design Workshops™

01 Mar 2018 - 30 Jun 2018

Multiple Dates / Locations


Avnet LogoXilinx logoSpeedWay

 

 

 

The MiniZed SpeedWay Design Workshops™ help engineers jump start the development of single-core Xilinx® Zynq®-7000 All Programmable SoC devices using the Avnet MiniZed™ Zynq SoC development board, a cost-optimized prototyping platform for embedded vision and Industrial IoT systems.

These one-day instructional programs will train customers on the latest design flows using Xilinx’s Vivado® Design Suite through a mix of lecture and interactive labs. The Workshops will be held in more than 10 cities in China.

Event Agenda:

Developing Zynq Software

In the Developing Zynq Software Speedway, you will be introduced to Xilinx SDK and shown how it offers everything necessary to make Zynq software design easy. This class will cover these capabilities, including BSP creation, built-in drivers, example C code, interrupts, debugging, flash programming, I2C interface between a TE connectivity Pmod, and where to get more help.

Developing Zynq Hardware

In the Developing Zynq Hardware Speedway, you will be introduced to the single ARM Cortex –A9 Processor core as you explore its robust AXI peripheral set. Doing so you will utilize the Xilinx embedded systems tool set to design a Zynq AP SoC system, add Xilinx IP as well as custom IP, run software applications to test the IP, and finally Debug your embedded system.

Integrating Sensors on MiniZed with PetaLinux

From within an Ubuntu OS running within a virtual machine, learn how to install PetaLinux 2017.1 and build embedded Linux targeting MiniZed. In the hands-on labs learn about Yocto and PetaLinux tools to import your own FPGA hardware design, integrate user space applications, and configure/customize PetaLinux. Use Xilinx SDK tools to develop/debug user applications and use example application code to capture data from a TE Connectivity HTU21D I2C sensor. Where service is available, an Internet of Things (IoT) application will be used to publish the sensor data periodically to the cloud using the MQTT protocol. Source code for the user applications are included with the hands-on labs for you to leverage as a launch point in your custom design.

A Practical Guide to Getting Started with Xilinx SDSoC

Using proven flows for SDSoC, the student will learn how to navigate SDSoC. Through hands-on labs, we will create a design for a provided platform and then also create a platform for the Avnet MiniZed. You will see how to accelerate an algorithm in the course lab. This experience should give you the background to assist you in developing custom platforms with custom algorithms, accelerated by SDSoC.

Contact Us

 

Beijing

+86 10 8414 8118

Qingdao

+86 532 8097 0718

Chengdu

+86 28 8652 8262

Shanghai

+86 21 3367 8387

Chongqing

+86 186 0235 0055

Shenyang

+86 189 0400 8421

Fuzhou

+86 591 8771 0381

Shenzhen

+86 755 2658 4925

Guangzhou

+86 20 6109 6913

Suzhou

+86 512 6956 7753

Hangzhou

+86 571 8580 0912

Xian

+86 29 8835 6518

Nanjing

+86 25 8483 8138

 

Learn More

minized-speedway-design-workshops

Display portlet menu

RELATED EVENTS

Horti Asia 2018

22 Aug 2018 - 24 Aug 2018
Thailand

At the sixth edition of Horti ASIA, the region’s largest trade exhibition for Horticulture in Asia, Avnet will be showcasing our Smart Agricultural solutions at booth C20, C22. We will be partnering with Osram, STM and Quectel to showcase the latest smart technologies.

Xilinx, Avnet, Webinars

Design Made Easy with Xilinx

10 Jul 2017 - 10 Jul 2018
Webinars

bnr-maxim-analog-deep-dive

Mobile World Congress Shanghai 2018

27 Jun 2018 - 29 Jun 2018
Shanghai

Mobile World Congress Shanghai, Asia’s premier mobile industry event, features a cutting-edge product and technology exhibition, a thought-leadership conference, and outstanding networking opportunities.