leveraging-the-range-of-sub-1-ghz-technology-to-connect-ultra-low-power-sensors-to-the-cloud

Display portlet menu

Leveraging the Range of Sub-1 GHz Technology to Connect Ultra-low Power Sensors to the Cloud

25 Jan 2017 - 25 Jan 2018

Webinar


There are so many wireless technologies one could use to connect sensor networks to the cloud. It becomes much more difficult to connect these networks to the cloud when you need longer range than just a few 10s of meters or in the use case where networks contain 100s of sensors.

In this presentation we will discuss:

  • The different characteristics of low-power sensor networks
  • The different architectures of a potential solution
  • Which wireless connectivity technology would fit each of the architectures?
    • We will cover: Wi-Fi®, ZigBee®, Thread, 6LoWPAN, Sub-1 GHz and Bluetooth® low energy
  • The specific advantages and disadvantages of using Sub-1 GHz technology
  • The required building blocks to create a Sub-1 GHz sensor network
  • Review Sub-1 GHz products that can connect sensors to the cloud
  • How to get started with TI sensor to cloud kit.

Event Details

Date: Wednesday, January 25, 2017
Time: 2:00pm ET / 11am PT
Available on demand until January 2018

REGISTER NOW

leveraging-the-range-of-sub-1-ghz-technology-to-connect-ultra-low-power-sensors-to-the-cloud

Display portlet menu

RELATED EVENTS

No related events found