ecosystems-a-critical-component-to-successfu-development-of-iot-applications

Display portlet menu

Ecosystems: A Critical Component to Successful Development of IoT Applications

11 Apr 2017 - 11 Apr 2018

Webinar


IoT applications require some development expertise that is significantly different from those required in a traditional embedded application. For example, the UI will typical reside on a mobile device rather than on the device itself. Most obviously, the device will need to connect to an IoT platform, which in turn will collect and analyze data. In addition, the IoT is encouraging many companies with no previous embedded development background to investigate embedded sensor-based solutions. As a result, embedded system integrators and product design houses are also an important component an IoT.

In this session, we will look at various IoT application developments flows and examine the underlying ecosystem required to support them, as well as understand the diversity of choice of IoT platforms and mobile SDKs that are required to support a broad range of IoT applications.

Event Details

Date: Tuesday, April 11, 2017
Time: 02:00 PM Eastern Standard Time
Duration: 1 hour

Available through April 2018

Register Now

ecosystems-a-critical-component-to-successfu-development-of-iot-applications

Display portlet menu

RELATED EVENTS

No related events found