Customising and optimising antennas with materials science and manufacturing techniques

Display portlet menu

Customising and optimising antennas with materials science and manufacturing techniques

In an increasingly connected world, performance demands on antennas are greater than ever. With wireless devices constantly shrinking, the antennas’ allowable size and weight is rapidly reducing, while demands for lower power consumption increase so that battery powered devices can last longer between charges. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a trade-off between performance attributes.

The most important relationship governing small antenna design is the link between size, gain and bandwidth; while it’s possible to optimise a design for any of these parameters, the trade-offs at play mean that they can be balanced but all three can’t be optimised in the same design. For example, if we widen the bandwidth (lower the quality factor, Q), the antenna would have to be bigger. If we reduce the gain (reduce the efficiency), we can increase the bandwidth. And so on.

Some of the ways that manufacturers have tried to bend the rules include integrating multiple antennas into a single package to save space. This results in smaller, cheaper and lighter components, but at the expense of efficiency and power consumption. Tuneable antennas are another idea – if only one part of the band needs to be covered at any one time, we can make a smaller, narrower band antenna and dynamically tune it to the required frequency. Again though, power consumption will suffer.

The latest techniques for optimising antennas’ size and bandwidth while preserving power consumption performance include developing new, higher permittivity materials and optimising designs using 3D shapes and low loss metallisation.

Custom Materials

An antenna’s substrate material has a huge effect on its performance. If permittivity and permeability of the material can be increased (perhaps by using new specially-designed robust ceramics) more bandwidth can be achieved in a smaller volume.  And if the permittivity of the material can be varied throughout its volume, it can also be used to ‘focus’ waves, another way to cheat the physical constraints and make thinner components. 

TE custom composite materials

TE Connectivity’s custom composite materials are typically a combination of a polymer material, chosen for its processing properties (mechanical, chemical and thermal), mixed with a metal oxide filler material, which is responsible for the dielectric properties of the composite. These filler materials are specially engineered to have as high a permittivity as possible. To create custom antennas, the right materials and their relative proportions are selected to yield the desired performance. The two materials can then be physically mixed to create the substrate, either by stirring filler particles into melted polymer, or by laminating the materials in alternating layers, or by 3D printing to produce exotic shapes.

Metallisation

As well as the substrate, the metallisation of antennas also has a big effect on performance. Three broad techniques are commonly used.

Formed metal antennas are made by stamping and bending sheet metal, resulting in high conductivity and high throughput devices. However, this method can’t create the 3D shapes needed for today’s more complex designs. It can also be expensive to revise designs, as new tooling is required each time.

MID (moulded interconnect device) antennas rely on plating metal onto a carrier to form a conductive surface, and there are many different ways of doing it. The substrate can simply be moulded, with a catalyst that allows plating onto that area applied via two-shot moulding. Moulding creates high conductivity antennas, though expensive tooling is required to create the moulds.

An alternative to moulding is Laser Direct Structuring (LDS), which uses a substrate that contains the plating catalyst. The catalyst in the plastic is activated via laser, in the specific areas where metallisation is required, so the metal antenna shape is formed during plating. This method is an entirely digital process, using the output from CAD programs, so there’s no tooling expense, but adding the catalyst to the resin has a cost penalty.

Printing conductive ‘inks’ in pre-defined patterns is another metallisation technique, which can be used with a wide variety of substrate materials. The inks are silver, tin or copper particles mixed with an organic binder and solvent, so conductivity is generally lower than for formed or plated metal. However, the ink formulation and thickness can be tailored to conductivity, adhesion, and environmental stability requirements. 

TE Connectivity metallisation techniques

The easiest printing method is screen-printing, which requires some tooling but this is at very low cost. Feature sizes as small as 50µm can be achieved this way, with a thickness of 10-30µm. Pad printing, essentially rubber stamping, can produce thinner layers, while computer-controlled inkjet printing can be used on 2D or 3D shapes at the expense of thickness.

The right combination of materials and techniques can produce antennas that push the boundaries of size, gain and bandwidth for the next generation of connected electronic products. TE Connectivity has many years’ experience designing and optimising substrate materials and manufacturing techniques to produce custom antennas. If you have any questions about the options available to you, visit the Ask an Expert page to get in touch with one of our field applications engineers.

Written by

Martin Keenan

As Technical Manager, Martin is responsible for marketing strategy across IP&E, power and battery products into key market segments. Martin has over 15 years' experience in electronics having begun his career at Nortel Networks, and since occupied roles at RS Components, Avnet and Altera.

Customising and optimising antennas with materials science and manufacturing techniques

Display portlet menu

RELATED ARTICLES

Future proofing lighting systems with Bluetooth

The lighting industry is not short of options for digital connectivity, but what it needs is a stand...

Choosing the right wireless technology for your IoT end-device

Wireless communications will connect the IoT, but it’s not quite as straightforward as adding a Wi-F...

Let your home do the work so you don't have to

Today, we need to interact with connected products in the home deliberately. But it does not have to...

Engineering Services

Ask an expert

Have a question? Our regional technical specialists are on hand to help