3-ways-All-Programmable-SoCs-create-new-opportunities-for-designers

Display portlet menu

3 ways All Programmable SoCs create new opportunities for designers

Two men and woman reviewing technology products.

Usually, two heads are better than one. Yet sometimes, they introduce conflicting perspectives and priorities.

Two heads means two places need processing power to handle data. Two heads with varied performance have two different effects on the final product. Plus, two heads means two new places with constantly changing technology, which hits software designers especially hard.

In the growing market of embedded vision, there’s a need to not only rapidly scale to compete but to also be ready for machine learning’s effect on the space. That’s all while keeping up with lightning fast design cycles. Luckily, that’s also where FPGAs merge two heads into one: all the processing power is happening on hardware. Instead of needing an external operating system, FPGA rewires the chip to do whatever you need—without running a software application.

This meeting of the minds means there are several opportunity areas for designers when it comes to an “All Programmable” environment for embedded vision: power efficiency from no OS, flexibility due to premade kits and a variety of applications enabled by a suite of cost-optimized devices.

No external OS, no problem

All Programmable solutions feature field programmable gate arrays, ICs that are configured post-manufacturing. This allows FPGAs to operate software applications out of a hardware implementation. In other words, a hardware system is dedicated to processing logic, so it doesn’t need an operating system

One of the biggest benefits of this for engineers is power efficiency. Because each processing path is parallel, operations aren’t all competing for the same processing resources. For embedded vision solutions, that means processing images in real time and turning those into actionable data that can stop a car on a dime or report safety data in an industrial factory—a big differentiator.

Multiple levels of hardware and software security also mean that privacy concerns are lowered while you are taking advantage of ARM® and FPGA architecture.

Hardware flexibility speeds time to market

All Programmable reference designs and hardware kits are bundled and ready off the shelf to customize to a specific engineering need. These bundles help speed your time to market.

No need to be an overnight expert in emerging technologies with deadlines looming. Peripherals like USB 2.0, Gigabit Ethernet and SD/SDIO can all be adapted on the processing system. Accelerators can be added to existing programmable logic allowing quick adaptations of kits to a lengthy list of applications. Despite integrating CPU, DSP, ASSP, and mixed signal functionality onto one device, dedicating hardware to processing logic reduces unnecessary power consumption, too.

While there’s less power needed, however, these bundles still deliver all the performance required depending on the cores, memory and application.

Embedded vision applications are nearly limitless

With a variety of cost-optimized devices with up to 866MHz cores and mid-range devices with up to 1GHz of core processing and from 1.8Mb to 26.5Mb of memory respectively, there’s a strong price-to-performance ratio. This means there’s a version of “All Programmable” that can work in a variety of high-end control applications.

  • Automotive: Autonomous driving depends on embedded vision to monitor drivers, the road and environment to eventually create safer roads.
  • Medical: Machine vision is crucial in treatment tools for hospitals, helping to create better diagnoses by doctors and more efficient scanners and x-ray machinery.
  • Industrial: Embedded vision powered by All Programmable SoCs can crop up in robotics, machine tools as well as conveyor, compressor, fan and pump controls across factory applications.

Still not convinced? Learn more about how embedded vision turns complexity to clarity.

Related Articles
interior of autonomous car
The State of Automotive Only Starts with Autonomous Driving
March 6, 2020
Learn how the state of automotive spans a variety of applications, from electrication to in-cabin AI.
view from autonomous vehicle as it interprets street signs
Somewhere Between the Flintstones and the Jetsons
March 6, 2020
Learn more about developing adaptable automotive automation with Xilinx
man using tablet computer
Specialists vs. end-to-end partners: the pros and cons for developers
March 27, 2019
Getting a product to market requires more than just the right idea; it also needs the right partner.
person holding superimposed globe with IoT symbols
Reimagining the ‘things’ of IoT
By Bill Amelio   -   February 28, 2019
While our collective vision for IoT’s impact on the future is grand in scale, it is still too easy for companies to get distracted by the minutiae of our present day IoT challenges.
Engineer participating in online community on desktop computer
In their words: Benefits of the world’s biggest engineering community
September 5, 2018
In the summer of 2018, Avnet celebrated a major milestone: 1 million community members across Hackster.io and element14. Here's the value of these communities from the members themselves.
Robotic hand touching laptop keyboard
Xilinx SoCs and the reVISION Stack Accelerate Embedded Vision Integration
May 4, 2018
See how designers can capitalize on the power and efficiency of Xilinx's Zynq Ultrascale+ MPSoC devices to implement designs using Avnet's Embedded Vision Kits.
Graphic of a green car flying in the air
Autonomous vehicles are the future
April 9, 2018
Autonomous vehicles do not just replace the driver, helmsman or pilot, but have the potential to create completely new business models worth billions.
Two young men and young woman looking at tablet computer in datacenter
IoT Technology 101
By Christian Curtis   -   March 6, 2018
Learn what’s in market today for IoT and what innovations are ahead.
futuristic automobile interior
How all programmable technology revolutionizes embedded vision
December 14, 2017
Autonomous driving is just the start of EV solutions. Learn how all-programmable is revolutionizing embedded vision.
yellow key imbossed on micromicrochip attached to circuitboard
Circuit Protection: Helping Drive Reliability and Longer Life
December 8, 2017
The primary concerns of engineers designing mobile devices connected to the IoT remain device functionality, performance and feature set. With more devices connected to the IoT intended for long life, remote operation circuit protection increasingly
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
Using Programmable Logic to Build Power-Efficient Systems
March 8, 2017
The successful implementation of the Internet of Things (IoT) requires new thinking about how to power connected devices.
blue eye image with green computer pupil
Embedded vision is everywhere! See for yourself
February 20, 2017
Embedded vision technology will soon touch nearly every aspect of our daily lives –- from automatic vacuum cleaners in our homes to augmented-reality applications in our mobile phones and even in the self-driving cars of the future.
Related Events
speedway logo
MiniZed SpeedWay Design Workshops™
Date: January 1, 2019
Location: Multiple Dates / Locations