Industrial automation demands high flexibility

Display portlet menu

Industrial automation demands high flexibility

Display portlet menu

Industrial automation demands high flexibility

dummy Photo
SMARC 2.0 module that was integrated 1:1 as Avnet Integrated
Picture 1 shows a SMARC 2.0 module that was integrated 1:1 as Avnet Integrated IP into an application-optimized board. In the example shown, the schematic of the module and the complete layout (except for the lower left corner) were adopted.

Based on deep expertise and an extensive portfolio of SMARC 2.0, Qseven, COM Express and nanoRISC standard modules, Avnet Integrated offers application-optimized single board computer solutions. These innovative products are designed for industrial applications and are developed and manufactured in-house in Stutensee, Germany.

Industrial products today need to be more than just innovative. To quickly secure revenue, they must be cost-effective and accompanied by a sophisticated go-to-market strategy. In the desire to do this, more and more often standardized computer-on-modules are being used, which can be integrated immediately and offer up to date PC functionality. It’s no wonder then that the embedded computer market is seeing double-digit growth globally, driven by a combination of new and existing applications in industry, transportation, energy technology, building automation, telecommunications and medical technology, not to mention the IoT or Industry 4.0 space.

Varied, scalable and powerful processor modules

Processor modules are ready to use and available in different variants with scalable performance and a variety of interfaces. Depending on your requirements, modules can use COM Express™ (from the PICMG organization), Qseven™ or SMARC 2.0 (of the SGeT). SMARC 2.0 meets today's industry-leading requirements for low-power, energy-efficient embedded modules and is equally designed for ARM / RISC CPUs and x86 processors.

Today’s powerful standard modules run reliably 24/7 and already have sophisticated security functions. No expensive emulators or low-level debuggers are required to develop the embedded system and, even at low volumes, flexible configurations and high individuality of embedded products are possible. When updating or upgrading the system (for example, when a new processor generation becomes available), the module can be easily replaced. Many COM families have long-term availability and are available for up to fifteen years from launch.

 

Custom solutions

As the name implies, the custom carrier board holds all the application-specific functions and the processor module can simply be plugged onto the board via a common standard plug. This is a tried and tested combination which enables the rapid development of modern embedded products. However, a word of caution – for many applications this solution is not appropriate. For example, products with a special mechanical design, or custom shape and size, have no capacity for the combination of carrier board and plugged module. Special surface treatments also cause problems.

For projects with relatively high quantities, however, customer-specific optimizations pay off.  Take industrial automation, which routinely includes products that run to around 5000 pieces per year. In these cases, Avnet Integrated relies on a single board (SBC) solution that reuses the design of the standard processor module.

Customized single board computers need a consistent platform and comprehensive range of building blocks within a short time and with optimized costs. At the heart of the single board solution is a standard module, selected according to the performance data, whose circuit diagram or layout is placed as a macro 1:1 in the carrier board. From a functional perspective, this corresponds to a module carrier board solution and has the advantages of freer form factor and lower production costs. In this way, the entire software ecosystem of the standard module can be used and only in a few cases further optimization is necessary. And even then, only absolutely necessary macro functions of the customer’s application. The goal is always to use the macro of the module (or parts of it) and customise as little as possible.

Of course, the prerequisite for an optimized single board solution is that many different processor modules are available as macros. Avnet Integrated has over 120 experienced Development Engineers in Aachen, Neufahrn/Munich, Stutensee and Freiburg, working to advance standardized and customer-specific embedded modules. Their task is to translate the ideas and requirements of the customers into a new pioneering product of the future.

SMARC 2.0 module (top left) integrated into an application board.

Picture 2 gives another example of how an existing SMARC 2.0 module (top left) can be integrated into an application board.

Does a single board design pay off? Absolutely.

By using a pre-defined processor module macro, custom development can be implemented at a similar speed and cost of a full custom SBC, as compared to a module/carrier board solution. Because Avnet Integrated provides the macro free of charge and the customer only pays the additional development share, it’s simply a case of assessing the suitability of the individual circuit in their application. The identical core can be evaluated in advance, based on the standard module and state-of-the-art design tools, teamed with an extensive database of building blocks ensure short development times. From here, the prototypes are verified against the specification.

For series production, however, special test equipment must be developed due to a different arrangement of connectors. Software design can be kicked off immediately with an optimized Avnet Integrated Starter Kit and a ‘Board Support Package’ is available to optimize product development time.

Single board solutions

A smart controller, based on an energy-efficient SMARC 2.0 standard module, is a typical application for the single board solution.

The MSC SM2S-AL board family is 82mm x 50mm and designed for low power dissipation between 6 and 12W at high speed (see Picture 3). The compact platform integrates Intel® Atom™ processor technology E3900 in different variants (or alternatively Pentium® and Celeron® processors – code name "Apollo Lake").

MSC SM2S-AL modules provide numerous interfaces such as USB 3.0/2.0, Gigabit Ethernet, PCI Express ™, SATA III and MIPI CSI-2 for connecting cameras. With DisplayPort ++ and LVDS/embedded DisplayPort (eDP) up to three independent displays can be connected. The module integrates a fast yet energy-efficient quad-channel LPDDR4 SDRAM with a capacity of up to 8 GB and optionally a 64 GB eMMC Flash.

Single Board Designs also feature Avnet Integrated's nanoRISC family of compact modules that integrate the latest low-power RISC controllers. The 70 x 50 mm MSC NANORISC-AM335X is based on the Cortex ™ -A8 CPU from Texas Instruments and is designed for the temperature range of -40 to +85 ° C.

The MSX SM2S-AL module family

Picture 3 shows The MSX SM2S-AL module family in 82 x 50 mm short size, which integrates Intel® Atom ™ processor technology E3900

Comprehensive expertise, from development and system integration to manufacturing.

Embedded products are used in virtually all areas of industry, medical technology, in the transportation sector and in building automation and Avnet Integrated’s ability to seamlessly interlink all product phases ensures consistently high quality. Using the critical criteria of Design for Manufacturability (DFM), Design for Test (DFT) and Design to Cost (DTC), our high-performance embedded products are mass-produced for a global market at our facility in Stutensee, Germany and this production facility is impressive for its high degree of automation and use of flexible machines. Modern, fast SMT lines, selective soldering systems and 3D AOI systems are standard, and intelligent shop floor management, functional and structural test systems are also all in use. It’s this full-service offering and critical expertise that gives a competitive edge to customers of Avnet Integrated worldwide.

About Author

dummy Photo
Klaus-Michael Hussmann

  Klaus-Michael Hussmann is a Senior Manager Embedded Solutions at Avnet Integrated...

Industrial automation demands high flexibility

Display portlet menu

Industrial automation demands high flexibility

Display portlet menu
Related Articles
computer screens
Regulatory insights: Are your computer, audiovisual and information technology products ready for the transition to 62368-1?
May 6, 2020
Regulatory certification can be confusing because of constantly changing standards, the complexity of the process and the amount of time needed to properly complete it.
Person placing a component on a board
Does hardware matter?
By Anatoli Lukkarinen   -   March 3, 2020
I believe every IoT and Industrial IoT system designer and software developer should consider the question in the title. Do you?
Processor laying in water
Two methods gaining steam as data center liquid cooling goes mainstream
By Alp Sezen   -   November 24, 2019
Liquid cooled computers for many years have been associated with gaming PC’s and more recently specialized markets like Bitcoin mining.
supply chain concept with vehicles and tools around the work IoT
For Industry 4.0, Reliability Builds on Robust Connections
June 11, 2017
Looking to relieve increasing product complexity and cost pressures, manufacturers are moving toward the next phase of industrial automation envisioned in Industry 4.0. In this concept, smart factories respond instantly to changing workloads to more
Sales clerk at retail display
3 use cases for embedded platforms enabling HMIs and IoT systems
January 22, 2020
Avnet Integrated takes the complexity out of embedding HMIs for demanding markets. In this article, we go through three common examples.
Woman using machinery to modify a display cover lens
Should you chemically or thermally strengthen your glass display cover lens?
August 20, 2019
Durability and safety considerations require the glass to be strengthened (hardened), using either chemical or thermal processes. Chemical hardening is possible with all glass, while thermal hardening is only available for thicknesses up to 3 mm.
An image of the MSC-6B-CFLH board
Highest computing and graphics performance
February 21, 2019
With the MSC C6B-CFLH, Avnet Integrated delivers an extremely powerful COM Express module based on processors from the 8th Generation Intel Core processor family. The high-end board has up to six CPU cores.
man using tablet computer in industrial setting
5 of the best artificial intelligence use cases
January 3, 2019
AI’s upgraded algorithms make predictive analytics, parse data, and help businesses make smarter decisions from the boardroom to the factory floor.
Doctor checking on a patient from a remote patient monitoring device -- artificial intelligence
AI From A-Z: The biggest buzzwords around artificial intelligence
November 28, 2018
Companies across markets from consumer electronics to factory floors are finding power in the introduction of two letters: AI (artificial intelligence).

Industrial automation demands high flexibility

Display portlet menu
Related Events

No related events found