Should you chemically or thermally strengthen your glass display cover lens?

Display portlet menu

Should you chemically or thermally strengthen your glass display cover lens?

Display portlet menu

Should you chemically or thermally strengthen your glass display cover lens?

Woman using machinery to modify a display cover lens

Durability and safety considerations typically require the glass to be strengthened (hardened), using either chemical or thermal processes. Chemical hardening is possible with all glass, while thermal hardening is typically only available for thicknesses over about three millimeters.

Of the two approaches, chemical hardening can make surfaces more scratch resistant, but it only affects the outer surfaces. Thermal hardening, on the other hand, hardens the material throughout, including below the surface. From a safety perspective, thermally strengthened (tempered) glass shatters into smaller pieces with less-sharp edges than untreated or chemically strengthened glass. The type of strengthening used on the glass also affects the types of inks that can be used to print on it.

-- Chemically hardened glass: organic inks are typical, which offer a wider choice of hues compared to ceramic color but less ultraviolet resistance.

-- Thermally hardened glass: requires ceramic color, which is superior in terms of scratch resistance, but because printing is done on the back side of the cover lens, that resistance is only relevant during manufacturing.

Note: While thermal tempering typically requires a minimum thickness of ~3mm, specialized processes enable Avnet to be one of the few suppliers that can offer ceramic colors on glass with thicknesses down to 1.8mm.

Ion-exchange strengthened glass

An option if your device needs a particularly robust cover lens, ion-exchange strengthened (alumino-silicate) glass is created using a chemical process that exchanges the native sodium ions in soda-lime glass for larger potassium ions. The result of that process is denser and more durable glass than other options, enabling lightweight, slim device form factors, especially with bezel-less designs.

This is the technology behind commercial offerings such as Gorilla Glass (made by Corning), Dragontail (made by Asahi) and Xensation (made by Schott). Relatively high cost and minimum order quantity (MOQ) associated with alumino-silicate glass, as well as a maximum thickness of 3mm, have made it less broadly used in the industry than other options for cover lenses.

Improve product form and function with sleek custom touch displays

To meet rigorous user experience expectations for devices, first-rate physical design has become a higher priority than ever before. For products that incorporate touch displays, customization can improve both aesthetics and functionality. Our free white paper addresses some key design requirements related to custom touch displays as well as materials and practices that can help you satisfy those requirements.

Download the Whitepaper

Helpful Links

Should you chemically or thermally strengthen your glass display cover lens?

Display portlet menu

Should you chemically or thermally strengthen your glass display cover lens?

Display portlet menu
Related Articles
Person placing a component on a board
Does hardware matter?
By Anatoli Lukkarinen   -   March 3, 2020
I believe every IoT and Industrial IoT system designer and software developer should consider the question in the title. Do you?
supply chain concept with vehicles and tools around the work IoT
For Industry 4.0, Reliability Builds on Robust Connections
June 11, 2017
Looking to relieve increasing product complexity and cost pressures, manufacturers are moving toward the next phase of industrial automation envisioned in Industry 4.0. In this concept, smart factories respond instantly to changing workloads to more
Sales clerk at retail display
3 use cases for embedded platforms enabling HMIs and IoT systems
January 22, 2020
Avnet Integrated takes the complexity out of embedding HMIs for demanding markets. In this article, we go through three common examples.
SMARC 2.0 module that was integrated 1:1 as Avnet Integrated
Industrial automation demands high flexibility
By Klaus-Michael Hussmann   -   August 22, 2019
Based on deep expertise and an extensive portfolio of SMARC 2.0, Qseven, COM Express and nanoRISC standard modules, Avnet Integrated offers application-optimized single board computer solutions. These innovative products are designed for industrial a
man using tablet computer in industrial setting
5 of the best artificial intelligence use cases
January 3, 2019
AI’s upgraded algorithms make predictive analytics, parse data, and help businesses make smarter decisions from the boardroom to the factory floor.
Doctor checking on a patient from a remote patient monitoring device -- artificial intelligence
AI From A-Z: The biggest buzzwords around artificial intelligence
November 28, 2018
Companies across markets from consumer electronics to factory floors are finding power in the introduction of two letters: AI (artificial intelligence).

Should you chemically or thermally strengthen your glass display cover lens?

Display portlet menu
Related Events

No related events found