Light, Home & Building

EBV - LightSpeed Trends & applications (LC)

Display portlet menu

Light, home and building trends & applications

Indoor lighting

LED lighting with number of advantages can make a difference within our indoor micro worlds and their needs

LEDs are gaining respect to new creative potential for indoor lighting especially in home surroundings , office and shop improving more and more the following main elements: as quality of light, its colour, direction and intensity adapting personal surrounding, task & mood lighting levels for each area of your indoor living place.

Learn More

Outdoor lighting

LED lighting is perfectly suited for outdoor use as they will bring you a number of years of virtually free maintenance service

LED technological ruggedness, low temperature operation and size allows designers to create luminaires in almost any shapes for outdoor use. Their durability is appropriate in applications with strong probability of lamp breakage especially in outdoor areas like industrial areas, gardens, bridges, public transportation objects and stadiums.

Learn More

Street lighting

LED technology is a key element for the future of dynamic traffic managment and street illumination

Wide usage of LED technology in Variable Message Signs (VMS) for traffic guidance and information purposes LED lighting provides better uniformity of illuminance of a street with main task - increasing visibility at night. Optical quality for street illumination and signalisation are used worldwide for safety purposes, better night vision and dynamic traffic management.

Learn More

Show lighting

Bring innovation and customer satisfaction riding on new LED technologies easy adapting personal style and integrity to each event

Various advantages of LED technology will bring you exceptional event lighting design, event production within electonic backup control, staging effects, optimised power solutions, exhibition lighting and an extensive selection of new ideas.

Learn More

LED advantage

The core element of every LED-based lighting system is, of course, the LED itself

While conventional incandescent ‘light bulbs’ heat a piece of metal wire called filament, which not only gets hot but also emits light, LEDs operate on a totally different basis as they use the photoelectric effect. As the colour of the emitted light is directly related to the specific temperature of the filament, the expression ‘Colour Temperature’ is still used today to describe the variations of white light. Find here several good reasons to gain on LED's advantages towards other light sources.

Learn More

Optics

Once the light is emitted from the light source it needs to be directed and guided according to the individual application needs

Proper optics are often just as important part of a good quality product, than other key components like the LEDs and drivers.Suitable high quality optics achieve better beam control by reduction of glare caused by the ”point source” LED and a wide angle intensity distribution. It offers now the possibilities to make more uniform light with different beams and cutoffs. This is needed for illumination standards in many applications such as street lights, aviation lights and medical lights. A good optic also gives a finished look and a protection for the LED.

Learn More

Thermal management

LEDs are temperature dependent

The thermal management of LEDs ensures the reliable operation of the LED, prevents early degradation and optimizes the LED’s optical performance. Operating LED-based lighting systems at high ambient temperatures without proper thermal design may overheat LED packages, eventually lead to short lifespan or device failure in the worst case. This is the reason why thermal management of LEDs is the most critical part within the LED based lighting system, and thus the designer needs to ensure that the LED will never exceed its specific maximum permissible junction temperature.

Learn More

Electronic control

With specific control it is not only possible to activate or deactivate the LED light but also to dim it, to change its warmness/coolness or colours and manage entire ambient scenes

Modern luminaires are asking for more added value like dimming, emergency unit, presence sensor, remote control, etc. where more complex electronic circuitry are required. LED lighting offers several inherent benefits compared to other lighting systems as they can be integrated into the electronic control system which allows control of colour balance and intensity, independent of each other while maintaining colour rendering accuracy. To keep today's development cycles as short as possible there are several EBV ELEKTRONIK suppliers offering intuitive online tools helping you to simplify your design.

Learn More

EBV LightLab

EBV LightLab was created to offer our customers a wide range of measurements on a lighting products portfolio offering the entire range of highly professional devices

The list of the measuring devices includes two integrating spheres for 2π and 4π measurements, a spectroradiometer for reference measurements, a goniophotometer, a light density measuring device and a luxmeter. This product range is complemented by special measurement/evaluation and control software, source meters and multimeters, a thermal camera and supplementary tools.

Learn More