Light, home & building hero banner (HB)

Display portlet menu

Light, Home & Building

Glossary Lightspeed Title (MT)

Display portlet menu

Glossary - light, home & building

Glossary LightSpeed Introduction (LC)

Display portlet menu

As experts in lightspeed market, EBV can help you to recognise the most common terms and abbreviations in the areas of Electronic control, LED basics, Lighting matters, Optics and Thermal:

Electronic control

What is LED DRIVER?

A device that controls the current flow and manages power for an LED lighting product. In some LED applications we understand under term LED Driver also part of the power supply like voltage conversion circuit used between input voltage and required output voltage. According to the type of output we have three groups of drivers: Constant Current (CC) – LEDs are in serial connection and driver delivers precise current value, Constant Voltage (CV)- LEDs are in parallel connection which is ideal for decorative LED strips, this topology is not recommended for dimming and Special Drivers (CC+CV) – which is a bit expensive solution allowing both serial and parallel connections. Beside mentioned there are following important parameters we shall pay attention when choosing LED Driver like Rated Current/Voltage – predefined output current and voltage, Rated Power – output power of the driver and Efficacy – Ratio between output/input power.

Learn More

LED basics

LED is abbreviation for Light Emitting Diode. LED technology stands for Illumination technology.

How does LED emit light?

When a voltage is applied in the forward direction (the direction in which the electrons move) to the LED chip’s pn junction – electrically seen as a diode – free charge(electrons and holes) will be forced to move into the depletion zone. Here, electrons recombine with holes, and some of these recombinations are accompanied by the emission of light. The combinations of materials (mostly for the p- and n-crystal as well as the physical set-up) determine parameters of an LED. Due to the fact that LED light originates from solid state devicesthe expression solid state lighting (SSL)is becoming popular.

Learn More

Lighting matters

Light sources for my lighting solution

Over the years many light sources have been developed and used in many and sometimes very special applications.
These include:

  • Fluorescent TL lamps; generally known as office ‘neon’ lamps.
  • CFL (compact fluorescent lamps); the ‘classic’ replacement for incandescent bulbs as they fit into the old sockets.
  • CCFL (cold cathode fluorescent lamps); mainly used for outdoor ‘neon’ signs and LCD display backlights.
  • HID light (high intensity discharge); typically used for street and stadium lighting as well as for car headlights.
  • LEDs; this very effective lighting technology is mature and provides the lamp designer with new possibilities in terms of the physical and optical construction of the entire lamp. As the operating lifetime of LEDs is between 20,000 and 50,000 hours, which is considerably longer than most lamp operating lifetimes, LEDs are and will be the light source of the future for general lighting applications.
     
Learn More

Optics

Why OPTICs are needed?

Once the light is emitted from the light source it needs to be directed and guided according to the individual application needs. This can be performed by reflection (from metallised or white diffuse surfaces), refraction through prisms or lenses or even absorption by black or structured surfaces. Compared to conventional lamp systems, the optical system of LED lights is about 30% more effective due to lower losses. Therefore it is important to consider the entire optical system within the evaluation process for the efficacy of a lighting system.

Learn More

Thermal

How THERMAL MANAGEMENT works?

The thermal management of LEDs ensures the reliable operation of the LED, prevents early degradation and optimizes the LED’s optical performance. Basically, LEDs follow a very simple rule: The higher the temperature of the LED, the shorter its lifetime. This is the reason why thermal management of LEDs is a must, and thus the designer needs to ensure that the LED will never exceed its specific maximum permissible junction temperature.

Learn More