Training & Events
TechTrends 2020
Date: April 23, 2020
Location: Auberge Du Pecheur, Ponstraat 41, B-9831 Sint-Martens-Latem, Belgium
Embedded Artificial Intelligence / Machine Learning
Date: May 5, 2020
Location: Multiple locations
Webinar - Ultra96 Technical Training Courses
Date: July 7, 2019
Location: Online, On Demand
Artificial Intelligence   Filter By  
AI is changing the game. Whether you're working on systems that act intelligently in a specific domain (narrow AI), or in general (strong AI). Designing those systems is no easy task. Explore our resources to stay up to date in the world of AI trends, technology, and technical expertise.
The brain functions like a machine, or so according to the theory of Marvin Minsky, one of the most important pioneers of artificial intelligence.
KI-Pionier Minsky: Vorläufig tot?
March 4, 2019
Das Gehirn funktioniert wie eine Maschine, so die ­These von einem der wichtigsten Pioniere der ­Künstlichen Intelligenz. Also kann man es nach­bauen – und sich durch ein Back-up des Bewusstseins auf einem Rechner unsterblich machen.
Could our entire life simply be a computer simulation
AI-pioneer Minsky: Temporarily dead?
March 4, 2019
The brain functions like a machine, or so according to the theory of Marvin Minsky, one of the most important pioneers of artificial intelligence. In other words, it can be recreated – made immortal by backing up its consciousness onto a computer.
Mit verschiedenen Ansätzen der Datenauswertung sollen Maschinen intelligent werden.
Neuronale netze simulieren das gehirn
February 27, 2019
Mit verschiedenen Ansätzen der Datenauswertung sollen Maschinen intelligent werden. Im ­Fokus steht dabei nicht nur die Leistungsfähigkeit, ­sondern immer mehr auch eine Flexibilität, wie sie das menschliche Gehirn bietet.
Kognitive Computerassistenten helfen Medizinern bei Diagnose- und Therapieentscheidungen.
Ist KI besser als der arzt?
February 27, 2019
Kognitive Computerassistenten helfen Medizinern bei Diagnose- und Therapieentscheidungen. ­Sie sind deutlich schneller bei der Auswertung von medizinischen Informationen und erreichen ­mindestens die gleiche Präzision.
Cognitive computer assistants are helping clinicians to make diagnostic and therapeutic ­decisions
AI better than the doctor?
February 27, 2019
Cognitive computer assistants are helping clinicians to make diagnostic and therapeutic ­decisions. They evaluate medical­ data much faster, while ­delivering at least the same level of precision.
Artificial neuronal networks are playing a big role
Neuronal networks simulating the brain
February 27, 2019
Machines are being made more intelligent based on a variety of data analysis methods. The focus of these efforts is shifting increasingly from mere performance capability towards creating the kind of flexibility that the human brain achieves.
Artificial Intelligence has enormous potential for improving our lives
AI Smarter than humans?
February 25, 2019
What began in the 1950s with a conference has grown into a ­key technology. It is already influencing our lives today, and as the intelligence of machines increases in the future that influence is bound to spread much more.
KI ist eine Schlüsseltechnologie, die sich in den kommenden Jahren nicht nur maßgeblich auf unser tägliches Leben, sondern auch auf die Wettbewerbsfähigkeit der gesamten Wirtschaft auswirkt.
Ist KI schlauer als der Mensch?
February 27, 2017
Was in den 1950ern mit einer Konferenz der KI-Pioniere John McCarthy und Marvin Minsky begann, ist zu einer Schlüsseltechnologie ­geworden.­ Sie beeinflusst schon heute­ ­unser Leben – und wird es mit steigender Intelligenz der Maschinen in Zu
<<    <    1    >    >>          Results Per Page:  30  60  90  All