Is teleportation possible? | EBV Elektronik

Display portlet menu

Is teleportation possible? | EBV Elektronik

Display portlet menu

Is teleportation possible?

Teleport information from a ground-control station to a satellite in space

In Star Trek, people are simply beamed from one place to another at the push of a button. What sounds like pure science fiction is actually already reality today thanks to quantum physics … At least, at the level of a single photon.

How great would it be if you didn’t have to waste another second commuting or travelling by car, bus, train or plane when instead – just like in Star Trek – you could simply be beamed anywhere you wanted to go at the push of a button? To put it another way, what would it be like if matter could also be transmitted wirelessly just like information can? That will surely remain a pipe dream for the foreseeable future. Or will it?
As it happens, physicists today are already in a position to at least beam the basic characteristics of matter (or “teleport” them, to use the correct parlance of the profession).


In two places at once

The basis for the technology is in one of the most spectacular quantum physics phenomena: entanglement. This describes the characteristic whereby two particles behave not as two independent physical objects, but rather as a single one. Entanglement cannot be understood merely in spatial terms: entangled particles correlate to one another on the basis of their characteristics. If the characteristics of the one particle are changed, this means that the other particle will change accordingly at the same time, irrespective of where it is situated. In the case of light particles (photons), it is possible to generate such entanglement by using a laser array with a special crystal to split a single particle into two photons.
Such entanglement can be used to transmit information from one location to another without any loss of time, or so the theory goes. Every measurement which changes the state of the one particle will result in the state of the other particle being changed immediately, regardless of how far apart the two particles are. This process has been known as “quantum teleportation” for a number of years now.


Incidentally: “Beam me up, Scotty” is doubtless the best-known phrase in Star Trek history, although it was never uttered word-for-word in that exact form by any character throughout the series or its films.


Teleportation across hundreds of kilometres

Last year, Chinese researchers succeeded in using this method to teleport information about the state of photons from a ground-control station to a satellite in space. In theory, it might even be possible to teleport information on the state of a human being in the same way. This would actually enable “beaming” as we know it from Star Trek. For this to work, all you would need to do is decode every single one of a person’s quantum states, send this information to the target location and “imprint” atoms with the same chemical elements.
 

Humans are just too complex

Two major problems are yet to be solved, however. Firstly, a vast amount of energy and extremely complex calculations would be required to teleport a human being. Researchers at the University of Leicester in the UK have crunched some numbers to answer this question: due to the fact that 10 billion bits are required just to describe a single human cell, the data volume for a person of average height and weight would come to around 2.6 x 1042bits – in other words, 2.6 with 42 zeroes behind it. Merely transmitting this information at a cycle rate of 30 GHz would take 350,000 times longer than the existence of our universe.
In other words, you’d be quicker to walk. And even if the rate were to be increased to reduce the duration of travel to a few thousand years, our planet’s energy resources would have been depleted within a single second. Nor would this solve the second problem: what happens to the person at the place of transmission when they arrive at their destination?
According to quantum physics, the original would be deleted and would cease to exist. Who in their right mind would actually be prepared to test a teleportation machine like this? Sadly, in light of all that we know today, it seems extremely unlikely that we will ever be transported to our desired destination simply by uttering the words “Beam me up, Scotty”. Nonetheless, teleportation is well worth all the attention it is afforded, but not for transmitting objects. Instead, quantum physics could be used to create fast computers and achieve lightning-speed data transmission by today’s standards. That’s what you might call wireless communication at its best.

 

****

This article is also available in German language. Click here for the German version.

 

Is teleportation possible? | EBV Elektronik

Display portlet menu

Is teleportation possible? | EBV Elektronik

Display portlet menu
Related Articles
woman with diabetic monitory
Connectivity Among Major Analog Design Considerations in Health Wearables
December 9, 2019
Development of very low powered analog body sensors, digital microcontrollers, and innovative power and battery management circuits are driving the growth of wearable healthcare products.
The rapid growth of the Internet of Things (IoT) is making increasing demands on microcontrollers (MCUs) for both performance and connectivity
Improved Security in IoT Systems
By Christian Krieber   -   November 4, 2019
The rapid growth of the Internet of Things (IoT) is making increasing demands on microcontrollers (MCUs) for both performance and connectivity. Local processing is needed at the edge to perform ever more complex processing of data.
Was nach reiner ­Science Fiction klingt, ist dank der Quanten­physik heute tatsächlich schon Realität.
Ist Teleportation möglich?
February 25, 2019
In den Star-Trek-Filmen werden Menschen einfach per Knopfdruck von einem Ort zum anderen gebeamt. Was nach reiner ­Science Fiction klingt, ist dank der Quanten­physik heute tatsächlich schon Realität.
Das Internet der ­Dinge wird ­zunehmend zur Realität, immer mehr ­Maschinen, Geräte, Gegenstände und letztlich auch Menschen ver­netzen sich.
In eine kabellose Zukunft dank drahtloser Kommunikation
February 22, 2019
Das Internet der ­Dinge wird ­zunehmend zur Realität, immer mehr ­Maschinen, Geräte, Gegenstände und letztlich auch Menschen ver­netzen sich.
Smart Cities leben von einer Vielzahl an Informationen, die von Menschen, Geräten und ­Sensoren übertragen werden.
Smart City Projekte und Technologien
February 21, 2019
Smart Cities leben von einer Vielzahl an Informationen, die von Menschen, Geräten und ­Sensoren übertragen werden.
rückt die ­Energieeffizienz der Wireless-Technologie zunehmend in den Fokus
Höhere Vernetzung, Geringerer Stromverbrauch
February 21, 2019
Mit der explodierenden Zahl an vernetzten Geräten und dem rasant steigenden Datenvolumen rückt die ­Energieeffizienz der Wireless-Technologie zunehmend in den Fokus.
Smart cities subsist on a large amount of information which is transmitted by people, ­devices and sensors
Smart networks for smarter cities
February 20, 2019
Smart cities subsist on a large amount of information which is transmitted by people, ­devices and sensors. A wide range of wireless technologies is used for this purpose, depending on the application in question.
Energy efficiency is becoming increasingly important when it comes to wireless technologies
Higher networking, lower power consumption
February 20, 2019
Due to the explosion in the number of networked devices and the rapidly increasing data volumes, energy efficiency is becoming increasingly important when it comes to wireless technologies.
A vast range of wireless technologies is used to transmit this volume of data securely
The Future of the Wireless Technology
February 14, 2019
The Internet of Thing is increasingly becoming reality. Ever more machines, devices, objects and - last but not least - people are becomig interlinked.

Is teleportation possible? | EBV Elektronik

Display portlet menu
Related Events
TechTrends 2020
Date: April 23, 2020
Location: Auberge Du Pecheur, Ponstraat 41, B-9831 Sint-Martens-Latem, Belgium
Secure your Hardware & Application Seminar with NXP
Date:
Location: Germany, Kaarst, EBV Elektronik GmbH & Co KG - Office Kaarst, An der Gümpgesbrücke 7, 41564 Kaarst