spare-tire-of-3d-facial-recognition

Display portlet menu

spare-tire-of-3d-facial-recognition

Display portlet menu

Can the “spare tire” of 3D facial recognition move into the mainstream?

facial recognition software assembling the face of a young man

The 3D facial recognition market is expanding rapidly. According to a forecast from Trend Force, the 3D sensing market will grow exponentially, reaching $10.89 billion in 2020 and $18 billion by 2023. The penetration rate of 3D facial recognition in the smartphone market is also expected to increase from 2.1% in 2017 to 28.6% in 2020.

The technology of choice for facial recognition

Although the pie is undoubtedly sweet, whether you’re able to “have your cake and eat it too” depends on whether or not that you have the technical cutting edge. Currently, there are two main technological options for 3D facial recognition in smartphones – one is a structured light solution, and the other is a time-of-flight (ToF) solution.

Of the two options, the most market-ready and commercially viable is the structured light solution. The widespread commercial application of structured light technology can be largely attributed to Apple, who took the lead in abandoning fingerprint authentication and adopting structured light 3D facial recognition technology for its iPhone X. Market feedback went from initial curiosity and doubt to the current total acceptance. Clearly, this technology can meet the criteria of picky users. Since Apple's move was presumably made after trialing many options, it should be a safe bet for other manufacturers. Thus, structured light 3D facial recognition already has many takers.

On the other hand, the ToF solution is regarded as a "spare tire." Nobody pays much attention to it. However, that can be partly attributed to its latecomer status. Latecomers have to work much harder than newcomers at proving themselves. Hence for the past two years, ToF has been trying very hard to prove itself.

Can the “spare tire” of 3D facial recognition move into the mainstream?

Figure 1. Schematic diagram of 3D face recognition scheme for ToF mobile phone (Image source: Internet)

In terms of its working principle, 3D structured light technology uses a near-infrared laser to project light with certain structural features onto the object to be photographed, and then collects it in a special infrared camera. Since the light of the structural features changes in accordance with the depth of the object, depth information can be obtained by comparing and calculating the acquired phase of the image, thereby obtaining the 3D structure of the measured object.

When ToF technology is used for 3D facial recognition, the surface source continuously emits light pulses. When light is reflected upon encountering an impermeable object, the light source can be measured by measuring the time the reflection takes to reach the receiver, thereby enabling the distance from the object to be calculated and obtaining a 3D image of the object that has “depth.”

In theory, structured light technology is superior in accuracy and resolution, but ToF has many advantages that cannot be denied. For example:

  • Relatively speaking, structured light technology requires more post-processing after obtaining information about the image to calculate the depth while ToF measurement is more direct and requires no post-processing. With ToF, the delay is shorter and the response is faster.
     
  • The ToF solution, which does not require post-processing, also saves costs and power consumption associated with the processor, significantly reducing the technical threshold.
     
  • The ToF solution requires fewer components and is smaller, making it more popular in mobile applications with space constraints and also more practical for mechanical devices.
     
  • ToF is less susceptible to ambient light interference than optical solutions such as structured light.

 

  Structured light ToF

Basic principle

Single camera stripe and speckle projection coding

Infrared light reflection time difference

Response time

Slow

Fast

Performance in low light environments

Good (depends on the light source)

Good (infrared laser)

Performance in strong light environments

Weak

Medium

Accuracy

Medium

Low

Resolution

Medium

Low

Recognition distance

Short, affected by the speckle pattern

Medium (1-10 meters), limited by intensity of light source

Hardware BOM cost

High

Medium

Software complexity

Medium

Medium

Power consumption

Medium

Low

Table 1. Comparison of technical characteristics of structured light and ToF


After comparing the characteristics of the two technologies, some people have concluded that structured light technology is more advanced and more suitable for static use situations, making it the first choice for facial recognition in front-facing cameras on smartphones. On the other hand, since the ToF solution has lower noise at long distances, it is thought to be more suitable for dynamic use situations. Thus, ToF is deemed more suitable for rear camera lens placement on mobile phones, where it can show its skills in AR and VR applications.

For ToF technology, AR and VR are still far into the future, while front-facing camera facial recognition is already an existing market waiting to be tapped. In the 3D facial recognition market, clashes between structured light and ToF technology are inevitable.

ToF technology is already here

Today, ToF technology suppliers are fully prepared to tap the growing market and win over future users. For example, Infineon's REAL3™ series of 3D image sensors is an advanced solution that is ready for commercial applications.

Can the “spare tire” of 3D facial recognition move into the mainstream?

Figure 2. Infineon REAL3™ series 3D image sensor system block diagram (Image source: Infineon)


Given that it has ToF's technical advantages, REAL3™ offers many more features of its own. For example:

  • The REAL3™ series supports a minimum of 38,000 depth points, each of which has a measurement depth of millimeters and an error rate of less than one in a million, making it safer and more reliable.
  • For resisting ambient light interference, REAL3™ uses patented SBI (Suppression of Background Illumination) technology to instantly eliminate all irrelevant signals for excellent camera performance.
  • The camera module of the RREAL3™ series only has two main components – the REAL3™ image sensor and lighting circuit. No mechanical base line between the two is required, thereby greatly simplifying assembly and debugging while enhancing mechanical stability and mechanical strength.
  • Naturally, this type of photographic lens module is also smaller, only 11mm × 7mm × 4mm in size, thus saving valuable smartphone space.
  • In addition, REAL3™ has an integrated eye-safety circuit that meets safety requirements and reduces the BOM, unlike other solutions that require external eye-safety circuits.

Can the “spare tire” of 3D facial recognition move into the mainstream?

Figure 3. Infineon's REAL3™ series 3D image sensors make the entire ToF camera module simpler and more robust (Image source: Infineon)

REAL3™, based on ToF technology, has already met with success in commercial applications. The front camera module of the LG G8 ThinQ mobile phone uses the REAL3™ solution. Infineon also revealed that the next-generation REAL3™ ToF image sensor will use advanced microlens technology to increase sensitivity and further optimize size and power consumption.

Of course, compared with structured light technology, the latecomer ToF still has a long way to go in terms of technical fine-tuning, commercial verification and supply chain support. However, well-known analyst Ming-Chi Kuo predicts that Apple is expected to adopt ToF technology in an iPhone in 2019. If this rumor becomes a reality, it will be a major boon for ToF's commercial expansion. Imagine, the “spare tire” of 3D facial recognition turns mainstream – now that would make for a very interesting scenario.

spare-tire-of-3d-facial-recognition

Display portlet menu

spare-tire-of-3d-facial-recognition

Display portlet menu
Related Articles
bluetooth speaker with IoT icons arround it
Will the smart speaker market cool off?
January 20, 2019
The news at the start of this year that Tencent had suspended its smart speaker project ‘Tingting’ sent chills down the spines of many. What’s more, statistics show that half of the 50 Chinese companies that had invested in smart speakers when
doctor taking patient's blood pressure
Choosing A Pressure Sensor
October 12, 2018
Pressure sensors’ accuracy is an important performance attribute, which is typically given as a percentage of full-scale pressure over a certain temperature range. Some sensors also exhibit hysteresis, non-repeatability and non-linearity, which sho
cityscape
MEMs Revolutionizes Sensor Landscape
July 19, 2018
Until fairly recently—roughly 15 to 20 years ago—sensors for ubiquitous physical parameters such as pressure, motion and magnetic fields were relatively large, costly, power-hungry and electrically incompatible with standard circuitry.
robot hand and human hand touching digital screen from oposite sides
How to create a touch screen you can “feel”
August 9, 2017
Haptics is an excellent “companion” for touch screens in that it gives users a “sense” of “touch”. Although the main sources of external information are visual and auditory, many users agree that the tactile stimulus enabled by haptics ac
disposal bins (recycle, trash, etc) on the side of a building with IoT icons hovering over them
What Can We Do About Waste Sorting?
August 1, 2017
With the aim of easing the pain and facilitating the process of waste sorting, intensive research and development is focused on smart rubbish bins. In the waste disposal process, from disposal, collection and transport to treatment, rubbish bins conn
snowboarder in yelow jacket and blue pants sits on snow overlooking the mountains
Monitoring Impact Levels in Sports
April 20, 2017
Concussion, also known as mild traumatic brain injury (MTBI), is a very serious topic in the world of sports today.
black smart watch
Wearables: Tracking, Computing and Making Sense of Context Awareness
April 15, 2017
Wearable devices are moving quickly from concept to reality based on evolving technologies such as sensor fusion, communications and vision. Wearables have evolved to become perceptually aware agents that learn through users’ experiences, activitie
smart watch with IoT icons on the screen
Wearable Electronics: Four Approaches to Implement a Sensor Hub and Save Power
March 17, 2017
As more sensors are added to nearly every electronic device including smartphones, tablets and wearables, more power is needed to run sensor data and turn it into useful information.

spare-tire-of-3d-facial-recognition

Display portlet menu
Related Events

No related Events found