Internet of Things: Designing Sensor-Based Devices with Coin Cell Batteries

Display portlet menu

Internet of Things: Designing Sensor-Based Devices with Coin Cell Batteries

Display portlet menu

Internet of Things: Designing Sensor-Based Devices with Coin Cell Batteries

nurse checking person wearing health monitoring system on wrist

A popular vision of the Internet of Things (IoT) is that it will comprise billions of sensors gathering information about their local environment and transmitting that data back to servers in the cloud. Such data will be compiled, analyzed and shared by server-based applications that will use it to do everything from controlling irrigation and managing traffic congestion, to monitoring diabetics’ blood sugar levels and automatically re-ordering stock when store shelves run low.

Turning this vision into reality requires engineers to design a new generation of sensors that are unobtrusive, low maintenance and inexpensive. Devices that are compact and lightweight, with relatively simple circuitry and wireless connectivity fit the bill. While energy-harvesting techniques are continually improving, constantly active IoT sensors will probably demand the more reliable resources of a battery. However, constraints on the size and weight of such sensors restrict the size of the power source, in turn limiting the battery’s capacity. And just to make the designer’s challenge a little harder still, sensors in the IoT will require long battery life to keep maintenance manageable.

Enter the Coin Cell Battery

Designers of mobile products are experienced in coming up with circuits that work efficiently and in choosing power-frugal components to ensure long battery life. But engineering tiny, battery-powered wireless sensors is an altogether tougher challenge.

However, designers can call on the experience of original equipment manufacturers (OEMs) that have fabricated compact wearable sensors, such as heart rate monitors (HRMs), that use wireless technology to send information to a sports watch. These products employ many of the technologies that will be needed for ubiquitous IoT sensors. The CR2032 coin cell battery (using lithium/manganese dioxide — Li/MnO2 — chemistry), which initially came to prominence as a common choice for electronic watches, is the popular choice for powering these wearable sensors. Manufacturers of the prevalent CR2032 coin cell battery include Duracell, Eagle Picher, Energizer, Maxell, Panasonic, Philips, Rayovac and Vinnic, among others.

Panasonic’s version of this battery, which is typical of the type, offers a nominal voltage of 3 V and nominal capacity of 225 mAh before the battery is exhausted. Panasonic advises a maximum continuous load of 0.2 mA from this battery. Research by others shows that the maximum transient current draw for a CR2032 coin cell is about 40 mA if the battery is not to be seriously compromised. While the nominal capacity provides a guide regarding the life of a CR2032 coin cell in a wireless sensor, there are many influences on how the battery will actually perform in practice. For example, a nominal capacity of 225 mAh for a device drawing a continuous load of 0.2 mA will provide 2 V or greater for approximately 47 days. But few products would exhibit this performance in the field.

CR2032 Panasonic battery

Fig. 1: Panasonic CR2032 coin cell battery. (Source: Panasonic)

There are three key factors that ultimately determine usable (as opposed to nominal) capacity of a coin cell:

The operating temperature

  • The battery load 
  • The “functional endpoint” (FEP) of the circuitry

Figure 2 illustrates the effect of temperature on the performance of a Panasonic CR2032 coin cell battery under a load of 0.19 mA. The graph shows that the effect of high temperature (60  C) isn’t overly dramatic, but lower temperatures do have a more significant impact that could come into play if wireless sensors are employed outside.

Fig. 2: The effect of temperature on CR2032 lifetime. (Source: Panasonic)

The FEP is determined by the component with the highest voltage requirement in the design. Modern silicon is economical, but there may be a chip, for example, that requires at least 2.2 V in order to function. Even if the rest of the components can operate from a lower voltage, if the 2.2 V device is critical to the operation of the sensor, the product will be useless once the voltage falls below this threshold.

One option is to swap the voltage regulator from a linear converter to a switching type (which can boost a battery’s voltage), but this adds cost and complexity to the design and may be hard to justify for a compact sensor. Figure 2 demonstrates it can be seen that, over a wide range of temperatures, the difference in lifetime for a product with an FEP of 2.2 V isn’t very much when compared to that of an FEP of 2 V; but under different operating conditions the effect can become much more significant.

For example, a wireless sensor typically employs a low-power radio technology, such as Bluetooth Low Energy or ZigBee. Such technology keeps the average power consumption down by engaging an extreme duty cycle whereby the radio is asleep for most of the time. However, when operating, the radio places a relatively high demand on the battery. Because the radio switches on and off in a regular sequence, the demand comes in pulses, which have a more detrimental effect on battery lifetime than a constant load.

Figure 3 shows discharge curves for a CR2032 coin cell battery (for a device with a nominal capacity of 225 mAh) when subjected the 10, 30, 50 and 80 mA high-peak, pulsed currents under a cycle comprising a 1-ms burst of activity at a frequency of 40 Hz. At 80 mA, it can be seen that both the high-peak current and the high-average current challenge the battery and will likely cause damage. At more practical operating currents of 30 and 10 mA, the 2 V FEP is reached after the battery has been drained of 180 mAh and 190 mAh, respectively. Note that at an FEP of 2.2 V, the difference is more marked. At a pulse current of 30 mA, the 2.2 V FEP is reached after just 160 mAh compared with 185 mAh for a pulse current of 10 mA.

Fig. 3: CR2032 discharge curves under various pulsed peak currents. (Source: Nordic Semiconductor)

Maximizing Coin Cell Battery Life

When formulating a design for a wireless sensor, a good place to start is the datasheet for the radio chip because that component exhibits one of the largest power draws in such a device. It’s advisable to check both average and peak-current for applications similar to the target use case.

Beyond the radio chip, the engineer should consider extending the FEP margin by selecting chips with as low a minimum supply voltage as possible and minimizing the current drain by selecting devices with the lowest peak current. To keep the design simple and reduce the bill of materials (BOM), the designer should select a linear voltage regulator, but take into account that this type of regulator can only step down the input voltage to a lower output voltage — and the higher the difference between input and output, the lower the efficiency of the regulation and the greater the impact on the battery.

By incorporating a power management system that prevents multiple high-drain devices loading the battery at the same time, the coin cell’s life can be further extended. Design engineers should remember that any high-peak, pulsed load — not only those from RF circuitry — will similarly impact battery life. For example, the high-peak, pulsed loads could also come from a combination of LEDs, vibrating motors, piezoelectric buzzers, LCD backlights and other components.

Dividing the “corrected” battery capacity (an estimate of the useable capacity for the particular application before the FEP is reached and is likely to differ from the nominal capacity) by the average current draw in the typical operational mode will provide a good estimate of battery life for the product in the field.

Internet of Things: Designing Sensor-Based Devices with Coin Cell Batteries

Display portlet menu

Internet of Things: Designing Sensor-Based Devices with Coin Cell Batteries

Display portlet menu
Related Articles
Person controlling robotic machinery with a tablet
IoT Platforms: Build, Buy, or Both?
By Lou Lutostanski   -   April 9, 2020
With the accessibility, affordability and overall democratization of technology, it is tempting today to try and do everything yourself.
Sensor for market of IIoT
Wi-Fi 6 is here. Is it time to make a move?
November 11, 2019
The Wi-Fi Alliance announced in September 2019. This refocuses attention on Wi-Fi, an old friend who has been quietly by our side but hardly top-of-mind.
A group of colleagues working in a computer security room having a discussion
Can IoT Apps be protected with Azure Sphere? Have you worked out how to bridge the hardware gap?
March 5, 2019
The three-in-one solution system offered by Azure Sphere – namely, secured MCU, secured OS, and cloud security, looks so perfect that you would expect comprehensive IoT security to be within easy reach.
A group of colleagues working in a computer security room having a discussion
Who provides the “hard” support behind Microsoft’s Azure Sphere IoT security platform?
March 5, 2019
Two years after its official release, Azure Sphere, Microsoft’s IoT high-security application service development platform, was launched for commercialization in February 2020.
A group of colleagues working in a computer security room having a discussion
Avnet and Microsoft Azure Sphere: IoT security in hardware, software and at the edge
March 5, 2019
IoT has transformed various industries by automating them at large, but the security concerns associated are just as large as the market opportunity this technology presents. That’s where Azure Sphere comes in.
A group of colleagues working in a computer security room having a discussion
Harnessing the power of IoT
March 5, 2019
Unique hardware, software and security requirements have to be addressed at every stage of the development cycle.
IoT conceptual icons in cloud server room
IoT: More Than Just Cool Technology
By Alex Iuorio   -   April 25, 2017
I can’t remember the last time I read an article about the Internet of Things (IoT) that didn’t start with market projections about the phenomenal number of devices that will be enabled in the next five to 10 years.
nightime cityscape with floating IoT icons
A decade of smart cities: What has changed and what has remained unchanged...
October 21, 2019
In the latest global smart city development report published by MarketsandMarkets, the global market size for smart cities is expected to grow from US$308 billion in 2018 to US$717.2 billion by 2023, at a compound annual growth rate of 18.4%. Since i
a cat and a dog laying next to each other on a bed
Strange Bedfellows: Marketing and IT
April 14, 2020
The Internet of Things (IoT) is creating a special alliance between two business departments that aren’t always a natural fit: Marketing and IT.
man wearing virtual reality headset with graphic overlays
How LoRaWAN and AI at the Edge Revolutionize the IoT
January 3, 2020
Learn how LoRaWAN and artificial intelligence (AI) at the edge can revolutionize the internet of things by reducing data transmission and improving latency.
couple checking smart watches while exercising
Redefining nanopower for the Internet of Things
December 9, 2019
Internet of Things trends today revolve around shiny objects—whether they be artificial intelligence or blockchain—but what if one of the most revolutionary parts of the IoT is something designers consider every day in devices?
Graphic of lightbulb made up of gears
Paving the way for IoT in your organisation
November 14, 2019
In order for businesses to accelerate innovation by harnessing IoT, they have to overcome three key challenges – getting stakeholder buy-in, implementation and lifecycle management.
2D image of smart phone charging on mobile battery
Why does Iq matter for USB Type-C?
November 11, 2019
This change is driving an increase in demand for Type-C AC/DC chargers and power banks because the Type-C connector has flip capability which gives convenience to users.
man controlling home security from a tablet
Would you believe it? The next five years will be the era of Smart Home 2.0
November 11, 2019
2014 was generally viewed as the beginning of smart homes, marked by Google’s symbolic acquisition of smart thermostat maker, Nest for US$3.2 billion. Since then, smart home companies have sprung up.
avnet branded USB type C connector
It is time to say goodbye to Micro USB!
November 11, 2019
Type-C’s greatest advantage is its integration capability. In addition to not having a right or wrong side (a perennial problem for Micro USB users), Type-C is able to offer integrated power delivery (PD) during charging.
depiction of data flowing against a black backdrop
Data Defines Your Destiny in IoT
By Lou Lutostanski   -   November 11, 2019
Data can be daunting. It’s intangible, invisible and typically isolated in physical things like the trucks in your fleet, monitors in your hospitals, or machines in your factory.
depiction fo digital security
Who decides whether an IoT device is secure
November 11, 2019
Global IoT is continuously expanding. A source of concern is that, along with network scale, the challenges of IoT security are also increasing.
depiction of digital security
Add security to your IoT devices
November 11, 2019
As the development of Internet of Things (IoT) gains momentum, its security issues have become increasingly important. Safety certification of IoT devices is critical to improve the security of IoT.
Sensor for market of IIoT
What Types of Sensors Are Required by the Trillion-Dollar IIoT Market?
November 11, 2019
The trillion-dollar IIoT is the driving force behind a new surge of development for industrial sensor products. Keeping abreast of this exciting trend in the IIoT sector will help ensure that our new designs are both relevant and innovative.
depiction of digital security
Providing one-stop service for IoT service development
November 11, 2019
To accelerate customers’ success in the Internet of Things market, Avnet has gained the capability to offer an end-to-end solution in IoT.
Using Programmable Logic to Build Power-Efficient Systems
October 29, 2019
The successful implementation of the Internet of Things (IoT) requires new thinking about how to power connected devices.
technician working on curcuit board
Wired together: How automation systems power the Industrial Internet of Things
July 16, 2019
From process control and automotive assembly, to robotics and the food and beverage industry, the concept behind Industry 4.0 touches all industries.
Four co-workers sitting at a table collaborating
Getting started in enterprise IoT: Six tricks for solving the puzzle
July 9, 2019
IoT is like a technological Rubik’s Cube. Here are some of the best tips to solving the IoT puzzle.
Solar panels providing an alternate power source with the city skyline they are powering in the background
Alternative Solutions For Powering IoT Devices
June 26, 2019
In this article, we look at why edge devices need power, and the options for reducing this need to a level where energy harvesting becomes sustainable.
technician working on circuitboard
Don’t ignore analog—it’s the secret sauce of IoT
May 19, 2019
Most of the innovation in IoT is focused on digital technology. From power servers running software in the cloud, to increasingly more intelligent devices operating ever closer to the edge in our factories, homes and personal devices. What is often l
IoT connect sign
Special Coverage | Chia-Yuan Chang at Avnet: One-stop solutions simplify and expedite the development of IoT
May 16, 2019
A hot new concept and enthusiasm are not enough to ensure a successful business. It requires steady research and development and lots of practice. And it needs more support from the upstream solution providers. Avnet is dedicating itself to providing
Robot holding holographic image of a brain
Robots, reimagined.
May 16, 2019
The era of cobots has dawned. Having a robot like C-3PO from Star Wars to keep you company may not be possible in the foreseeable future. However, having a cobot prepare your daily bento box may soon become a part of the “new normal.”
smart car 2D image displaying safety sensor ranges
We’re All Part of the Automotive Evolution
April 23, 2019
ADAS (Advanced Drive Assist Systems) and its evolution into full autonomy could see the end of road-based fatalities, injuries and incidents. Technology is now providing the solutions that can help the automotive industry achieve Vision Zero within
designing for intelligence chart
Designing for the IoT as Intelligence Moves to the Edge
April 23, 2019
The Internet of Everything will be all inclusive, from huge data centers to single-purpose sensors. While individual power requirements vary across the IoT, the need for energy efficiency will be present everywhere.
Woman sitting at a desk looking at her cell phone and with also has her laptop open
Don’t get caught in proof of concept purgatory
April 9, 2019
Here are the 5 classic signs you are in PoC purgatory.
design engineer working on tablet
Specialists vs. end-to-end partners: the pros and cons for developers
March 27, 2019
Getting a product to market requires more than just the right idea; it also needs the right partner.
smart watch with IoT icons around it
Wearable product plays a key role in IoT
March 27, 2019
Just as its name implies, Internet of Things (IoT), is a kind of Internet among connected things. This can be interpreted by breaking it down into two parts. The first is ‘Internet’. In other words, the Internet is still the core and foundation o
weather monitoring sensors near a lake
Making sense out of sensors
March 26, 2019
If creators still don’t think that sensors are getting the attention they deserve now, then there really is no limit to where the IoT can go.
illustration of two people shaking hands with overlay of data points
How to Turn IoT Insights into Action
By Bill Amelio   -   March 22, 2019
While an IoT platform can generate a lot of insight, you don’t improve your organization’s efficiency, increase customer satisfaction, or open a new business opportunity without applying it.
Home security system on tablet
Video Doorbells: Big Business in a Small “Cat’s Eye”
March 21, 2019
Home security has always been one of the primary focuses in a smart home. It is no surprise that home security cameras have become one of the hottest market trends over the past few years. But what will be the next up and coming product? From the loo
hand navigating home security on smart watch
Will Smart Homes Become the Next Fulcrum for the NFC Market after Mobile Payment?
March 21, 2019
Engendered in 2002, near-field communication (NFC) stands out from among other wireless connection technologies. With an operating frequency of 13.56 MHz, maximum speed of 848 kbps and typical communication distance of 10 cm, it is a safer and more c
field of green icons
The Art of Creating IoT Insights
By Lou Lutostanski   -   March 13, 2019
One of the biggest opportunities created by the Internet of Things (IoT) is the ability to use data to generate surprising new insights that guide you to act.
person holding superimposed globe with IoT symbols
Reimagining the ‘things’ of IoT
By Bill Amelio   -   February 28, 2019
While our collective vision for IoT’s impact on the future is grand in scale, it is still too easy for companies to get distracted by the minutiae of our present day IoT challenges.
A male nurse writing on a clipboard
How AI-powered virtual assistants can transform healthcare
February 26, 2019
We have witnessed a paradigm shift in the way patients are being treated by the doctors with the help of AI and machine learning.
A shopping cart sitting in front of the freezer section at the grocery store
4 ways AI connects retailers and customers
February 25, 2019
Technologies like machine learning and AI help retailers to process massive amounts of customer data. And with this data in hand, retailers can thoroughly understand their customers’ buying behavior.
Person controlling a robotic arm with a tablet
How leading manufacturing companies are reaping various benefits of AI
February 25, 2019
Manufacturing companies are applying AI-powered analytics for multiple use cases, such as, cutting unplanned downtime, better product designing, increasing product quality, ensuring employee safety, and many more.
futuristic city traffic with saftey sensor icons
The Car: A Rolling Smart Device
February 5, 2019
Be it for streaming your favorite music, sending emails or getting real-time information on traffic jams: cars have long since played host to mobile internet—and will continue to via diagnostics, hotspots and ADAS.
 Avnet booth at CES 2019
Our Top Takeaways from CES 2019
January 15, 2019
More than 180,000 people flocked to Las Vegas for CES, where Avnet debuted IoT and AI products as well as showed the expertise within our global ecosystem.
Person controlling a robotic arm with a tablet
5 of the best artificial intelligence use cases
January 3, 2019
AI’s upgraded algorithms make predictive analytics, parse data, and help businesses make smarter decisions from the boardroom to the factory floor.
People walking arund the Avnet City booth
The Avnet ecosystem comes to life at Electronica 2018
December 28, 2018
As much as we learn from our established industry experts, emerging developers as well as creators in our online communities, element14 and Hackster, are forging new paths, too.
 A group of people sitting at a table each using virtual reality headsets
Top 6 Trends: Get ready to meet the demand for IoT solutions
December 11, 2018
Gartner predicts that in less than two years, more than 20 billion Internet of Things (IoT) devices will be deployed. Here are the top six technology trends to ensure your IoT strategies are successful.
Person going through security using thumbprint scanning technology
2018 Was IoT’s Breakout Year
December 11, 2018
From connected devices at home to security cameras and sensors in factories, the acceleration of IoT has ignited the imagination and pushed product development in new directions in 2018.
Doctor checking on a patient from a remote patient monitoring device
AI From A-Z: The biggest buzzwords around artificial intelligence
November 28, 2018
Companies across markets from consumer electronics to factory floors are finding power in the introduction of two letters: AI. The world of artificial intelligence is vast...
worker using tablet computer to monitor industrial robotic arm
The Building Blocks of IoT: You Just Can't Stack Them Up
By Bill Amelio   -   November 14, 2018
I’ve spent my entire career in the business of technology, and I’ve watched many ideas go from “shiny new object” to “buzzword” to “table stakes.”
Group of men and women in meeting
How startups can integrate with design partners
November 9, 2018
While it might feel like the rubber truly meets the road at the manufacturing stage, the design process is truly where creators’ great ideas take shape. It’s also where you’ll make major decisions that impact your production and deployment.
Concert goers attending the Music Not Impossible concert
How the Deaf Experience Music—Then and Now
November 8, 2018
When you think of experiencing music, what comes to mind? The rhythm, cadence, beat, pitch—the sound.
three buisness men standing looking at monitor
The 3 IoT Security Fundamentals Startups Need to Know
November 6, 2018
An enterprise healthcare business faces risk and privacy considerations every day. However, in a startup environment, when funding sources—or lack thereof—are looming every day, security might not be on the top of your mind.
young professionals in office setting around computer screen
How to Turn Your IoT Solution into Recurring Revenue
By Lou Lutostanski   -   November 6, 2018
Companies in almost every industry are investing in Internet of Things (IoT) applications with high hopes of creating new revenue streams. Here's how you can ensure ROI from your deployment.
Edge AI robotic hand using laptop
IoT at the Edge: How AI Will Transform IoT Architecture
By Lou Lutostanski   -   October 26, 2018
Futurists say artificial intelligence (AI) and the Internet of Things (IoT) will transform business and society more profoundly than the industrial and digital revolutions combined, and we’re now starting to see how that world might shape up.
professional man and woman shaking hands at informal meeting
Does Your IoT strategy have a connection problem?
September 7, 2018
You’ve heard it everywhere: IoT is a game-changer, a disrupter and a gigantic business opportunity for everyone. That’s all well and good. However, the reality is that many companies have eyes bigger than their stomachs when it comes to the Inter
arial view of a planning meeting with charts and graphs
Customization comes with a competitive edge—and security challenge
By Guillaume Crinon   -   September 6, 2018
We talked about this before: there’s no one-size-fits-all IoT solution because every industry, vertical and business is different. Whether you have an in-house team or are exporting the building of infrastructure to a trusted partner, make sure the
Business people around a table in a meeting about IoT security
Customization comes with a competitive edge—and security challenge
By Guillaume Crinon   -   September 6, 2018
Whether you have an in-house team or are exporting the building of infrastructure to a trusted partner, make sure the team is asking the right questions when it comes to implementing and deploying IoT solutions.
Battery powering
Batteries are key to charging options
July 6, 2018
Wired power is a strong option for developers that need to get to market fast and require an inexpensive, proven solution. For products where convenience and future compatibility are paramount, you can move forward confidently with standards-based wi
Smartphone held next to locked door
How Secured Is Your IoT Business?
June 18, 2018
Think of reliability, safety and profit when considering security in the Internet of Things
group gathered at Avnet's IoT World booth in 2018
Blending IT, OT among hot topics at IoT World 2018
May 17, 2018
Avnet Internet of Things experts harnessed the knowledge gained from working with more than 2 million customers around the world to present ideas at this year’s IoT World in Santa Clara, Calif.
Bill Amelio, Chief Executive Officer, Avnet, Inc
As technology reshapes our world, ecosystems reshape our business models
By Bill Amelio   -   April 25, 2018
There’s an old saying, “You are only as good as the company you keep.” That has never been more true than today.
Man and woman making an adjustment to hardware wiring
Why Blockchain May Not Reach Beyond the IP Gateway in IoT Security
By Guillaume Crinon   -   April 19, 2018
Blockchain is a technology initially deployed at the heart of crypto-currency systems such as Bitcoin or Ethereum where the basic idea is to get rid of centralized banking systems ruling monetary transactions.
young professionals in engineering design studio
Survey Says: Creators See Progress Moving Technology from Development to Market, but Hurdles Still Remain
April 9, 2018
It’s become cliché, but nonetheless it still holds true: hardware is hard. There are dozens of reasons why your product may never see the light of day, but the good news is that creators and makers have an unprecedented access to technology.
young man and woman inspecting equipment in computer datacenter
Buy or build your IoT infrastructure
By Michael Lamp   -   March 6, 2018
To build or not to build? That’s the question many businesses face when starting to create plans for an IoT project.
Three young men and young woman chatting in meeting room
3 Steps to IoT Deployment
March 6, 2018
Learn how to set your IoT solution up for success.
Business people in meeting
IoT for Enterprise: 4 Concerns to Consider Before Deployment
By Michael Lamp   -   March 6, 2018
Interoperability, customization and convergence - some of the main concerns businesses tend to face when it comes to deploying IoT.
Two young men and young woman looking at tablet computer in datacenter
IoT Technology 101
By Christian Curtis   -   March 6, 2018
Learn what’s in market today for IoT and what innovations are ahead.
Two men and woman reviewing technology products.
3 ways All Programmable SoCs create new opportunities for designers
March 2, 2018
Usually, two heads are better than one. Yet sometimes, they introduce conflicting perspectives and priorities.
smart devices on charge pad: phone, watch and tablet
With the rising popularity of 7.5W wireless charging, Avnet helps companies obtain rapid product certification
February 25, 2018
The current wave of wireless charging technology, fueled by the new iPhone from Apple, is showing strong momentum growth. Semiconductor suppliers around the world have started making substantial investments in new IC solutions while a low barrier to
A couple sitting at their kitchen counter
Sigfox is the world’s leading provider of connectivity for the Internet of Things (IoT)
February 12, 2018
With its global LPWA (Low Power Wide Area) network, Sigfox has reinvented connectivity for the IoT.
Young male engineer working on a prototype
5 (nearly) universal IoT security problems
February 6, 2018
Can you solve your Internet of Things dilemma for a couple bucks? Just maybe.
Four people sitting at a table collaborating on a project
Why does it take 10 partners to start an IoT project?
January 18, 2018
The Internet of Things is more than just a buzzword, it’s a multibillion dollar industry opportunity—at least, for those brave enough to take on the complexity.
Avnet booth at the 2018 Consumer Electronics Show
3 Hardware Takeaways from CES 2018
January 18, 2018
At times, it feels like software dominates the headlines in technology. But if this year’s Consumer Electronics Show (CES) is any indication, a huge hardware evolution is coming.
Woman using tablet and working in data center
The importance of end-to-end security schemes for IoT deployments
By Guillaume Crinon   -   January 18, 2018
IoT machine and device security relies on trusted identities.
Person checking battery charge level on their cell phone
3 levels of Qi testing
November 24, 2017
You’ve designed, prototyped and built a revolutionary product with cutting edge Qi technology – congrats! Before you get to officially certifying your Qi product, you’ll need to do some testing to ensure its veracity.
man pulling smartphone from pocket
Watch for these two problems in your Qi wireless charging project
November 14, 2017
Here are two of the most common problems engineers face in integrating Qi wireless charging in their projects.
charging cell phone in automobile
How to get your Qi project certified by the Wireless Power Consortium
November 14, 2017
By aligning with the Wireless Power Consortium and Qi standard—the way big name brands like Apple, Samsung and Avnet have—you can help verify the quality of your product to new customers.
Bill Amelio, Avnet CEO
Qi standard is for more than just smartphones
By Bill Amelio   -   November 14, 2017
I’m not alone in my suspicion that the engineering world will soon follow a singular standard for wireless charging: the Qi standard. I think it would be the right move—and its impact would extend far beyond the charging of mobile phones.
blue digital screen
LEDs: The Eyes and Ears of the Internet of Things
November 8, 2017
It may seem to be a stretch to assert that LEDs play a truly important role in the future of the Internet of Things. After all, by themselves, they’re just lights. However, with sensors tucked neatly inside and a bit of intelligence...
Graphic depicting kitchen appliances talking to each other
Alarm bells ring for unsecured connected devices
October 11, 2017
A hot topic at the annual Black Hat cybersecurity conference in Las Vegas this summer was the increasing risk companies are facing with the Internet of Things (IoT).
senior couple having tea with green IoT icons overlay
Worried about your elderly parent living alone at home?
September 10, 2017
New technologies can help the elderly to continue leading independent lives. Sensor-based systems using complex analytical methods are able to detect emergencies and call for help when necessary.
side view of a sports car from the ground up
Understanding the Power of Battery Management Systems
August 28, 2017
According to estimates, China's EV battery market will reach RMB 120 billion by 2010, at which time the EV BMS market is expected to be valued at RMB 17 billion. Although the cost of BMS relative to the entire EV is relatively low, developers should
person looking at smartphone with IoT icons overlay
Sigfox enters market
August 28, 2017
The goal of Sigfox is to build a wireless wide area network that is completely independent from the existing wireless lattice network, to provide low speed connections for low power sensors. As of the end of 2017, it has covered a total area of 3.8 m
2D image of blue and orange city buildings with hovering IoT icons
Looking to develop NB-IoT technology?
August 28, 2017
Narrowband-IoT (NB-IoT) is a technology standard developed by 3GPP to work in licensed bands. It holds a key position in the evolution of cellular mobile communication technologies (between LTE and 5G), and has therefore been gaining followers among
conceptual image of tablet with connected IoT icons on top
The Spring for the Industrial Internet of Things
August 28, 2017
If we combine traditional industries (including manufacture, exploitation of natural resources, construction, public utilities, etc.) with the transportation and health service sectors, about 46 percent of the global economy, or US$32.3 trillion in g
smart phone with bluetooth logo on the screen and IoT icons overlay
Bluetooth 5.0 and Business: So, you think you've see the bigger picture?
August 28, 2017
Bluetooth 5.0 provides a solution to the issue by extending the data length to 255 bytes, thereby allowing more possibilities in commercial applications.
man pointing to bing map on smart phone
Redefining HMI in the intelligent age
August 28, 2017
Looking at how common smart technologies have become, it is hard to imagine that they have only came into existence in recent times. Impressive as it may seem, what we are witnessing is only the tip of the iceberg. Technology giants around the world
smart car driving towards a sunset
How far exactly can an Electric Vehicle (EV) travel?
August 20, 2017
"How far can an EV travel" is no longer just a question of mileage range technology but also one of great concern to businesses within the field, or rather how much more the industry can achieve. From the technical perspective, two problems must be r
smart phone controlling smart TV
Say goodbye to “reaching out for money” in the near future
August 15, 2017
In the past, we’ve always had to remember to bring the four things we should have on us when leaving the house: ID, cell phone, keys, and wallet. Nowadays, cell phones have become the only, absolute necessity, because the wallet has been replaced b
hand holding digital image representaiton of biometrics device
An overview of the top six commercialized biometric authentication technologies
August 8, 2017
“The best of times” refers to the accelerating development of the biometric authentication market. Research data indicates that the global biometrics market is slated to grow from US$15 billion in 2016 to US$30.5 billion in 2021, a compound annua
Graphic illustrating connectivity clouds hovering above a city
Harnessing the power of IoT: Microsoft’s unique approach
June 11, 2017
Little could this now-famous British serial entrepreneur have known in 1999 that the name he chose to define his approach for using RFID in P&G’s supply chain would top Gartner’s 2015 Hype Cycle for Emerging Technologies report.
man drawing schetch of an electric car attached to a battery
Technologies and Components for Designing Electric Vehicles
April 29, 2017
Hybrid electric vehicles (HEVs) such as the Toyota Prius and the Chevy Volt and electric vehicles (EVs) such as the Nissan Leaf, BMW i3 and Tesla Model S are growing in popularity amid concern for global warming.
Depiction of a city connected via wireless connectivity
How Retailers are Using Location Awareness Technology to Track Buyers’ Habits
April 25, 2017
Location tracking has been in use for a lot longer than one may expect. For example, military Special Forces and intelligence organizations have been using trackers and tracers for decades.
energy harvesting concept with green batteries sprouting from the ground
Powering the Internet of Things via Energy Harvesting
April 25, 2017
The push is on to add Internet capability to everything—often called the Internet of Things (IoT)—and the challenge for design engineers is to figure out how to power each of these IoT nodes.
Clothes hanging on racks in a store
The Internet of Slacks? IoT and Smart Clothing
April 25, 2017
When you think of wearable technology you probably think about those fitness trackers that you wear on your wrist. What you probably don’t think about is your shirt, your pants or even your socks.
IoT icons with a world map background
Insurance and the Internet of Things
April 25, 2017
It’s one of those things you only think about when you need it. Insurance. It’s our safety net for so many important parts of out lives and can sometimes be the key to a quick recovery – both physically and financially.
illustration of clouds with data storage symbols
The Internet of Things Pushes the Possibilities Offered by Big Data
April 24, 2017
The concept of the Internet of Things (IoT) encompasses things as tangible as a light switch, things as ethereal as a cloud, and all things in-between.
man pointing to the word insurance
Risky Business: IoT’s Impact on Insurance
April 23, 2017
Risky Business: IoT’s Impact on Insurance By Steve Gereb August 25, 2016. I enjoy reading about how the data collected by Intelligent Systems will help people live better lives.
woman looking at tablet on airplane
The Internet of Things at Cruising Altitude: Airlines and the IoT
April 20, 2017
What are your thoughts when you step onto an airplane? “Where’s my seat?” “Is this a Wi-Fi flight?” “I hope I make my connection.”
man holding tablet with chart image
Study: Digital Intelligence Driving Massive Business Transformation
April 14, 2017
The Internet of Things (IoT) is widely regarded as the next revolution in technology. Cisco predicts that by 2020, there will be 50 billion things connected to the Internet, generating revenues of $19 trillion.
man holding out his hand with icon overlay
The Internet of Everything is Here…or Is It?
April 11, 2017
The next great age of technology is the Internet of Things (IoT), if, that is, you believe everything you read on the Internet.
Yellow rainboots and gardening tools on flowerbed
The Internet of Things Has Thumbs – And They’re Green
April 10, 2017
It’s no surprise that technology, data and intelligent systems are transforming industrial agriculture.
graphic spelling out internet of things
Microsoft and GE Partnership to Make Industrial IoT More Accessible to Businesses
April 4, 2017
General Electric (GE) and Microsoft Corporation recently announced the beginning of a new alliance. The technology collaboration will make available GE’s Predix platform for Industrial Internet on the Microsoft Azure cloud for industrial businesses
Graphic of a person using IoT for several applications
Going Up? Elevators, Windows 10 And The Internet Of Things
March 30, 2017
People are excited about the Internet of Things for a variety of reasons. It’s already made us more connected. And as more and more things are connected, a number of industries are poised to become faster, more efficient and more reliable.
IoT concept -- smart phone with IoT icons
OCF and Thread Group Alliance Boosts Windows 10 and its Smart Home Initiative
March 29, 2017
Open Connectivity Foundation (OCF) and Thread Group, recently collaborated to fire up the automated ‘smart home’ functionalities on the Windows 10 operating system.
beer taps in a row
Internet of Beer? Avnet Helps iKeg ‘Tap’ Into the Internet of Things
March 26, 2017
You might think that running out of beer is only a major concern if you are the “refreshment coordinator” for a college fraternity, but it turns out that beer inventory management is actually a pretty big deal for bar and restaurant owners these
Depiction of IoT for various modes of transportation
How the IoT will Change the Supply Chain?
March 24, 2017
The potential applications of Internet of Things (IoT) technology across any industry or sector are vast. Existing and future IoT applications promise new ways of value creation and revenue streams for businesses in a digital world.
chart depicting device power states
Power Management Techniques for Low-Energy IoT Devices
March 24, 2017
With the rise of the Internet of Things (IoT), embedded designers are, more than ever, focusing their attention and efforts on system energy usage.
cyber security chip on circuit board
IoT Proliferation Teeters on the Edge
By Alex Iuorio   -   March 24, 2017
Cybersecurity and the irony of what happened during U.S. President Barack Obama's January 12, 2015 speech to the Federal Trade Commission on the growing threat, during which he declared: “If we’re’re going to be connected, we’ve got to be pro
Robotic machinery building a car in a factory
Ensuring robust connectivity in the industrial Internet of Things
March 23, 2017
The industrial Internet of Things promises to bring greater visibility and control of manufacturing processes.
Pigeons perched on the side of a building
London’s Pigeon Population Flocks to IoT
March 21, 2017
In one of the strangest, most innovative uses of Intelligent Systems we’ve seen so far, DigitasLbi Creative Director Pierre Dequesnoy came up with the idea of using pigeons equipped with sensor-loaded backpacks to analyze pollution in the UK’s ca
cloud servers
Securing LED Networks in the Age of the Internet of Things
March 20, 2017
Recently, in Nuevo Arenal, a little sleepy village in the Guanacaste region of Costa Rica, a dozen criminals cut the lights to the town’s main street during the quiet 3 a.m. hour, and then injured...
3D cityscape with IoT icons
Invest in the Future with IoT
March 20, 2017
You and I have known for a long time that connected devices are becoming pervasive throughout society, and it seems like the investment world is finally catching up.
diagram of smartphone and connected devices
IoT Security: Real Problems and Solutions
By Guillaume Crinon   -   March 18, 2017
Learn about the real issues behind “IoT security,” and challenges for customers both from hardware and embedded / server software aspects.
America flag with WIFI icon
It’s Time For The Government And The Internet Of Things
March 18, 2017
The Internet of Things or IoT has become quite the well-known term in the past year or two. What started out as a radical concept – connecting everything to everything else and to the Internet!
low power concept alphabetical chart
Internet of Things: Low Power, Low Cost Connected Devices Fuel Demand for Microco
March 17, 2017
At the heart of the devices that make up the Internet of Things (IoT) are a variety of ultra low power microcontrollers (MCUs), sensor networks, systems-on-chip (SoC) and communications protocols such as ZigBee. These underlying technologies operate
Front view of a man pointing his index finger and a gear icon
One-Click Manufacturing: Could It Really Be That Easy?
March 16, 2017
One click manufacturing (OCM) is a concept that arose from the 3D printing world: design a 3D model of a part ...
Graphic of cloud computing hovering over a tablet
Finding the best wireless option for your IoT design
March 16, 2017
The Internet of Things (IoT) relies on a facile communications framework able to move data easily between embedded "things" and systems located at higher levels of the IoT hierarchy.
digital image of the continents
The Edge to Enterprise - Avnet and IBM Partner to Deliver IoT Offering
March 13, 2017
This white paper examines the Internet of Things market with a lens on the complexity of the vendor ecosystem and how partnerships are enabling holistic solutions to come to market.
conceptual image of hand with legs and city background
Smart Cities: What To Look For In 2016 And Beyond
March 11, 2017
In a recent article in Government Technology, IDC research director Ruthbea Yesner Clarke discusses three trends emerging around the growing smart cities movement
hand holding smart phone with IoT icons emanating from the phone
Indispensable Building Blocks of Mobile IoT Devices
March 10, 2017
The concept of IoT connected devices connotes many different ideas. Some think of data centers full of servers, network switches and storage arrays aggregating untold gigabytes of random data. Others identify with Ethernet-enabled devices in their pl
bee polinating a puple flower field
What’s All The Buzz About? Bees And Smart Map Technology
March 8, 2017
You’ve heard about the problems with the bees, right? Their population numbers are dwindling and that’s not good news.
person wearing smart watch, working on laptop and  holding smart phone
Will HaLow open the door for more intelligent systems?
March 7, 2017
Reporting on the recent announcement of the “long-awaited Wi-Fi HaLow standard for products incorporating IEEE 802.11ah wireless networking technology,” Jim Hunter of Tech Crunch explains why this new standard may pave the way for more connected
conceptual graphic of IoT icons around a blue globe
An Introduction to IoT Components
March 7, 2017
From locomotives and jet engines to baby monitors and home appliance controls, new applications are challenging the imaginations of designers — both in startup companies and within giant corporations.
Graphic depicting the Internet of Things
For industry 4.0, reliability builds on robust connections
March 6, 2017
Looking to relieve increasing product complexity and cost pressures, manufacturers are moving toward the next phase of industrial automation envisioned in Industry 4.0.
business man standing on small rowboat in the ocean
What To Do With All That Data
March 6, 2017
Just as important as the hardware and the data it collects in an Intelligent System are the tools we need to process and analyze information. Otherwise, an Intelligent System does nothing to serve our purposes.
Binary code
Driving data with unintentional new uses: Internet of Things
March 3, 2017
The Internet of Things (IoT) is a natural evolution of the things we already make today.
Graphic depicting a human head with IOT written of to the side
Cognitive computing and IBM Watson IoT: unlocking the power of information
March 3, 2017
Businesses, academic institutions, cities, and other enterprises may have diverse objectives and missions but all have two things in common: Data, lots of it.
Graphic depicting cyber security
Circuit Protection: Helping Drive Reliability and Longer Life
March 3, 2017
The primary concerns of engineers designing mobile devices connected to the IoT remain device functionality, performance and feature set.
A person using their cell phone to connect to several mobile apps
Avnet: your key enabler for efficient IoT product development
March 3, 2017
There’s no shortage of hype when it comes to IoT! Fashion designers, futurists, gadget geeks, salespeople...
Depiction of a digitally connected city
Antennas for RF Designs in the IoT
March 3, 2017
The physical connection for many IoT nodes leverages legacy wired networks found in homes, offices, schools, factories and other areas. As we become mobile, wireless physical connections are becoming the norm.
Graphic depicting Wi-Fi connectivity
A “Canned” Module/IC Solution Simplifies Wireless Implementation, but Potential Design-in Issues Remain
March 2, 2017
Incorporating wireless connectivity into a product is now a standard design requirement for Wi-Fi, IoT, and other applications.
A city at dusk
10 companies and municipalities that are harnessing the Internet of Things to run smarter cities
March 2, 2017
Many of the devices we interact with today are enabled by computers and connected to the Internet. Much of the popular interest in the Internet of Things (IoT) focuses on consumer electronics, with everything from smart refrigerators to thermostats,
A graphic reading
10 things every intelligent systems needs
March 1, 2017
The Internet of Things (IoT) is changing the way businesses use technology. This web of interconnected devices and machines gathers information from gas-oil-water exploration sensors to sensors in corn fields, to medical devices and train control

Internet of Things: Designing Sensor-Based Devices with Coin Cell Batteries

Display portlet menu
Related Events

No related Events found