Four tech trends that improve the driver experience

Display portlet menu

Four tech trends that improve the driver experience

Display portlet menu

Four tech trends that improve the driver experience

Person using the navigation systemm on their car dashboard

According to a survey by the AAA Foundation for Traffic Safety, adult drivers spend up to 58 minutes a day in their cars. So it’s no surprise that with all that time spent commuting to work or stuck in traffic, drivers want the most enjoyable in-car experience possible. Car manufacturers are continually packing in more features to improve the driver experience.

In this article, I’ll discuss ways to integrate some the most innovative features into cars, including haptic-feedback touch screens, knob replacement, smart glass and driver-notification applications.

Integrated haptic touch screens

Some infotainment touch screens lack tactile feedback to confirm that users pressed the correct buttons. Screens that incorporate haptic feedback have the potential to improve road safety by decreasing the amount of time that the driver spends glancing at the center console screen. Typical haptic feedback found in tablets and phones is not sufficient, because the feedback strength needs to overcome the road and engine vibrations of everyday driving.

Many engineers are finding that a good way to achieve strong feedback is through the use of one or multiple solenoids paired with a solenoid driver such as TI’s DRV251x-Q1 family of solenoid drivers. Providing feedback with solenoids is different than using typical actuators like linear resonant actuators (LRAs), eccentric rotating masses (ERMs) or piezo. In order to drive solenoids that push a large mass, such as an 8-inch infotainment screen, you need a high-current-capable device. The DRV2511-Q1 integrated driver provides up to 8A of peak current to charge solenoids.

Figure 1 shows the current needed to drive a typical solenoid at 15V; the peak current is 2A. Depending on the weight of the mass being moved, solenoids could require a peak charging current up to 6A or more.

Chart showing solenoid acceleration - Texas Instruments

Figure 1: Solenoid acceleration graph: acceleration = 5.85G/div; current = 2A/div; voltage = 5V/div

 

Knob replacement

Replacing traditional knobs with newer haptic-enabled options can save automobile manufacturers money while extending the lifetime of car dashboards. Mechanical knobs consist of several moving parts that naturally degrade over time. At CES, TI will showcase a prototype that allows automotive designers to remove the mechanical parts and incorporate haptic feedback instead. This solution also uses solenoids and the DRV251x-Q1 family of drivers.  

We are working on a reference design that will integrate capacitive touch into the knob design to complete the feedback loop for a haptic knob. The knob will remain stationary, but as the user slides their fingers around the knob, the solenoid will actuate, providing a sharp click feeling. That feedback will make it seem as if the knob is moving like a typical mechanical knob. The images below show the top and bottom view of our 3D printed prototype knob.

TI 0825 3D printed solenoid knob   TI 212 3D printed solenoid knob

 

Smart glass

Did you know that there may be a revolution going on with your car’s tinted windows? With the advancement of glass materials, electrically tinted windows are now realistic. Using high-voltage piezo drivers, automobile drivers can have the ability to control the amount of tint on their windows based on the time of day or mood. TI’s DRV2700 piezo driver can provide the high voltage needed to tint smart glass while running off USB power levels. The DRV2700 has an integrated boost converter capable of 105VP, with a quiescent current of 24mA. Used in conjunction with a microcontroller, the DRV2700 can provide custom window tinting from clear to dark, as shown in Figure 3. This application of smart glass could even allow drivers to tint their windshields more when they leave their cars in the sun all day.

Man holding two samples of smart glass

Figure 3: Side-by-side image of glass changing colors

 

Driver notification

Driver notifications have also been widely integrated into automobiles. These notifications can be found in steering wheels or seats and alert drivers when other automobiles are in their blind spots, or when they cross over lanes unintentionally. Typically, powerful ERMs create a strong, rumbling haptic feedback. The DRV2605L-Q1 was created to drive ERMs and includes an integrated waveform library for different types of effects. This gives designers the flexibility to notify drivers with effects such as ramping buzzes, pulsing alerts and buzzes of different lengths. TI’s EvoCar, shown in Figure 4, demonstrated these different effects in the seats and steering wheel.

Man sitting in advanced electric car

Figure 4: TI’s EvoCar demo from CES 2016

While I’ve covered four different features, many more are in development to help drivers get the most out of their experience. Whether you are looking to update knobs to lower replacement costs and extend life spans or incorporate luxurious smart glass to increase driver privacy, TI has solutions to help bring your designs to life. Be sure to explore the TI Designs library for more automotive reference designs.

Additional resources

Contributed by Texas Instruments

Four tech trends that improve the driver experience

Display portlet menu

Four tech trends that improve the driver experience

Display portlet menu
Related Articles
interior of autonomous car
The State of Automotive Only Starts with Autonomous Driving
March 6, 2020
Learn how the state of automotive spans a variety of applications, from electrication to in-cabin AI.
view from autonomous vehicle as it interprets street signs
Somewhere Between the Flintstones and the Jetsons
March 6, 2020
Learn more about developing adaptable automotive automation with Xilinx
Smart car branded with Avnet and supplier logos
ADAS: paving the way for autonomous vehicles
November 11, 2019
In order to realize fully automated driving without human intervention, three conditions must be met - the vehicle must be fully aware of the surrounding environment, be able to respond accordingly when the environment changes, and the security of th
road view from inside self-driving smart car
Unreliable autonomous driving? Take a look at how difficult vehicle-mounted vision processing is
November 11, 2019
We all have high expectations for autonomous driving, a fact that’s exemplified by the display of autonomous driving technologies at every major tech expo. Development in this sector has however been accompanied by an increase in accidents related
test car colliding with object
Transportation Safety: 5 Protocols & Processes to Know
May 29, 2019
A dynamic range of protocols can help make our transportation technology safer.
cargo ship at port
Transportation Trends in Commercial & Non-Passenger Vehicles
May 29, 2019
Some of the most exciting technology trends shaping transportation are for commercial vehicles.
Graphic of 5G uses for automotive
5G is here – and maybe it’s time to buy a new car!
May 27, 2019
The mission of 5G is to create the ‘Internet of Everything’, drastically expanding the scale of the Internet in the process. As one of our most valuable possessions, it is inevitable that cars will join the network.
Interior of European self-driving car
Meeting Next-Generation Automotive Design Challenges
April 2, 2018
Thanks to engineering ingenuity and the electronic components that have become pervasive inside vehicles of all types, cars are smarter and, in many ways, safer to drive. As the automotive industry advances toward Level 5 fully autonomous vehicles, a
smartphone showing alarm feature
Key Design Considerations for Selecting the Right RF Antenna
March 16, 2018
Know when to choose standard, when to go custom.
smart car on the road at sunset with IoT icons overlay
Mastering the road ahead
August 28, 2017
The market demand for Advanced Driver Assistant Systems (ADAS) has increased by leaps and bounds. In fact, the global automotive electronics market is forecast to grow robustly over the next few years. In particular, the market value of entertainment
side view of a sports car from the ground up
Powering the future—the hidden heroes of electric vehicle technologies
August 14, 2017
The automobile industry in Mainland China has developed at an unimaginably rapid pace in recent years and a general trend can be observed in car sales figures. A little more than twenty years ago, automobile production in Mainland China numbered only
man in dirverless car with hands off the wheel
The Growth and Increasing Sophistication of ADAS in the World
July 5, 2017
As electronics in our cars continue to become more sophisticated, ADAS (Advanced Driver Assistance Systems) are taking center stage. These systems make many of the aspects of driving easier, and---most importantly—safer.
self-driving car at intersection
Top 5 Tech Trends in Advanced Driver Assistance Systems
June 15, 2017
Advanced driver assistance systems (ADAS) promise to enhance vehicle safety by helping to simplify the driving process, reducing sources of driver distraction and inattention that often lead to accidents. With ADAS support, drivers and their passenge
rear view camera on car dash with image of child riding a toy
Top 5 Myths in Automotive Vision: Designing Embedded Vision Systems Is Easier Than You Think
June 11, 2017
Vision has always occupied a special place in information science and popular culture. One does not need to be an engineer to appreciate the vast bandwidth available in normal human vision. Most people understand that the common saying “a picture i
man drawing schetch of an electric car attached to a battery
Technologies and Components for Designing Electric Vehicles
April 29, 2017
Hybrid electric vehicles (HEVs) such as the Toyota Prius and the Chevy Volt and electric vehicles (EVs) such as the Nissan Leaf, BMW i3 and Tesla Model S are growing in popularity amid concern for global warming.
Man navigating an IoT car dashboard
The Internet of Things is Driving The Internet of Autos
April 24, 2017
In the early 1900s Henry Ford made the automobile affordable and accessible. But what he really did was offer people connection. Rural residents could connect with more urban areas to sell crops and buy supplies.
smart car dashboard
New TFT LCD Technology Shape Infotainment for Cars of the Future
April 15, 2017
Although the technology has been around since the 1990s, the use of thin-film-transistor liquid-crystal displays (TFT LCDs) is on the rise in automobiles.
person driving a semi
Getting Started in Automotive Smart Vision Design
March 27, 2017
Advances in embedded vision technology have heightened interest in applying smart vision solutions for automotive safety.
Graphic of a car's outline
Gesture Recognition, Proximity Sensors Drive Advances in Automotive Infotainment
March 17, 2017
Safety must remain paramount when designing interactive interfaces for automotive applications, including guarding against distracted driving.
Person using the navigation console in their car
Automotive Electronics: Top 5 Tech Trends of Tomorrow’s Smart Cars
March 3, 2017
In the United States alone, motor vehicles travel well over four trillion miles each year according to the U.S. Department of Transportation.*
WiFi router with man in the background using tablet
How wireless communication protocols make or break designs
March 3, 2017
The design process includes many critical decisions for engineers, such as which wireless communications protocol to use.

Four tech trends that improve the driver experience

Display portlet menu
Related Events

No related Events found