batteries-are-key-to-charging-options

Display portlet menu

batteries-are-key-to-charging-options

Display portlet menu

Batteries are key to charging options

Battery powering

Editor’s note: A version of this article appeared on Hardware Studio.

Wired power is a strong option for developers that need to get to market fast and require an inexpensive, proven solution. For products where convenience and future compatibility are paramount, you can move forward confidently with standards-based wireless power. However, whether you are ditching cords for coils and diving into the $22 billion wireless charging industry or taking advantage of the tried and true wired method, one thing is for certain: it all comes down to the battery.

Making sure the battery matches the charging option, no matter if it’s the next great AI robot or a full industrial IoT deployment, is key to a product’s success.

Application can dictate battery, charging types

Countless battery types have emerged over the years. Lead acid technology dates back to the 1800s, yet it’s still used heavily in automotive and solar applications—so you’ll likely not come across it while researching applicable options for an instrument or wearable.

Nickel-metal hydride technology came along in the late ‘60s and remains a popular choice for consumer electronics and electric vehicles so it might be nice to consider.

However, for portable applications, these batteries are increasingly being eclipsed by lithium-ion, which offers superior power density and faster charging—at a higher price that’s usually worth paying. Lithium-ion batteries are common in consumer electronics and are gaining popularity in automotive and aerospace applications.

Which of these batteries is right for you? You’ll need to balance size and weight with cost, capabilities, and safety. Here are a few important characteristics that you should consider when exploring battery options.

Battery topologies important for powering devices

Get comfortable with two phrases: battery gauging and cell balancing. Battery gauging refers to a battery's ability to accurately assess and report its energy levels. This is an essential feature for most consumer electronics applications. Cell balancing is crucial to maximizing the capacity and extending the life of a battery. These attributes can greatly impact a user's experience of your product.

Battery configurations, also known as topologies, can have a big impact on the complexity and costs of your designs as well. These span centralized, distributed and modular:

  • Centralized topologies employ a single controller connected to multiple battery cells, each with its own communication wire. It's an economical approach that is a good choice for most consumer electronics products such wearables, connected home sensors, and even drones.
  • Distributed topologies feature separate controllers for each battery cell. This is the most expensive option but also the easiest to install, and most expandable.
  • Modular topologies provide a compromise between the centralized and distributed configurations – they use several controllers, each connected to a small number of cells. These topologies are most often used in products that require networks of batteries, like electric cars.

Consider all the options when designing new products

Understanding the pros and cons of each charging and battery option is key to realizing the full potential of your new product. To learn more about how startups can vet which options are right for your project, check out our communities, Hackster.io, element14 and Hardware Studio.

 

batteries-are-key-to-charging-options

Display portlet menu

batteries-are-key-to-charging-options

Display portlet menu
Related Articles
2D image of smart phone charging on mobile battery
Why does Iq matter for USB Type-C?
November 11, 2019
This change is driving an increase in demand for Type-C AC/DC chargers and power banks because the Type-C connector has flip capability which gives convenience to users.
avnet branded USB type C connector
It is time to say goodbye to Micro USB!
November 11, 2019
Type-C’s greatest advantage is its integration capability. In addition to not having a right or wrong side (a perennial problem for Micro USB users), Type-C is able to offer integrated power delivery (PD) during charging.
Using Programmable Logic to Build Power-Efficient Systems
October 29, 2019
The successful implementation of the Internet of Things (IoT) requires new thinking about how to power connected devices.
smart devices on charge pad: phone, watch and tablet
With the rising popularity of 7.5W wireless charging, Avnet helps companies obtain rapid product certification
February 25, 2018
The current wave of wireless charging technology, fueled by the new iPhone from Apple, is showing strong momentum growth. Semiconductor suppliers around the world have started making substantial investments in new IC solutions while a low barrier to
Person checking battery charge level on their cell phone
3 levels of Qi testing
November 24, 2017
You’ve designed, prototyped and built a revolutionary product with cutting edge Qi technology – congrats! Before you get to officially certifying your Qi product, you’ll need to do some testing to ensure its veracity.
man pulling smartphone from pocket
Watch for these two problems in your Qi wireless charging project
November 14, 2017
Here are two of the most common problems engineers face in integrating Qi wireless charging in their projects.
charging cell phone in automobile
How to get your Qi project certified by the Wireless Power Consortium
November 14, 2017
By aligning with the Wireless Power Consortium and Qi standard—the way big name brands like Apple, Samsung and Avnet have—you can help verify the quality of your product to new customers.
Bill Amelio, Avnet CEO
Qi standard is for more than just smartphones
By Bill Amelio   -   November 14, 2017
I’m not alone in my suspicion that the engineering world will soon follow a singular standard for wireless charging: the Qi standard. I think it would be the right move—and its impact would extend far beyond the charging of mobile phones.
side view of a sports car from the ground up
Understanding the Power of Battery Management Systems
August 28, 2017
According to estimates, China's EV battery market will reach RMB 120 billion by 2010, at which time the EV BMS market is expected to be valued at RMB 17 billion. Although the cost of BMS relative to the entire EV is relatively low, developers should
smart car driving towards a sunset
How far exactly can an Electric Vehicle (EV) travel?
August 20, 2017
"How far can an EV travel" is no longer just a question of mileage range technology but also one of great concern to businesses within the field, or rather how much more the industry can achieve. From the technical perspective, two problems must be r
man drawing schetch of an electric car attached to a battery
Technologies and Components for Designing Electric Vehicles
April 29, 2017
Hybrid electric vehicles (HEVs) such as the Toyota Prius and the Chevy Volt and electric vehicles (EVs) such as the Nissan Leaf, BMW i3 and Tesla Model S are growing in popularity amid concern for global warming.
energy harvesting concept with green batteries sprouting from the ground
Powering the Internet of Things via Energy Harvesting
April 25, 2017
The push is on to add Internet capability to everything—often called the Internet of Things (IoT)—and the challenge for design engineers is to figure out how to power each of these IoT nodes.
chart depicting device power states
Power Management Techniques for Low-Energy IoT Devices
March 24, 2017
With the rise of the Internet of Things (IoT), embedded designers are, more than ever, focusing their attention and efforts on system energy usage.
nurse checking person wearing health monitoring system on wrist
Internet of Things: Designing Sensor-Based Devices with Coin Cell Batteries
March 13, 2017
A popular vision of the Internet of Things (IoT) is that it will comprise billions of sensors gathering information about their local environment and transmitting that data back to servers in the cloud. Such data will be compiled, analyzed and shared

batteries-are-key-to-charging-options

Display portlet menu
Related Events

No related Events found