The global MLCC shortage: What are your options?

Updated on 23/06/2020
 

The state of the market

Back in August 2018, we reported the word was experiencing a global shortage of Multi-layer Ceramic Capacitors (MLCCs). Since then, the situation has changed, and growing demand across almost all areas of electronic applications is creating extremely challenging market conditions for the industry.

Industry-wide shortages of MLCCs are likely to recur in shortening market cycles, and may cause sudden increases in prices and lead times, in the worst cases leading to production line stops.

Alternative capacitor technologies may offer a more stable market environment and help offset the impact of unexpected MLCC shortages, from both a manufacturing and cost perspective. 
 

Why are MLCC shortages happening?

Increase in demand for MLCCs in smartphones, portable computing and the automotive industry has been considerably higher than manufacturers had previously anticipated.

While a car powered by an internal combustion engine has an MLCC count of around 2,000, the Tesla Model 5 is nearer 10,000. And between the iPhone 6s and the iPhone X, there was a jump in MLCC count from 500 to 1,000 per handset!

Although the development of the electric vehicle has played a role in the global shortage, the main demand is coming from mobile communications and computing devices. The increased functionality of these devices, combined with the need for portability, means the demand for high capacitance in small case sizes has increased, and will continue to do so.

On the supply-side, there are a number of factors contributing to a fluctuating MLCC market

Generally speaking, when prices are driven down on commoditised components, top tier producers often shift their focus to higher-margin opportunities. When this happens, and top tier producers move a product to a later stage in its life cycle, the slack is typically picked up by lower tier producers who can still make sufficient gains from these lower-priced products.

However, at the higher end of MLCC production, the technical challenges involved in the manufacturing process have prevented lower tier producers entering the market.

The manufacturing process for MLCCs (layering microscopically thin alternating layers of ceramic and metal) is complicated and results in varying yields, which poses challenges to profitability for less developed manufacturers. As a result, there are still only a small number of manufacturers who can achieve the highest levels of capacitance in this fashion.

This has created a significant barrier to lower tier manufacturers. Previous decreases in prices prevented top tier manufacturers from investing further, and this, combined with the increase in global demand has resulted and will result again in supply falling behind demand.
 

So what's the alternative?

One option to consider is downsizing, to follow the production trend of major MLCC producers, we recommend polymer capacitors as the most viable alternative.

Avnet Abacus is here to help you identify the best capacitor solution for your application, and in this article, we'll guide you through the technical considerations to determine whether polymer might be the right option for you.

If you’d prefer to discuss your precise requirements with a technical expert, you can get in touch with our capacitor experts in your local language.

 

 

Original article, published August 2018

The global shortage in Multi-layer Ceramic Capacitors (MLCCs) is creating extremely challenging market conditions for the electronics industry.

There’s an industry-wide shortage of MLCCs, and lead times, where quoted, are up to 50 weeks on new orders. In many cases, manufacturers have increased prices with immediate effect and have even applied price increases to back orders, regardless of when they were placed.

We’ve seen manufacturers move from extending lead times in 2017 to imposing strict allocations over a defined period in 2018, based on their capacity and the distributor’s historical backlog. Many manufacturers are no longer accepting new purchase orders from customers and in some cases are even cancelling existing orders.

Companies of various sizes are struggling to get their hands on MLCCs, which could result in production slowing down or even stopping. We’re already receiving anecdotal evidence of companies having reached line-stops because they can’t get the MLCCs to assemble their printed circuit boards.

Customers might consider resorting to non-franchised channels. But this comes with the increased risk of receiving counterfeit components which could lead to product failure and no recourse to the manufacturer.

The current market conditions are having a dramatic impact on customers, from both a manufacturing and a cost perspective.

And the situation is unlikely to improve for the next 12 to 18 months.

It’s not our intent to cause alarm. It’s our aim to provide you with information and help guide you through your options in this challenging environment.
 

Why the MLCC shortage is happening

The reason for the shortage is the increase in demand for MLCCs in smartphones, portable computing and the automotive industry. The increase in demand from these markets has been considerably higher than manufacturers had previously anticipated.

While a car powered by an internal combustion engine has an MLCC count of around 2,000, the new Tesla Model 5 is nearer 10,000. And between the iPhone 6s and the iPhone X, there was a jump in MLCC count from 500 to 1,000 per handset!

Although the development of the electric vehicle has played a role in the global shortage, the main demand is coming from mobile communications and computing devices. The increased functionality of these devices, combined with the need for portability, means the demand for high capacitance in small case sizes has increased, and will continue to do so.

So far, the situation has largely been driven by genuine demand as opposed to panic-buying, though it’s likely that mobile handset and automotive manufacturers will do what they can to shore up inventory to ensure continued production.

On the supply-side, there are a number of factors contributing to the current situation.

Generally speaking, when prices are driven down on commoditised components, top tier producers often shift their focus to higher-margin opportunities. When this happens, and top tier producers move a product to a later stage in its life cycle, the slack is typically picked up by lower tier producers who can still make sufficient gains from these lower-priced products.

However, at the higher end of MLCC production, the technical challenges involved in the manufacturing process have prevented lower tier producers entering the market.

The manufacturing process for MLCCs (layering microscopically thin alternating layers of ceramic and metal) is complicated and results in varying yields, which poses challenges to profitability for less developed manufacturers. As a result, there are still only a small number of manufacturers who can achieve the highest levels of capacitance in this fashion.

This has created a significant barrier to lower tier manufacturers. Previous decreases in prices prevented top tier manufacturers from investing further, and this, combined with the recent increase in global demand has resulted in supply falling behind demand.

The increase in demand, due to smartphones and electric vehicles means other sectors are feeling a squeeze on availability and delivery times, alongside price increases.

Manufacturers who can produce high cap MLCCs will, in due course, increase production capacity in response to the demand and increased pricing, but the time until shortages in the supply chain are overcome will be significant. Unfortunately, the component manufacturing business can’t move as quickly as the high-paced consumer electronics industry.

Overall, the situation has been described by some market analysts as the “perfect storm” of (economic) factors.
 

How long will the current situation last?

There is little sign of improvement in the next 18 months to 2 years. If anything, things look to be worsening in the short to medium term. 

Some expect the shortage to last up for up to three years at least.
 

So what can you do?

Previously, when there’s been supply difficulties with a specific manufacturer, we would recommend looking to other manufacturers for an alternative product. However in the current market conditions it’s  impossible to find availability on any direct alternatives as a short-term solution.

Because it isn’t going to get better any time soon, it’s advisable to consider alternative capacitor technologies and redesign products to minimise your exposure to the ongoing shortage of MLCCs.

If your design is reliant on MLCCs, you need to take action as soon as possible. And as such, it would be prudent to allocate engineering resource to consider redesign.

It’s important to gain a clear understanding of the potential impact on your current design cycle. And also to assess the opportunity in the medium term by considering MLCC downsizing or the possible application of polymer capacitors

All of these options will be application dependent and will require weighing up a number of important criteria.
 

What's the alternative?

We recommend polymer capacitors as the most viable alternative to MLCCs.

While tantalum capacitors could provide a suitable alternative in some applications, the lead times are now extending on those too. And as a result, they are rapidly becoming a less viable option.

In this article, we’ll guide you through the technical considerations to determine whether polymer might be a viable solution for your application:

If you’d prefer to discuss your precise requirements with a technical expert, you can get in touch with our capacitor experts in your local language.

MLCC Polymer Design Support Grid Box Light

Display portlet menu
Contact our product specialists

Ready to discuss your design options?

Want to talk over your design options with a capacitor expert? Have specific design requirements and need some samples? Our team of technical specialists are on hand to help.

Solutions

Yageo MLCCs

Alongside continual investment in R&D, Yageo is dedicated to the design and manufacture of reliable, RoHS compliant and Halogen free MLCCs.

Polymer vs MLCCs article Grid Box Dark

Display portlet menu

Technologies

Replacing MLCCs with polymer capacitors

Polymer capacitors are a viable alternative to MLCCs in a number of applications. Learn how some of their key characteristics compare and whether they could be suitable for your design.

An assortment of polymer capacitors

Panasonic Polymer Caps Grid Box Dark

Display portlet menu

Solutions

Panasonic polymer capacitors

With drop in replacements for a range of specifications, Panasonic polymer capacitors are go-to products when it comes to the replacement of MLCCs.

Panasonic OS-CON polymer capacitors

Subscribe to our Newsletters

Researching technology for your next application design? We can help you get project ready. Get the latest design tools and solutions, Engineers' Insight and Focus magazine sent straight to your inbox.

SUBSCRIBE