Customising and optimising antennas with materials science and manufacturing techniques

In an increasingly connected world, performance demands on antennas are greater than ever. These increased performance demands also have to be balanced with cost, and of course, the limits imposed by the laws of physics, which make antenna design a trade-off between performance attributes.

Read More

Keeping the noise down: Converter and inverter output filtering

Most modern power conversion topologies use switched-mode techniques for highest efficiency and smallest size and cost. Inevitably, switching noise is produced and output filters are required to minimise EMI and provide reliable operation of the powe...

Read More
Selecting DC-link capacitors in power converters

‘DC-link’ capacitors feature in many power conversion topologies and must be chosen carefully to give the best trade-off between cost, size and performance. ...

Read More
Input filtering and protection for switched mode inverters and converters

Inverters and converters have become basic building blocks for many modern power applications. These applications must meet statutory and practical requirements for input EMI filtering and protection against injury to personnel and equipment...

Read More
Specifying explosion-proof connectors

The threat of explosion is real in many of today’s industrial applications, and connectors are critical to explosion proofing since they have the potential to create arcs and sparks as part of normal operation....

Read More
Hybrid capacitors combine technologies to get the best of both worlds

Supercapacitors are commonly used as an alternative to a rechargeable battery wherever a quick energy boost is needed, however there is another type of device on the market which combines the best features of EDLCs and Li-ion batteries....

Read More
Sensor Fusion: The future of intelligent devices

Combining the data from multiple sensors can tell us a great deal more about the application environment than each sensor could on its own....

Read More

Filter Articles



 RESET

Engineering Services

Ask an expert

Have a question? Our regional Product Specialists are on hand to help

Subscribe to our Newsletters

Receive Engineers' Insight and Focus Magazine, plus all the latest NPI and manufacturer information straight to your inbox.

SUBSCRIBE