What’s Super About Supercapacitors? | Avnet Abacus

Display portlet menu

What’s super about supercapacitors?

Supercapacitors are an alternative to using a battery or indeed the more common-or-garden variety of capacitor in many energy storage applications, perhaps as backup power or for high-surge demand applications. Also known as ultracapacitors or electric double-layer capacitors (EDLCs), these devices come with many advantages over batteries including, very importantly, a maintenance-free long life. And of course the environmental impact of products is becoming increasingly important, which makes supercapacitors highly attractive for use in designs rather than batteries as they do not contain lead or other potentially harmful substances, making them compliant to EU directives such as RoHS. 

The range of applications these devices can address is extremely diverse ranging from long-life replacements for coin-cell batteries that back up real-time clocks, up to high capacity units that power servomotors in industrial control. In terms of energy storage, supercapacitors fit nicely into the gap between aluminium electrolytic capacitors and batteries: offering significantly greater capacitances and energy densities than conventional capacitors, but still only a fraction of the energy density offered by batteries. 

How supercapacitors compare to convential batteries and aluminium electrolytic capacitors is shown in the graph above

 

What is really super about supercapacitors is their ability to deliver a much greater power density – delivering energy to the load. They are ideal devices where there is a requirement for high capacitance and also rapid charge and discharge, so they bring significant benefits in both peak- and power-assist applications. Talking of this specific ability, there was a rather good blog about supercapacitors published last year by the Berkeley Energy & Resources Collaborative (BERC) that made a metaphor of the well-known Aesop fable of the Tortoise and the Hare (although strangely featuring a turtle instead of the tortoise). 

In this reimagining of the tale, the ‘rather-slow-moving-creature-that-lives-in-a-shell’ (in North Atlantic détente speak) is the battery, which delivers a slow and steady supply of energy. Whereas the pleasingly consistent hare (recognised on both sides of the pond) is the supercapacitor, which offers quick charging and discharging in lower energy applications. But unlike the moral tale, where it seems somehow important to have a winner, the point is to view these competing technologies as offering complementary qualities, combining to meet a desired goal, especially in next-generation vehicle applications such as electric and/or hybrid cars or buses. For example, supercapacitors are used for acceleration and deceleration and decreasing the weight of the batteries, which of course are required to provide the bulk of the energy required to power these vehicles. So, in many applications, at the system level, the combination can be much more than the sum of the parts.

Of course, possible applications for supercapacitors go well beyond electrically powered equipment and regenerative power systems in automotive hybrid and electric vehicles, although there is much excitement for the technology in this area. But in fact, the list of applications is extremely diverse. In energy storage applications, they can make a significant contribution to power saving in equipment that uses energy storage devices for standby power such as TVs, set-top boxes or other consumer equipment. Alternatively, they can be used as short term power backup in power utilities; or in power supplies used in life-support equipment, meaning there is no need to change batteries, thereby achieving a virtually maintenance free environment. In addition, they can work as power supplies in conjunction with solar batteries (for example), perhaps for outside or street lighting or flashing ‘cat’s eye’ road safety markers.  The other side is their use in high input or output load levelling for the protection of equipment such as control systems or potentially assisting in energy saving in power generation such as solar or wind-power generation systems.

In this area, Avnet Abacus offers a wide range of supercapacitors from world-leading suppliers such as AVX (BestCap series), Eaton (PowerStor XB and XV series), Murata (DMG series), Nichicon (UK series of EDLCs), Panasonic (Gold Cap range, plus the RF and RG series) and now KEMET. The Avnet Abacus KEMET product line has recently been extended to include a range of new devices including small-cell supercapacitors that target a wide variety of board-mounted applications such as RAM backup and small motor assist. If you require advice on the best supercapacitor for your application design, click the Ask an Expert button to get in touch with our regional technical specialists.

Written by

Adam Chidley

Adam joined Avnet Abacus in 2006 as a Sales Consultant, moving into Product Management 18 months later. As European Senior Product Manager, Adam is responsible for key supplier relationships and marketing strategy for Avnet Abacus’ passive business unit.

What’s Super About Supercapacitors? | Avnet Abacus

Display portlet menu

RELATED ARTICLES

Women in engineering – where are we now?

To mark International Women’s Day, we spoke to two female engineers at different points in their car...

Design trends: Automotive passives

Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough ...

From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica

And so electronica 2018 is over. In our final post, we look back on the best bits of day three....

Engineering Services

Ask an expert

Have a question? Our regional technical specialists are on hand to help