The Unstoppable Rise Of Polymer Capacitors | Avnet Abacus

Display portlet menu

The unstoppable rise of polymer capacitors

Capacitor dielectrics each have their advantages and disadvantages. Aluminium electrolytics offer high capacitance in a small space but are notorious for limited operating life, particularly in harsh environments, due to their wet electrolyte and the ongoing chemical reaction needed to maintain the aluminium oxide dielectric layer. Ceramic capacitors are noisy in acoustic applications and prone to short circuit failure when exposed to over-voltage conditions. Plastic film capacitors (polyester, polycarbonate, polypropylene and polystyrene) have a wonderful ‘self healing’ characteristic that makes them robust, particularly in response to voltage spikes, but their lower dielectric constants mean that they’re bulkier, at a time when most electronic devices are getting smaller. Tantalum electrolytics pack a lot of capacitance into a small space but they’re relatively expensive and when they fail the results can be explosive, creating a potential fire risk. Capacitors with impregnated paper dielectrics are expensive and big, but robust, so are still found occasionally in high voltage applications.
 
Just to confuse the situation, the plastic dielectrics mentioned earlier are all types of polymer but the ‘polymer capacitor’, first introduced in 1983, is an altogether different kind of component. Polymer electrolytic capacitors employ a conductive polymer as a solid electrolyte that forms the component’s cathode, rather than as an insulating dielectric layer, which is how it’s used in conventional plastic film capacitors.
 
The primary types of polymer capacitor are polymer tantalum, polymer aluminium, in both multilayer and wound metal can, and polymer hybrid, and the market for these devices is predicted to grow 30% to 40% in the next five years.

 

The benefits of polymer capacitors

The reasons for their popularity vary with the application but in general they offer high capacitance in small packages, long life, high reliability, and a host of other desirable electrical characteristics including:

  • Good high frequency performance, including low impedance and ESR (Figure 1)
  • High ripple current capability
  • Stable operation with respect to changes in temperature and bias voltage (Figure 2)
  • Elimination of the acoustic noise created by ceramic capacitors (piezo effect)
  • Wide operating temperature range, typically from -55 to +105 or +125 degrees C or more
 
Figure 1: Murata’s ECAS multilayer polymer capacitors offer lower ESR than other types of polymer capacitor – only multilayer ceramic capacitors are better in this respect   Figure 2: Polymer capacitors are far more stable than class 2 multilayer ceramic components, both with respect to bias voltage and temperature variations

 

Overview of polymer capacitor types

Polymer tantalum capacitors offer significant cost savings over traditional tantalum capacitors and don’t suffer from the ignition risk that the latter present. They have lower voltage de-rating yet still provide good volumetric efficiency, coupled with low ESR and ESL, so ripple current ratings are high too. The capacitance range is 0.47 to 1500µF at rated voltages from 2.5 to 125Vdc. The ESR can be as low as 5mOhms and ripple current ratings can be 4A or more for some devices.

Polymer aluminium of a wound construction in a metal can  come in values from 3.3 to 4700µF with voltage ratings from 2.5 to 125Vdc. They have lower capacitance per unit volume and higher leakage current than conventional aluminium electrolytic capacitors but this is offset by an ability to withstand high ripple current, low ESR and much longer operating life. 

Polymer hybrid capacitors are designed to combine the advantages of aluminium electrolytics with conductive polymer components, primarily the low leakage current of the first with the long operating life, low ESR (down to 14mOhms) and high ripple current capability (up to 4.34A) of the second. They’re sometimes called Polymer Lytic components. Capacitance values range from 6.8 to 1000µF and voltage ratings from 6.3 to 125Vdc.

Polymer aluminium multilayer capacitors are low voltage devices, rated from 2 to 25Vdc, and are available in values from 6.8 to 1000µF. ESR is very low – down to 2mOhms - and ripple currents can exceed 7A in some types.

More information

Avnet Abacus represents the world’s leading manufacturers of polymer capacitors including AVX (acquired Nichicon Polymer range), KEMET (including NEC Tokin), Murata, NIC, Panasonic (former Sanyo products), Rubycon and Vishay (acquired Holystone Polymer range).

A detailed white paper from Panasonic that explains the technologies of several polymer capacitor types can be downloaded here.

If you don’t mind registering your contact details, Murata has a good tutorial on polymer aluminium capacitors vs tantalum capacitors here.

Additionally, KEMET have an interesting technical piece on bringining the benefits of polymer tantalum capacitors to high-voltage, high reliability markets here.

If you need application advice or want to request samples, our pan-European team of technical specialists is always on hand to help. Visit the Ask an Expert page to get in touch.

Written by

Ekaterina Rachel

The Unstoppable Rise Of Polymer Capacitors | Avnet Abacus

Display portlet menu

RELATED ARTICLES

Design trends: Automotive passives

Cars used to be little more than four wheels, four seats, an internal combustion engine, and enough ...

From humanoids to holograms and humanity projects - How Avnet showcased the future at electronica

And so electronica 2018 is over. In our final post, we look back on the best bits of day three....

electronica 2018 day two highlights

Another day at electronica 2018 has passed and it was arguably even busier than the first. A constan...

Engineering Services

Ask an expert

Have a question? Our regional technical specialists are on hand to help